Představení bateriového elektrobusu GILLIG

Louisville, Kentucky
Bateriový elektrický autobus GILLIG poháněný motorem Cummins

Společnosti GILLIG LLC a Cummins Inc. (burzovní index NYSE: CMI) dnes oznámily, že bateriový elektrický autobus GILLIG s nulovými emisemi poháněný společností Cummins je nyní k dispozici. 

„Jako přední dodavatel autobusů vyráběných v Americe je společnost GILLIG nadšená, že může rozšířit své portfolio nabídkou na trhu nejkomplexnějšího řešení na bázi bateriové elektřiny u autobusů. This best-in-class bus is designed on our proven Low Floor platform, which offers the highest-quality, most reliable bus while retaining fleet commonality," said Derek Maunus, GILLIG President and CEO. "With more than 200 years of combined experience, GILLIG and Cummins have a long history of collaborating to adopt new technologies and innovate power solutions for transit applications. This new offering is continued evidence of our commitment to do so." 

The zero-emission battery electric bus incorporates the Cummins electrified powertrain, which features remote diagnostics and over-the-air connectivity and is backed by Cummins' unparalleled support network and service training programs. The bus initially incorporates the standard 444 kWh battery capacity (six packs) and supports charging interoperability via industry standards. Variants will include a 35' version and opportunity charging.

"Cummins is incredibly proud to bring a best-in-class fully electric bus solution to market with GILLIG," said Julie Furber, Vice President-Electrified Power, Cummins. "Our Battery Electric System is another example of Cummins unrelenting commitment to quality, dependable products. We're deeply committed to understanding our customers and their unique needs and providing market-leading solutions that enable their success."

Bateriový elektrický autobus GILLIG poháněný motorem Cummins

GILLIG is taking orders for the Cummins-powered battery electric bus. Sales inquiries for the bus can be directed to [email protected]

Note: Media are invited to join Maunus and Furber for the unveiling of the new GILLIG zero-emission battery electric bus on Monday, May 20, at 11:30 AM EST at the American Public Transportation Association (APTA) Bus & Paratransit Mobility Conference in Louisville, Kentucky. The event will take place at the GILLIG Bus Display on 4th Street.

O společnosti GILLIG LLC

GILLIG je předním výrobcem těžkých autobusů ve Spojených státech. GILLIG offers a portfolio of clean energy propulsions ranging from battery electric and diesel to natural gas and hybrid electric, all designed on the proven GILLIG Low Floor platform to maximize fleet commonality. Since 1890, our dedicated employees have been supporting customers and delivering on promises to improve quality of life through transformative mass transit solutions. From initial design through final assembly, each GILLIG bus is designed and built by American workers in Livermore, California, who are committed to building and supporting the safest and most reliable transit buses in the United States. GILLIG buses are known for their unmatched quality and have earned their reputation as the lowest-cost buses to maintain and operate. Our products help reduce congestion, contribute to a cleaner environment and provide mobility to all. GILLIG is also proud to create American jobs and recycle tax dollars back into the community to further support public transportation. Further information about GILLIG can be found at www.gillig.com.

Chcete se dozvědět více?

Dostávejte od společnosti Cummins nejnovější informace o technologiích, produktech, novinkách a poznatcích.