Spouštění plachet a nastartování se společností Cummins

Cummins engine receives a major overhaul after boat owner commits to a power vessel after years spent sailing the Pacific Northwest.

Katie Yoder, specialistka marketingové komunikace

MV brigáda

Pár ze Seattlu ve státě Washington (USA) strávil první polovinu 2020 přestavbou svého nového motorového člunu Hampton 490 Pilothouse. Chris Jones vyrostl kolem přístavů a během svého života vlastnil různé lodě. V poslední době se se svou ženou plaví kolem Pugetova zálivu na plachetnici Hunter 46. But with the turn of the new year, they decided to trade in the slow and steady lifestyle of sailing for a new power boat - the M/V Brigadoon.

After identifying they were ready to make the switch back to faster speeds, Chris and his wife began narrowing down what kind of vessel they were looking for. After weeks of extensive research, they found two Hampton boats available that met their requirements for quality, systems and seaworthiness.

Jones ventured down to California to look at one of the options, and at first glance thought the vessel had too much work to be done. But as the couple explored other boats, even comparing her to the alternative Hampton in the area, they found the M/V Brigadoon had the most potential.

But it would not be without major rework. The vessel needed a massive overhaul for the engine, control systems, and cosmetics. The 20-year-old boat only had 800 hours on it, which is quite low for an engine of that age. After years of sitting idle, it needed some tender love and care.

MV Brigadoon - Cummins

With an eye for improvement, Jones left his new acquisition in the hands of Marine Diesel Services in Newport Beach, California. The significant overhaul of his Cummins 6CTA 8.3 series engine included replacing aftercoolers, turbo chargers, hose clamps, seals, etc. Chris said, “They really did fantastic work on the boat. I have a lot of confidence in the power plant and that it has been adequately serviced.”

Once the mechanical work was complete, the M/V Brigadoon was ready to be delivered to the Pacific Northwest. At Emerald Harbor Marine, she received electrical work and new alternators, wiring, and navigation system. Finishing touches included more minor maintenance and a fresh paint job.

MV Brigadoon - Cummins

Six months have passed since the Jones' heralded the M/V Brigadoon as their own. In mid-July, they put their new baby into the water for their first cruise since stepping off their sailboat last year. Looking forward to the speed and freedom of a power boat once again, they intend to vacation in the San Juan islands during their shakedown cruise and find new ports to explore.

For more photos and information about the M/V Brigadoon refit or to follow her journey, check out Chris Jones’ Instagram.

Profily autorů

Sedlem Voder - Cummins Inc.

Katie Yoder, specialistka marketingové komunikace

Toto ubytování je specialistka na marketingovou komunikaci. Nastoupila do společnosti Cummins v roce 2018 jako členka obchodního týmu pro veletrhy, ale nyní podporuje marketingové iniciativy v segmentech námořní dopravy a ropy a zemního plynu. Jako absolventka Univerzity ve Wisconsinu tráví Strávila volný čas sledováním sportovních aktivit Voiltschingr.

Chcete se dozvědět více?

Dostávejte od společnosti Cummins nejnovější informace o technologiích, produktech, novinkách a poznatcích.