5 způsobů, jak mohou flotily zvýšit úsporu paliva
Cummins Inc., globální lídr v oblasti technologií pohonu
Fuel economy is of a chief concern across the trucking industry, and improving it can have a huge impact on your fleet.
Existuje mnoho sil, které tlačí na zlepšení spotřeby paliva těžkých nákladních vozidel, od nových vládních norem až po úsilí o úsporu nákladů v celém odvětví.
Despite this focus on fuel economy improvement, accurately measuring fuel consumption can be a real challenge for fleet managers. Rather than meticulously measuring every drop of diesel or LNG, fleets can focus on maximizing efficiency through the five ways listed below in order to ensure their fuel takes them as far as possible.
Work With Drivers
Pardon the pun, but operators will drive the majority of your fuel savings across the fleet. Since fuel typically accounts for more than 30% of trucking budgets, it's easy to see why educated, empowered drivers can have such a big impact on the health of the fleet. Drivers should be rewarded for efficient driving habits, and encouraged to place safe performance ahead of speed.
Maintain Maintenance Schedules

It can be easy for drivers and technicians to skip over a maintenance cycle or push it back until after their next trip, but we all know how proper maintenance affects fuel economy and engine performance. Key contributors to fuel economy, such as tire pressure and aerodynamic drag, should be assessed regularly. While drivers can ensure proper tire pressure, service technicians should always keep an eye on engine components and trailer aerodynamic devices to ensure minimum drag.
Right Equipment
Equipping your fleet with more efficient, versatile powertrains is one of the most effective ways to improve fuel economy and performance. Modern automated powertrains like the Cummins SmartAdvantage™ Powertrain have been shown to help improve driver efficiency and deliver up to a 6% increase in fuel economy.
SmartAdvantage Powertrains pair the strength of the Cummins ISX15 with the precision of the Eaton Fuller Advantage® 10-Speed automated manual transmission (AMT), delivering power when drivers need it most. Since the most efficient drivers can see about 30% better fuel performance than their peers, equipping drivers with precision powertrains can deliver immediate performance enhancements.
Spec to Your Duty Cycles
Choosing the correct powerhouses for your heavy-duty truck fleet is only the first step. Every Cummins diesel can be tuned and spec’d to meet the exact needs of every duty cycle and route in the fleet. Fleet managers no longer have to sacrifice power and performance for fuel economy – starting with Cummins PowerSpec™, your dealer or any Cummins Sales and Service Locations can tailor your Cummins diesel to meet any of your truck’s specific needs. Ask your dealer these questions to ensure that any truck rolls off the lot ready for duty.
Enable Uptime and Performance with Over-the-Air Programming (OTAP)
Cummins Connected Software Updates provides the required technology integration for vehicles to take advantage of our upcoming suite of new performance features, including over-the-air trim parameter calibration, designed for power and fuel optimization. Within a span of minutes versus hours, Connected Software Updates can update engine control modules using cellular or Wifi connectivity, which helps our customers stay running at peak performance.
Profily autorů
Cummins Inc., globální lídr v oblasti energetických technologií
Společnost Cummins Inc., globální lídr v oblasti energetiky, se zavázala pohánět prosperující svět. Od roku 1919 dodáváme inovativní řešení, která posouvají lidi, zboží a ekonomiky kupředu. Našich pět obchodních segmentů – Motory, Komponenty, Distribuce, Napájecí systémy a Accelera™ by Cummins – nabízí široké portfolio, včetně pokročilých dieselových, elektrických a hybridních pohonných jednotek; integrované systémy výroby energie; kritické součásti, jako je následné čištění výfukových plynů, turbodmychadla, palivové soustavy, ovládací prvky, převodovky, nápravy a brzdy; a technologie s nulovými emisemi, jako jsou bateriové a elektrické pohonné systémy. S globální působností, hlubokými technickými znalostmi a rozsáhlou servisní sítí dodáváme spolehlivá, špičková řešení šitá na míru potřebám našich zákazníků a podporujeme je během energetického přechodu prostřednictvím naší strategie Destination Zero. Vytváříme hodnotu pro zákazníky, investory a zaměstnance a posilujeme komunity prostřednictvím našich globálních priorit v oblasti společenské odpovědnosti: vzdělávání, rovnost a životní prostředí. Společnost Cummins se sídlem v Columbusu ve státě Indiana zaměstnává přibližně 67 400 lidí po celém světě a v roce 2025 vydělala 2,8 miliardy dolarů při tržbách 33,7 miliardy dolarů.
Související Tagy