Silnik 6.7 firmy Cummins dla pojazdów RAM do zastosowań komercyjnych
There's something to be said about confidence. Confidence gives you the feeling of security, support, and strength.
Autor: Cummins Inc., globalny lider technologii energetycznych
Wszyscy szukamy przewagi, która pozwala nam osiągać najlepsze wyniki, niezależnie od tego, czy jest to w pracy, czy podczas pracy. Dlaczego nie mieć silnika, który zapewni Ci dodatkową pewność w samochodzie ciężarowym?
6.7 litrowy Turbo Diesel Cummins przenosi pickupa 3500 I 45/5500 RAM oraz klientów komercyjnych na wyższy poziom wydajności.
WYDAJNOŚCI
An engine needs to provide the power and performance you need on and off the job. Cummins is committed to providing customers with an extra edge of confidence in performance while hauling, so you can work hard and play hard.
The Cummins 6.7L Turbo Diesel for Chassis cabs boasts 360 horsepower and 800 pound-feet of torque. The RAM 3500 / 4500 / 5500 Chassis Cabs with the Cummins 6.7L turbo Diesel are offered with an Aisin 6-Speed Auto Transmission. With the 3500 delivering a 25,890 lbs. of best-in-class towing capability Also available with the 45/5500 RAM Chassis Cab, with 800 pound-feet of best-in-class torque, delivering 35,220 lbs. of maximum towing capability.
HIGH RELIABILITY
From hauling your equipment on and off the job site, to Hauling your toy hauler on the weekend, you should have the highest level of reliability when it comes to hauling, towing, and payload. This legendary engine provides fuel efficiency and class-leading 12,000 thousand mile oil change intervals. To moc i niezawodność, na które zawsze możesz liczyć.
DURABILITY
As the only engine with its own high mileage club, there is no denying that at 100,000 you're just getting started with a Cummins powered RAM. Wear your engine's high mileage like a badge of honor. Become part of the Cummins legacy of longevity with an engine that will withstand what you need for your work, business, or personal needs. Sign up with your high mileage RAM today at highmileage.cummins.com
LEGACY
Cummins has been providing confidence for100 years. From pioneering new technology to first partnering with Ram in 1989 to haul two tons more than any competitor at the time. Cummins has been a leader in the diesel engine world since Clessie Cummins launched the company in Columbus, Indiana in 1919, with a commitment to producing the finest diesel engines on the planet. From humble beginnings grew an international enterprise that today provides products and service to customers in more than 150 countries. Nearly a century spent perfecting diesel engine performance provides Cummins unmatched insight and expertise. The Cummins 6.7L Turbo diesel in RAM HD Pickup and CC are manufactured in our plant in the same community where it all started. And Customers can expect the same reliability and dependability they have experienced since Cummins began powering Ram trucks in 1989.
Profile autorów
Cummins Inc., globalny lider technologii zasilania
Firma Cummins Inc., światowy lider w dziedzinie energetyki, jest zaangażowana w tworzenie bardziej zamożnego świata. Od 1919 roku dostarczamy innowacyjne rozwiązania, które napędzają ludzi, towary i gospodarki. Nasze pięć segmentów biznesowych – silniki, podzespoły, dystrybucja, systemy zasilania i Accelera™ by Cummins – oferuje szeroką ofertę, w tym zaawansowane silniki wysokoprężne, elektryczne i hybrydowe; zintegrowane systemy wytwarzania energii; elementy krytyczne, takie jak układ oczyszczania spalin, turbosprężarki, układy paliwowe, elementy sterujące, skrzynie biegów, osie i hamulce; oraz technologie bezemisyjne, takie jak akumulatory i elektryczne układy napędowe. Dzięki globalnemu zasięgowi, głębokiej wiedzy technicznej i rozległej sieci serwisowej dostarczamy niezawodne, najnowocześniejsze rozwiązania dostosowane do potrzeb naszych klientów, wspierając ich w transformacji energetycznej dzięki naszej strategii Destination Zero. Tworzymy wartość dla klientów, inwestorów i pracowników oraz wzmacniamy społeczności poprzez nasze globalne priorytety odpowiedzialności korporacyjnej: edukację, równość i środowisko. Firma Cummins z siedzibą w Columbus w stanie Indiana zatrudnia około 67 400 osób na całym świecie i zarobiła 2,8 mld USD przy 33,7 mld USD sprzedaży w 2025 r.
Powiązane tagi