¿Qué tan silencioso debería ser un generador para acampar?

Por Cummins Inc., líder mundial en tecnología de energía

una familia se reúne para una comida bajo su capota para RV

Aunque puede venir como un pensamiento de último momento, invertir en un generador silencioso-o comprar equipos de control de ruido de generador adicionales-en realidad es una necesidad cuando se viaja en un vehículo recreativo. Los generadores tienen una energía inmensa, por lo que el ruido es un efecto secundario natural de esa energía generada y utilizada. 

En este artículo, explicaremos cómo administrar el nivel de ruido de su generador. Interested in finding the quietest RV generator for camping? We’ll also list a few quiet RV generator options for you to consider. Let’s get started.


Why are some generators so loud?

With all generator models, electrical energy is directed through an engine which generates a lot of power-and a lot of noise to come along with it. It is important to investigate the noise level of a generator before you commit to any purchase .

Here are a few important things to consider when you’re assessing if a generator operates at an acceptable generator noise level. 

  • Size - The size of the generator impacts the amount of noise it produces. The larger the generator, the more noise it will make.
  • Built-in RV generator models - manufacturers measure the noise level of a generator before it is installed. Therefore, the generator will sound quieter than the stated decibel rating provided by the manufacturer. 
  • Portable Generators - People often ask, “Why is my portable generator so loud?” The answer is simple; portable generators sound louder than installed RV generators since they are housed outside your coach. 
  • Distance - Account for the distance at which quietness is measured when investigating a generator’s noise level. If you measure the noise level for the same RV generator at 5 feet vs.10 feet, the results will be different. Many manufacturers note the distance used when they produce their sound measurements in product brochures. At Cummins, we measure at 10 feet (3 meters) for maximum accuracy. 
  • Load Level - Consider the load level at which noise is measured. Generators make more noise when working at higher load levels. Make sure you check the generator’s product brochure to ensure you are comparing quietness at similar load levels. 
  • Angle - The angle you use when measuring noise should also be considered. Although most manufacturers don’t share this information on brochures, it’s still very important to check. At Cummins, we measure the noise levels at seven different angles all around the RV generator, then take the average of those measurements to determine the noise level of the generator.


Why does RV generator noise level matter?

Many campgrounds have generator noise level regulations. According to the National Park Service’s Soundscape Management Policy, “Operating motorized equipment or machinery that exceeds a noise level of 60 decibels measured on the A-weighted scale at 50 feet is considered to be unreasonable.” Breaking the noise level rules of a campground would be a sad reason to cancel a camping trip, wouldn’t it?

But don’t worry, there are quiet generator models available. 


¿Cuál es el generador más silencioso para acampar?

We are proud that our Onan RV generator models are the quietest options out there and they fall well under the National Park service’s noise restriction requirements. The recently released Onan RV QG 2800i and 2500i generator models are excellent options when it comes to noise reduction. These models are quiet, efficient, and easy to maintain. We offer many other ultra-quiet and efficient Onan generator and portable generator models, all of which are excellent for camping and other RV adventures.


Don’t let a noisy generator ruin your adventures—Explore Onan RV generators.

Perfiles de autor

Edificio de oficinas de Cummins

Cummins Inc., líder mundial en tecnología energética

Cummins Inc., líder mundial en energía, está comprometida a impulsar un mundo más próspero. Desde 1919, ofrecemos soluciones innovadoras que hacen avanzar a las personas, los bienes y las economías. Nuestros cinco segmentos comerciales (Motor, Componentes, Distribución, Sistemas de energía y Accelera™ de Cummins) ofrecen una amplia cartera que incluye trenes motrices diésel, eléctricos e híbridos avanzados; sistemas integrados de generación de energía; componentes críticos como postratamiento, turbocompresores, sistemas de combustible, controles, transmisiones, ejes y frenos; y tecnologías de cero emisiones como sistemas de batería y tren motriz eléctrico. Con una presencia global, una profunda experiencia técnica y una extensa red de servicio, ofrecemos soluciones confiables y de vanguardia adaptadas a las necesidades de nuestros clientes, apoyándolos durante la transición energética con nuestra estrategia Destino Cero. Creamos valor para clientes, inversionistas y empleados y fortalecemos comunidades a través de nuestras prioridades globales de responsabilidad corporativa: educación, equidad y medio ambiente. Con sede en Columbus, Indiana, Cummins emplea aproximadamente a 67,400 personas en todo el mundo y ganó $2.8 mil millones sobre $33.7 mil millones en ventas en 2025.

¿Desea obtener más información?

Reciba lo último de Cummins en tecnologías, productos, noticias y perspectivas.