Realty

Commercial

Safeguard your business from the increasing number and severity of costly power outages with Cummins. Cummins Gensets are available in range of sizes to meet your needs. Able to start and assume load in less than 10 seconds, and rated load in a single step, Cummins GenSets are the epitome of rugged dependability and reliable mechanical and electrical performance. 

Residential

Cummins is the brand homeowners & the builders trust for reliability, durability and power. With a Cummins home generator, your family won't be left in the dark.

 

Ratings: 125, 250, 320, 400, 500, 600, 625, 750, 810, 910, 1010, 1250, 1500, 2000, 2250

 

Features of Construction Site Generator

•    Must be durable and able to withstand rough weather conditions.
•    The large stationary ones are preferred since they tend to be the most powerful. You can, however, use portable generators if you are constantly moving from one area to another.
•    Most construction site generators come in either three-phase or single-phase configurations and produce a wide range of power.
•    Ensure you choose the genset with a long run time for faster and more efficient outputs.
•    The backup generators for construction come with enclosed outlets, which ensure that harsh weather conditions, such as rain and snow, won’t disrupt the functioning of the generator engine.
 

Frequently Asked Questions

1.    What types of generators are used in construction sites?

There are several types of generators used on construction sites as they need a reliable and robust source of energy to run heavy machinery in case of outages. the most common generators include standby generators, induction generators, portable generators, and inverter generators. Standby diesel generators are among the most popular types of generators used across construction and realty projects.

2.    How do I choose the best backup generator for construction sites?

If you are a construction contractor, you will need to power all your equipment and heavy machinery in rough and remote terrains where electricity is not readily available. Portable diesel generators are the best option for such cases. The size of a generator will vary for different types of worksites.