커민스, 르완다 최고의 스포츠 여행지 키갈리 아레나 백업

작성자: Adam Sidders, Power Systems 마케팅 커뮤니케이션 리더

커민스 터키 공인 유통업체인 Mepa Energy의 프로젝트 엔지니어인 Adem Ersoy는 키갈리 아레나의 대기 전력 시스템 옆에 서 있습니다.

Kigali Arena, the largest sports stadium in eastern Africa, is now open. Located just outside the Amahoro National Stadium in Remera, Rwanda, the 10,000-seat facility was inaugurated in August by Rwandan President Paul Kagame.

Kigali ArenaThe arena is scheduled to host the inaugural Basketball Africa League inaugural semi-finals and finals in March 2020, and expected to host the 2021 FIBA Men’s Africa Basketball Championship after it was announced earlier this year that Rwanda will host the tournament. In addition to sporting events like basketball, volleyball and martial arts, it will also be a centre for concerts, conferences and exhibitions. The complex sits on 28,000 square metres of land and includes 13 cafeterias and restaurants, six changing rooms, two coaching staff rooms , a fitness centre and a media hall.

Summa Company of Turkey built the arena in only six months. The standby power system consists of three units of Cummins C1100D5B 0.4 kV generator sets, which are synchronized and commissioned. The three Cummins C1100D5B generator sets proves this capability by being able to start and synchronize with each other and take the full load at about 8-12 seconds. Cummins Turkey Dealer Mepa Energy has engineered, installed and commissioned the power system with daily fuel tanks, automatic replenishing system and sound attenuators.

저자 프로필

아담 사이더스 마케팅 커뮤니케이션 리더 파워 시스템

Adam Sidders, Power Systems 마케팅 커뮤니케이션 리더

애덤 시더스(Adam Sidders)는 커민스 파워 시스템 사업부의 마케팅 커뮤니케이션 리더입니다. 2012년 커민스에 입사하기 전에는 유럽 최대의 독립 소유 보험사의 금융 서비스 부서에서 마케팅 및 커뮤니케이션 매니저로 근무했습니다. [이메일 보호]

더 자세히 알고 싶으신가요?

커민스의 기술, 제품, 뉴스, 인사이트에 대한 최신 정보를 받아보세요.