Tek Modüllü Son İşlem Sisteminin Geliştirilmesi

Küresel Güç Teknolojisi Lideri Cummins Inc. tarafından

cummins tek modüllü son işlem sistemi ken federle

Ken Federle, Cummins Emission Solutions'ın Araştırma ve Geliştirme İcra Direktörüdir. Yakın zamanda ağır hizmet kamyonları için yeni Single Module ürünü ve tasarımın nasıl geliştirildi hakkında soru sormak için ona yetiştik.

Interviewer: The Single Module is a revolutionary product. Bize konseptin nereden geldiğini biraz anlat.

Ken: We heard clearly from our customers that they wanted a smaller, lighter and more reliable aftertreatment system.  From the beginning, the focus of the Single Module was to address those voices from the customer.

Interviewer: How important was it for Cummins Emission Solutions to achieve such an incredible size reduction in this next-generation system?

Ken: We had a goal to reduce the size by at least half so that all of the components could fit into the size of one of the elements of the switchback system we have today. We weren’t sure we would be able to achieve this, but in the end we exceeded our goal and accomplished a reduction of 60 percent.

Interviewer: What features of the Single Module contribute to the improved efficiency?

Ken: There are many features that play some role, all the way from the inlet to the outlet and everything in between.  The catalysts, urea mixing system and urea dosing system work in combination with one another, which leads to a more efficient system.

Interviewer: How does the Single Module differ from aftertreatment technologies of today?

Ken: Virtually all aftertreatment systems require the exhaust to travel in many directions within the system, like the switchback design.  The straight flow-through system has no change in direction, simplifying the air-flow and offering improved efficiency.

Interviewer: What about the Single Module stands out among other industry aftertreatment solutions?

Ken: The Single Module is the first second-generation aftertreatment system that has been brought to market and is a major step forward in diesel aftertreatment systems.

Interviewer: How do today’s stringent requirements on emissions play a role in Cummins Emission Solutions’ approach to designing a new product?

Ken: With advances in catalysts, we’ve achieved over a 99 percent reduction of particulate matter and a 96 percent conversion of NOx, which allows the engine to be optimized for economy and performance rather than for emissions reduction.

Interviewer: What do you want our customers to know about this product?

Ken: This product has been in development for over five years and has been well tested and validated to ensure customers have a great experience at production launch in 2017.

Interviewer: What’s next on the horizon for Cummins Emission Solutions?

Ken: One of our guiding principles is innovation, and Cummins Emission Solutions is continuously working on new innovations that we will bring into US markets and markets around the world. There are still many additional improvements that can be made to aftertreatment solutions.

Learn More About Cummins Aftertreatment Systems

Yazar Profilleri

Cummins Ofis Binası

Cummins Inc., Küresel Güç Teknolojisi Lideri

Küresel bir güç lideri olan Cummins Inc., daha müreffeh bir dünyaya güç vermeye kararlıdır. 1919 yılından bu yana, insanları, malları ve ekonomileri ileriye taşıyacak yenilikçi çözümler sunuyoruz. Cummins'in beş iş segmenti olan Motor, Bileşenler, Dağıtım, Güç Sistemleri ve Accelera™, gelişmiş dizel, elektrikli ve hibrit aktarma sistemleri dahil olmak üzere geniş bir portföy sunar; entegre güç üretim sistemleri; son işlem, turboşarjlar, yakıt sistemleri, kontroller, şanzımanlar, akslar ve frenler gibi kritik bileşenler; ve akü ve elektrikli aktarma sistemi sistemleri gibi sıfır emisyonlu teknolojiler. Küresel ayak izi, derin teknik uzmanlık ve kapsamlı bir servis ağı ile, Hedef Sıfır stratejimizle enerji geçişi boyunca onları destekleyerek müşterilerimizin ihtiyaçlarına göre uyarlanmış güvenilir, en son çözümler sunuyoruz. Müşteriler, yatırımcılar ve çalışanlar için değer yaratıyoruz ve kurumsal sorumluluk küresel önceliklerimiz aracılığıyla toplulukları güçlendiriyoruz: eğitim, eşitlik ve çevre. Merkezi Columbus, Indiana'da bulunan Cummins, dünya çapında yaklaşık 67.400 kişiyi istihdam ediyor ve 2025 yılında 33.7 milyar dolarlık satışla 2.8 milyar $ kazandı.

Daha fazla bilgi edinmek ister misiniz?

Teknolojiler, ürünler, haberler ve içgörüler alanında Cummins'ten en son bilgileri alın.