Le F/V Sea Hound : donner vie à l'effort et au plaisir.

A commercial fishing boat brings prosperity and comradery to the New England fishing community. 

Par Katie Yoder, spécialiste en communication marketing.

FV Sea Hound

Le week-end, Chris Devine échange sa blouse de pharmacien contre son équipement de pêche par mauvais temps pour passer du temps sur le F/V Sea Hound - son homardier bien-aimé de 37 pieds. Selon Chris et son partenaire, Troy Collins, chaque moment passé au large des côtes de la Nouvelle-Angleterre est un temps bien investi. The pair carry over 800 traps to sea each weekend with intentions to only return once their boat is overflowing with the day's catch. 

As soon as they were old enough, childhood friends Chris and Troy began working on charter fishing boats along the New Hampshire (USA) coast. Once in college, Chris also started lobstering over the summers to pay for his education. Little did he know that his side gig would cultivate a new passion and become a life-long hobby. 

Chris bought his first boat at the age of 18 and has had two others since then. He started with only 100 traps on his 27-foot skip boat and has now worked his way up to his current vessel, the F/V Sea Hound.

F/V Sea hound

Purchased in northern Maine, only minutes from the Canadian border, the F/V Sea Hound required some major work before it could hit the water. Chris and Troy trucked the boat down to their hometown of Hampton, New Hampshire (USA) where it lived in the shipyard for eight months. 

The duo had the original Cummins B-series engine rebuilt, then two years ago upgraded to a remanufactured Cummins C-Series 8.3L engine. Reflecting on his experience with Casco Bay Diesel, a Cummins dealer, Chris says, "Honestly, the reliability of the product and the ease of work and connection is amazing. Everyone is a phone call away and so willing to help."

While they love their weekends lobster fishing, the F/V Sea Hound gets plenty of use for other fun excursions. Devine and his wife Haley will use the boat for offshore fishing tournaments, date nights on the coast, snorkeling, sunset cruises and so much more. 

Haley mentions the comradery that the vessel brings for their friendships and fishing community. "The boat has brought a lot of our friends closer together, they enjoy helping out, fixing things and building things. It has truly created a family, and everybody loves it."

She says, "The lobster community can be so cut throat, but at the same time these guys have such a bond. They will give you anything and everything they can to ensure your boat is up and running. Everyone will be there to help."

F/V Sea HoundJoking about all the love for the F/V Sea Hound, Haley says, "I like to refer to the boat as the dirty mistress. But as much as I make fun of it, it has been an awesome experience and we are truly lucky to own a boat and be a part of the fishing community."

The F/V Sea Hound is absolutely adored by her owners, deckhands, family and community. It brings so much joy, not only in the form of weekends lobster fishing but also with leisurely activities on the water and the wholesome environment it provides.

For mariner families like Chris, Haley and Troy, there really is no better place to be than the open water.

Want to see and learn more about the F/V Sea Hound? Check out their Instagram page

Looking for information about Cummins Marine? Visit cummins.com/marine

Profils d'auteurs

Katie Yoder - Cummins Inc.

Katie Yoder, spécialiste en communication marketing.

Katie Yoder est spécialiste en communication marketing. Elle a rejoint Cummins en 2018 en tant que membre de l’équipe des opérations des salons professionnels, mais soutient désormais les initiatives de marketing des segments Marine et pétrole et gaz. En tant qu'ancienne élève de l'Université du Wisconsin, Katie consacre son temps libre à regarder les sports des Badgers.

Vous voulez en savoir plus ?

Recevez les dernières nouveautés de Cummins en matière de technologies, de produits, de nouvelles et d’informations.