Chaque équipe a besoin d'un soutien fiable.
Lorsque le quart-arrière titulaire d’une équipe se blesse tôt dans la saison, la panique se propage parmi les supporters de l’équipe. Les propriétaires et les entraîneurs restent confiants, car ils savent qu'ils disposent d'un remplaçant fiable. Fast-forward to the end of the season, and that backup quarterback may even lead your favorite team all the way to The Big Game. It just goes to show, you can't underestimate the value of a great backup plan.
Par Cummins Inc., leader mondial des technologies d'énergie
C’est la même chose avec l'Alimentation. C’est pourquoi les stades du monde entier, y compris l’US Bank Stadium où se jouera le Big Game le 4 février et le 2018, comptent sur l’alimentation de secours de Cummins pour maintenir l’alimentation allumée pour les milliers de fans et de joueurs dans le stade.
Cummins offers reliable power for your home’s backup plan too, with home standby generators to ensure that when the power goes out, your lights, refrigerator or even your Ultra HD 4K television set (you know, the one you’re watching The Big Game on) stay on.
Last year, millions of homeowners in the United States lost power due to devastating hurricanes, heat waves, blizzards and an aging power grid. Hurricane Irma alone caused more than 7.8 million customers to lose power in the southeast - 6 million in Florida, 1.3 million in Georgia and 200,000 in South Carolina.
Cummins home generators automatically provide your family power when severe weather strikes or an over-loaded power grid fails. Unlike portable generators, there’s no gas to fill or cords to pull. Your Cummins home standby generator is permanently installed, turns on in seconds and keeps running until utility power is fully restored, so you won’t miss that last-second field goal during The Big Game.
In the meantime, here are a few tips to ensure your ‘big game’ isn’t interrupted should a power outage occur:
- Make sure electronic devices are fully charged. So, in the event of a power outage during The Big Game, you can continue watching it on your mobile device.
- Have flashlights on hand, so if the lights do go out you can still find your way to the buffalo wings and nachos!
- Of course you and your family could go to The Big Game at the US Bank Stadium. However, for a similar investment you could install a home standby generator and have back-up power for years to come.
And it just so happens, we know a thing or two about generators and how to have a game plan when your lights go out.
Cummins QuietConnect series generators, manufactured in Minnesota, feature patented neighbor-friendly sound technology, coupled with advanced housings, making them some of the quietest generators available. Compact design allows for installation as close as 18 inches from your home, making them comparable to air conditioning units in size and curb appeal. The use of natural gas or propane allows for more power with less fuel and lower emissions compared to portable generators.
To learn more about Cummins home standby generators, contact a Cummins-authorized dealer today to schedule a free in-home assessment.
Profils d'auteurs
Cummins Inc., leader mondial des technologies de l'énergie
Cummins Inc., un leader mondial de l'énergie, s'engage à fournir une énergie pour un monde plus prospère. Depuis le 1919, nous avons livré des solutions novatrices qui font progresser les personnes, les biens et les économies. Nos cinq segments d’activité — moteurs, composants, distribution, systèmes d'énergie et Accelera™ par Cummins — offrent un large portefeuille, incluant des motorisations avancées diesel, électriques et hybrides ; des systèmes de génération de réseau électrique unifié ; des composants critiques tels que le post traitement, les turbocompresseurs, les systèmes d'alimentation en carburant, les commandes, les transmissions, les essieux et les freins ; et des technologies zéro émission comme les batteries et les systèmes de groupe motopropulseur électrique. Grâce à notre présence mondiale, à notre expertise technique approfondie et à notre vaste réseau de services, nous fournissons des solutions fiables et de pointe adaptées aux besoins de nos clients, en les soutenant tout au long de la transition énergétique grâce à notre stratégie Destination Zero. Nous créons de la valeur pour les clients, les investisseurs et les employés, et nous renforçons les communautés grâce à nos priorités mondiales en matière de responsabilité sociale : l’éducation, l’équité et l’environnement. Basée à Columbus, dans l'Indiana, Cummins emploie environ 67 400 personnes dans le monde entier et a réalisé un chiffre d'affaires de 2,8 milliards de dollars en 33, dont 7,2025 milliards de dollars de bénéfices.