Cummins isporučuje gorivne ćelije za kamione za otpad u Evropi

Cummins Inc., globalni lider u tehnologiji pogona

kamion za smeće na gorivne ćelije

Đubrenje nije tema o koju mnogi od nas redovno razmišljaju. Otpad kao industrija, kada se obavi ispravno, postaje malo obožavalaca. Međutim, snaga i izdržljivost kamiona za otpad su okosnica prikupljanja i transporta otpada. Though waste may not always make prime time news, the technologies that help with waste management have made great strides, and now Cummins is pushing it even further by providing fuel cells for some of the first licensed and commercially operational fuel cell refuse trucks in Europe. 

FAUN illustration
Slika ljubazno od FAUN-a

In partnership with leading European truck manufacturers, system integrators, waste management fleet operators and hydrogen infrastructure providers, Cummins is aiding in the development of fuel cell electric heavy-duty refuse trucks for the European market. To date, Cummins has provided more than 20 fuel cell power modules, often referred to as fuel cell "engines," to a range of truck builders across Europe.  

Cummins recently supplied fuel cells for FAUN, a leader in waste collection vehicles and sweepers in Europe, for their electric refuse truck program. Each truck has 100% electric drive and is 100% emissions free with a range of up to 560 km, which is enough to run the collection route multiple times carrying 10 tons of waste.  

Fuel cell refuse truck
Slika ljubazno od FAUN-a

In addition to the electric motor and batteries, fuel cells are used to extend the range of the truck. Each truck contains three fuel cells - the number is determined by route requirements - with an output of up to 30kW per cell. Each truck has up to six hydrogen tanks, each with a capacity of four kilograms of hydrogen. The total weight of each vehicle is equal to that of a refuse truck equipped with a conventional engine, meaning payload is the same. These trucks will soon be on the road in multiple towns across Germany.   

Providing zero-emissions and noise reduction are some of the benefits of fuel cell technologies, benefits that are vital when operating in densely populated urban areas with strict emissions regulations. Proving technology viability means refuse trucks act as a persuasive first mover for other government vehicles, like buses and applications where current battery technology is not able to handle all requirements for heavier vehicles and longer ranges. As a result, in early spring, Cummins joined 43 other companies and pledged their support for the 'Joint call for the deployment of hydrogen fuel cell trucks' in Europe.  

With the help of Cummins technology waste just got a little bit cleaner.  

With more than 2,000 fuel cell systems in operation already, we’re excited to see what’s next! 

Profili autora

Poslovna zgrada kompanije Cummins

Cummins Inc., globalni lider u tehnologiji napajanja

Cummins Inc., globalni lider pogona, posvećen je pokretanju prosperitetnijeg sveta. Od 1919. godine isporučujemo inovativna rešenja koja pomeraju ljude, robu i ekonomije napred. Naših pet poslovnih segmenata-motora, komponenti, distribucije, sistema za napajanje i Accelera™ kompanije Cummins nudi širok portfelj, uključujući napredne dizel, električne i hibridne pogonske sklopove; integrisani sistemi za proizvodnju električne energije; ključne komponente kao što su sistem za prečišćavanje izduvnih gasova, turbopunjači, sistemi za gorivo, kontrole, menjači, osovine i kočnice; i tehnologije sa nultom emisijom kao što su baterije i električni pogonski sistemi. Uz globalni uticaj, duboku tehničku stručnost i opsežnu servisnu mrežu, isporučujemo pouzdana, najsavremena rešenja prilagođena potrebama naših kupaca, pružajući im podršku kroz energetsku tranziciju sa našom strategijom Destination Zero. Stvaramo vrednost za kupce, investitore i zaposlene i jačamo zajednice kroz naše globalne prioritete korporativne odgovornosti: obrazovanje, jednakost i životnu sredinu. Sa sedištem u Kolambusu u državi Indijana, Cummins zapošljava približno 67.400 ljudi širom sveta i zaradio je 2.8 milijardi dolara na prodaji od 33,7 milijardi dolara u 2025.

Želite da saznate više?

Primajte najnovije vesti od kompanije Cummins o tehnologijama, proizvodima, vestima i novim iskoracima.