Prekidači za flašu za pića za Cummins radi rezervnog napajanja

Anisha George , specijalista za marketinške komunikacije

Uključena 1974. godine, Sukkur Pića su bila glavni uvod u gazirana bezalkoholna pića u unutrašnjem regionu Sindh i graniči se sa južnim regionom Punjab, Pakistan. To je prvobitno bila fabrika koka-kole, a zatim je predstavila Pepsi 1980-tih. 

While the manufacturer has a standby power system in place, it was looking for a new supplier to partner with that could provide more dedicated support and stronger capabilities. Cummins local distributor Orient Energy Systems demonstrated these assets to Sukkur Beverages, switching their preference to specify a Cummins.  "The customer was looking for an OEM product with better aftersales support and engineering expertise available within the country," said Muzaffar Iqbal, Sales & Marketing - GO for OES. In the event of a utility failure, operations can continue seamlessly with dependable backup power in the form of a Cummins Power Generation C550D5e emissionized generator set. This provides 500 kVA of standby power to the 170,000-square-foot plant and offices.

The project was a success due to the demonstrably high standard of the technical deployment. OES performed installation and local synchronization with the existing 2 x 1250 kVA generators through a control system. The system was successfully integrated and commissioned, and is perfectly running. As OES and Cummins enter into the beverage industry of interior Sindh, this presents an opportunity to demonstrate the superior product and aftersales support to other specifiers seeking the right partner.
 

Profili autora

Anisha George, specijalista za marketinške komunikacije

Kao specijalista za marketinške komunikacije, Anisha podržava marketing, komunikacije i upravljanje događajima za regione Afrike i Bliskog Istoka. Pre nego što se pridružila Cumminsu 2011. godine, stekla je industrijsko iskustvo radeći na polju upravljanja događajima. [zaštićeno e-poštom] 

Želite da saznate više?

Primajte najnovije vesti od kompanije Cummins o tehnologijama, proizvodima, vestima i novim iskoracima.