Adam Sidders Marketing Communications Leader Power Systems

Adam Sidders

Marketing Communications Leader, Power Systems

Adam Sidders is the Marketing Communications Leader for the Power Systems Business Unit of Cummins Inc. Prior to joining Cummins in 2012 Adam worked in Financial Services for Europe’s largest independently owned insurer as their Marketing and Communications Manager. [email protected]

43 Articles

Not only that, the Niger International Airport represents a major gateway into the country, expanding Niger’s global connection by servicing both domestic and international routes from its capital, Niamey.

Generator paralleling is a complex topic that has changed drastically from the operator in the early 1970s to today's autonomous microprocessor-based technology.

NFPA 110 defines “Type” as the maximum time, in seconds, that the emergency power supply system will permit the load terminals of the transfer switch to be without acceptable power Type 10, therefore, has a 10-second time to readiness: meaning that a source of electrical power of required capacity, reliability, and ...

The sensitivity of loads to the power quality is often of extreme importance and plays a major role in purchasing decisions.

In Milan, the new 50-story Allianz Tower required cutting-edge design along with protection against power grid blackouts.

Cummins Turkey’s authorized dealer Mepa Energy attended the fair for the first time to meet with new customers and showcase Cummins technology at one of the largest international forums for the manufacturing industry.

Consulting and specifying engineers can earn continuing education credits (PDH/CEU) and keep up on critical technology updates, the latest codes and industry applications.

Cummins has been a longtime member of EGSA, and six Cummins staff recently joined over 400 attendees representing generator manufacturers, fuel tank manufacturers, accessory manufacturers, engine suppliers, logistics organizations and engineering firms at the EGSA 2019 Spring Conference.

Cummins Turkey provided two Cummins C2250 D5 generator sets for the first and second phases of Vodafone’s office remodel project in Ankara, providing 4,500 kVA of standby power to meet additional power requirements of the building project.

With a power density of up to 2.0 MW from a 78L engine, which will be displayed on stand, the HSK78G series offers reliable power no matter how extreme the fuel source or operating conditions.

As part of a $1.2 billion capital investment programme to reduce emissions and drive energy independence, Fingrid required power for a black start application that could fit a highly complex sequence of operations for their reserve Power Plant in Forssa – a city uniquely situated in the center of the three largest majo...

A 2,500 kVA power system from Cummins is a reliable emergency source of power for a boron mine facility in Turkey’s northwestern region.