Cummins Case Studies
We’re in it for the long haul. We build lasting partnerships that lead to smarter innovations for our customers. These customer stories demonstrate our commitment and success in providing customers like you with improved power solutions through world-class innovation in a number of industries.
Liveaboard, Spanish-inspired llaut loaded with style, creature comforts Wrapped in luxury amid the waves gently lapping the hull of the Menorquin 68 is a sensual experience at sea. Three lovely staterooms with four berths encourage sleeping in just a little bit longer. Upon awakening, stepping up the companionway into the well-appointed salon's open entryway brings the sunlight in with the sea
“The whisper-quiet genset, proven reliability, ease of maintenance and longevity are prime reasons why Nordhavn’s long range vessels are built standard with Onan marine generators.” - Jim Leishman, Vice President & Co-owner, Nordhavn Yachts Nordhavn 41 fuel-miser boasts a small carbon footprint The Nordhavn 40 set the world record for a production boat under 70 feet, circumnaviga
Modutech Marine, of Tacoma, Washington, has gained recognition on meeting the stringent conditions of military contracts. In 2020 they completed a contract to build a fleet of five small tugs. These carry the military designation Work Boat Docking. Compact and highly versatile Modutech’s Brian Swindahl describes the vessels, “The mission of the CNIC Work Boat Docking (WB Docking) i
“We can confidently say that this project will be a real revolution in the towage operations and a great milestone for our green tug solutions." - Noyan Altuğ, CEO of UZMAR The concept of ‘hybrid tug’ is getting a whole new definition with an innovative new tug under construction at Turkey’s Uzmar Shipyard for the Danish Port of Aarhus. From the outside it looks very similar to other Robert
“Loaded with creature comforts, the audio in an Azimut is like a night club with an amazing sound system.” - Peter Kurki, Sales Executive, Allied Marine Semi-displacement hull for smooth sailing in Azimut style Azimut, the world’s leading builder of seductive, fast-planing flybridge yachts, now builds vessels for long-range cruising. The 43 navetta-style yacht is the fourth m
As progressive nations worldwide commit to reducing greenhouse gases, a fishing vessel is built to do its share with Cummins marine propulsion. Designed by Norway’s Skipsteknisk and Selvåg AS, the Selvåg Senior is under construction at Cemre Shipyard for Sorheim Holding and is truly a remarkable concept. Capable of both trawling and purse seining, the 79.5 by 16.2-meter vessel with have a molde
Voyage confidently in the Fleming 55, the ultimate passagemaker Open oceans. Icy fjords. Inland rivers. Tropical seas. Aleutian Islands. Florida Straits. Designed for serious cruising in every condition, the Fleming 55 is a raised pilothouse motoryacht for a capable owner-operator voyaging the world in confidence and comfort. The Fleming low profile provides stability and comfort at se
“The QSB6.7's are tried, true and exceptionally reliable. There is extra strain on a high-speed vessel... That’s why we use Cummins. Their marination is simply better.” - Nick Williams of SMJB Thrills and water adventures Smoking hot! Powered by twin 350HP Cummins QSB6.7’s with 274 Hamilton Jets, this Subchapter-T passenger vessel for Miami WaterSports is built to fly, spinning exc
Custom built for offshore tournaments With large cockpits and custom configurations, Henriques Yachts produces canyon-capable fishing machines with the muscle and seakeeping capability of a real, rough-water boat. Capable of venturing out safely in the chop over 100 miles to reel in a big trophy tournament fish, the strong and solid Henriques hull is strategically designed to endure ha
DEME and Royal I HC split-hopper vessels offer modern functionality with Cummins marine propulsion. DEME partners with Royal I HC As ships grow larger with increased draft and harbors continue to silt, the demand for modern dredges continues to grow. The acknowledged masters of the design and operation of these are the lowland countries, the Netherlands and Belgium. It came as no surprise wh
A new standard of comfort, aesthetics, and performance is set with Cummins marine propulsion. Carefully crafted for the client’s every need When word spreads of a good design well-executed, the reward for the boat builder is a customer who says, “Make me one just like that other one.” That is where the discussion starts, and then come the clients’ requests for modifications. Such was
The converted VLCC Ariake will offer substantial oil storage with Cummins marine propulsion. FPSOs are big, expensive pieces of equipment As the search for oil has moved into deeper waters with more distance to shore-based facilities, Floating Production Storage and Offloading vessels have become essential tools in the process. Typically, the large FPSO is stationary with a number of wells f
Overview Challenge: Provide power for a remote marina with load demands varying between 5 and 500kW while impacting year-round operating costs to increase maximum efficiency and allow the system to run completely on renewable energy when the system is not at peak capacity. Solution: An integrated microgrid power system using Cummins Power
Overview Challenge: Provide power system technologies for a completely off-grid microgrid solution in a remote location but at a commercial scale. Solution: An integrated renewable power system with two of Cummins 72 kW diesel generator sets. Result: A fully integrated remote microgrid energy solution that has been in oper
This US Army tug offers versatile utility with Cummins marine propulsion. Built for an important task Modern-day naval architects are accustomed to accommodating a number of design parameters. Tullio Celano, of Crescere Marine, recently took on an unusual set of design specs for a new tug. The US Army Corps of Engineers wanted a little 26-foot tug to handle the bulkhead stoplog at the Little
Welcome aboard SeaVee Boats’ new flagship 450z center console. Offering a combination of luxury and style, the 450z offers is a solid fishing machine that’s easy to maneuver with offshore performance bolstered by Cummins marine auxiliary. Designed with a sensible, safe deck arrangement, the 450z is equipped with all around zail fishing rods and four live wells to reel in a big tournament catch.
Danish wind farm support vessels, MHO Exbjerg and MHO Gurli, combine form and function with four Cummins marine propulsion engines. Wind farm support vessels MHO Exbjerg and MHO Gurli Form and function are the hallmarks of good design, but seldom have they been melded more effectively than with the Danish MHO-Co’ wind farm support vessels MHO Exbjerg and MHO Gurli. These 39 by 10.3-meter Inc
The new Sunreef 60 power catamaran offers comfort and seaworthiness with cummins marine propulsion. The new Sunreef 60 motoryacht combines elegance and power As the entry level boat in Sunreef’s catamaran series, the 60 is a versatile, power motoryacht offering comfort and seaworthiness in a flexible deck arrangement. Contemporary and sporty, the 60 Power Cat is easily maneuverable,