Cummins Case Studies

We’re in it for the long haul. We build lasting partnerships that lead to smarter innovations for our customers. These customer stories demonstrate our commitment and success in providing customers like you with improved power solutions through world-class innovation in a number of industries.

Filter Case Studies

Challenge:  Provide sustainable power capabilities for Myanmar to reach 100% electrification by 2030. Solution: A fully integrated off-grid solution in remote Kyaw, Myanmar with eight HSK78G natural gas generator sets supported by Cummins Power Generation from conceptualization to commissioning. Result: Energy efficient and cost-e

“Builders choose Onan generators because of the ease of using Onan, and it is backed by Cummins, so the supply chain should be better, too." Fishermen appreciate quiet Onan gensets Custom-built pleasure crafts represent the ultimate vessel in luxury design, naval architecture and craftsmanship. As the epitome and vision of a discriminating, private yacht owner, one-off dreamboats demand pr

"I’m a big believer in Cummins products, and I’ve never had a problem getting Cummins parts." — Capt. Norm Bekoff Do the math: Counting on Cummins cuts fuel costs in half! Several variables impact the success of a commercial fisherman with a charter operation. There’s the unpredictable weather, identifying a hot fishing spot and getting potential customers to choose your boat – it’s a com

License to Thrill Always moments away from leaping aboard a classy powerboat and then driving it like he stole it, the fictional James Bond would gravitate to the Technohull Omega 47 for his next dramatic, implausibly long, high-speed boat chase from some nefarious villain headquartered in a remote island compound. The Technohull Omega 47 luxury RIB is a Bond-inspired, high-performance speed

Challenge:  Digea required standby power for more than 45 digital television broadcast sites around the country, which was essential to keep the sheltered equipment running, and transmissions on-air, in the event of a grid failure. Solution: Cummins distributor Ergotrak supplied back-up systems for the 45 plus sites, deploying three types of Cummins g

"The Cummins KTA19s provide the perfect amount of power to do our job." — Brennan Templet, mate and pilot of Richard B Scream all you want in the swamp, no one will ever hear you - or help you. Down on the bayou, autonomy and self-preservation is key, because in a remote area, you’re on your own, in the elements. Having an engine like the Cummins KTA19 with torque, power and maneuverabi

Challenge:  To install a reliable critical protection power system for Digital Realty to meet stringent Tier 3 certification requirements, as defined by Uptime Institute. Solution: Cummins Power Generation delivered six roof mounted C2250D5 diesel generator sets powered by QSK60-G4 engines, together with custom-built acoustic enclosures and fuel syste

Challenge:  To install a reliable standby power system for the LG CNS Busan Global Data Center, ensuring service continuity and preventing data loss in the event of a power failure. Solution: Cummins delivered a comprehensive power system comprising 12 units of C2250D6A diesel generator sets to provide a total of 27MW of standby power. Res

Challenge:  Cummins was entrusted to supply the Twin Arrows Navajo Casino Resort in a rural location with emergency standby power. The critical need for standby as a gaming operation is so the resort wouldn’t lose power to the gaming floor or the gaming slot systems to maintain play on the floor. Cummins Power Generation was selected to supply diesel generators for critic

Challenge:  Design a backup power system tailored to meet NEXTDC’s criticality level requirements and install it in an unconventional environment, but also meet the customer’s rapid time to market demand without comprising the integrity of the work and equipment. Solution: 5.4 MW of standby power comprising of three C2250 QSK60 Generator Sets of CPG g

Challenge:  To reduce reliance on National Grid by upgrading the university’s 32 years old cogeneration solution. Using technology that complies with environmental regulations and can run continuously on a 24/7 basis, while being able to fit into a limited allocated space. Solution: A new cogeneration solution with Cummins C2000N6C, QSV91G singe turbo

Cummins power solution for KBC Bank   Challenge:  KBC Bank and its Hungarian subsidiary K&H selected Cummins for standby power at two of the bank’s mirrored data center sites in Hungary. Solution: Each of the mirrored sites were equipped with two C3000 D5 generator sets per site, both with QSK78 engines and PCC 3.3 controls.

Cummins Data Center Continuous Solution is Top Choice for Turkcell   Challenge:  To become the main provider of continuous power to Turkcell’s Datacenter. Solution: Cummins installed ten C1675 D5A generator sets plus two C1100 D5B units and a single C700 D5 in the basement of a three-story building.  Cummins also won a contract to supp

Challenge:  CalBank, one of Ghana’s leading banks, needed a standby power solution for its Head Office in Accra. Cummins Ghana were tasked with providing a standby power system that the head office buildings, including a banking hall and data center, could rely on to provide uninterrupted, efficient service and solutions to its customers, even during power outages.

"Up here, near Cape Cod, there’s a lot of support [from Cummins]. The Dunham dealership is open all the time. I also have Cummins X15’s in all my work and pickup trucks for my excavation company." — Capt. Anthony Belculfine  Smart diesel QSC8.3 600 gets out in front of the fleet The shocking combination of horsepower with efficiency is just one benefit of finding the perfect boat and

Overview Challenge: Provide power systems technologies for a completely off-grid microgrid solution that has the capacity to provide continuous reliable power in high ambient conditions, for a gold mining company.  Solution: A hybrid renewable energy solution with nine C2000N5CB QSV91G gas generator sets, two C2250D5 QSK60 diesel generator

What: Four 1250 kW at 13.8kV AC generator sets with on-board autonomous microprocessor-based PowerCommand® Control for paralleling and protection. The PowerCommand® DMC 8000 which is a state-of-the-art system level control. Arc-Resistance switchgear rated at 15kV, and the PowerCommand Cloud™ for real-time monitoring. The system runs in an extended parallel operation with the utilit