Cummins Case Studies
We're in it for the long haul. We build lasting partnerships that lead to smarter innovations for our customers. These customer stories demonstrate our commitment and success in providing customers like you with improved power solutions through world-class innovation in a number of industries.
Purpose: To install a standby power system for a remote lodge and associated water-treatment facility
PrevenTech’s proactive failure detection leads to significant cost savings and preserved uptime
Purpose: To supply dependable emergency power for a leading-edge supercomputer facility
Purpose: To install robust backup systems at a range of BAPCO fuel retail sites
PrevenTech’s predictive analytics detected early signs of injector wear to help prevent injector failures.
PrevenTech’s advanced analytics helped identify root causes of slow speeds and recommended optimized maintenance actions.
PrevenTech used to extend oil and filter life while ensuring engine health.
Purpose: To deliver a new backup system for phase 1 of a major new financial data center
Purpose: To deliver Phase 1 of a standby power system for East Africa’s first hyperscale data center
Purpose: To develop and ensure the efficient operation of multiple hyperscale data centers, enhancing Saudi Arabia’s digital infrastructure.
Kyle Myrick is a proud owner of a 2015 Cummins Turbo Diesel-powered Ram Tradesman pickup truck, with over 300,000 miles on the odometer. As a mining engineer with over 20 years of experience, his truck is continuously put to the test in harsh environments-not only as part of Kyle's work but also in support of his passion for travel and adventure.
Purpose: Upgrade a 20-year-old legacy DMC to enhance the power system capacity and reliability for a major network and communication service provider in Saudi Arabia.
STAMFORD P7 alternators play a critical role in powering the Ambatovy Project, a landmark mining and processing development in Madagascar.
Cloud boom behind Naver's supremacy push With soaring traffic on its platform, Naver embarked on the project to construct one of Asia's largest data centers which will be developed over six phases using a substantial volume of generator sets. The first phase of the Gak Sejong data center features 18 Cummins QSK95 gensets with a 60 Hz standby rating of 37