Cummins Case Studies
We're in it for the long haul. We build lasting partnerships that lead to smarter innovations for our customers. These customer stories demonstrate our commitment and success in providing customers like you with improved power solutions through world-class innovation in a number of industries.
Overview Where: Johannesburg, South Africa Purpose: To reduce carbon emissions and take a significant step towards Cummins 2030 Environmental Social and Governance (ESG) goals Supply: PowerCommand Microgrid Control® MGC900, 700 AC kWp of Solar power, Two KTA 38G5 Diesel Generators Cummins South Africa installs Microgrid System in Power Hub Headquarters Cummins is act
Overview Challenge: Provide power systems technologies for a completely off-grid microgrid solution that has the capacity to provide continuous reliable power in high ambient conditions, for a gold mining company. Solution: A hybrid renewable energy solution with nine C2000N5CB QSV91G gas generator sets, two C2250D5 QSK60 diesel generator
Overview Challenge: Provide power for a remote marina with load demands varying between 5 and 500kW while impacting year-round operating costs to increase maximum efficiency and allow the system to run completely on renewable energy when the system is not at peak capacity. Solution: An integrated microgrid power system using Cummins Power
Overview Challenge: Provide power system technologies for a completely off-grid microgrid solution in a remote location but at a commercial scale. Solution: An integrated renewable power system with two of Cummins 72 kW diesel generator sets. Result: A fully integrated remote microgrid energy solution that has been in oper