CENTINEL
Available as an aftermarket kit for K Series engines or installed as a factory option on Quantum Series MCRS engines, CENTINEL eliminates or extends oil change intervals by burning used oil and replacing it with clean oil.
The CENTINEL Advanced Engine Oil Management System automates oil changes. While the equipment is running, CENTINEL monitors the engine's duty cycle. At precise intervals, it bleeds off a small amount of used oil and sends it to the fuel tank, where it blends with diesel fuel and is burned during combustion.
CENTINEL allows equipment to work up to 4,000 hours between service events. Depending on the duty cycle, that could eliminate 15-20 oil changes from current maintenance schedules.
- Reduces downtime and the cost of oil change service
- Reduces the risk of engine damage due to poor oil change maintenance practice