Model F powers first diesel excavator

1926

Model F powers first diesel excavator

As diesel becomes an alternative to steam, Northwest Engineering begins using a 4-cylinder Cummins Model F engine in its power shovel excavator. This is the first use of a Cummins engine for excavation, initiating a history of innovation for harsh environments.

Model U begins production

1928

Model U begins production

Applying lessons learned from the power shovel, Cummins introduces what may be the world's first wholly enclosed diesel engine. The Model U features vertical valves and a more dependable fuel pump, making it more suitable for dusty and dirty conditions.

Launch of the Model K

1929

Launch of the Model K

Cummins begins production of the Model K, an "upsized" Model U capable of delivering up to 210 horsepower. The engine and its descendants - the KO, L and LR - will go on to serve industrial markets for the next four decades.

Cummins Model H

1932

Cummins turns a corner with the Model H

With the launch of the H672, Cummins achieves its first major success with a heavy-duty diesel engine. The Model H will dominate the U.S. trucking industry for the next 70 years and be adapted for mining and other industrial uses.

NH Series engine

1947

NH Series introduced

The "New H" series upgrades the Model H and quickly goes on to establish reputations for durability and serviceability. Descendants of the NH Series will include electronically controlled engines like the N14, which will carry its architecture into the 1990s.

Cummins NVH Series

1949

NVH Series launched

The first NVH Series units combined two NH engines to deliver 400 to 600 horsepower at up to 2,100 rpm. NVH is part of Cummins' expansion into very large displacement engines for mining and other industrial applications and will endure through the 70s.

Cummins PT Fuel System

1952

PT Fuel System

The new PT (Pressure-Time) Fuel System revolutionizes diesel fuel systems by eliminating timing adjustments and many bulky components. It becomes a hallmark of Cummins mining engines for its ability to maintain stable power and cooling under heavy loads.

12-cylinder V engine Turbocharged

1954

From supercharging to turbocharging

In a major technological advancement, Cummins begins offering turbocharged versions of its 12-cylinder V engine (the VT-12), as well as its 6-cylinder NTs, NRTs and JTs.

Cummins begins building its first international manufacturing plant in Shotts, Lanarkshire, Scotland

1956

Expanding overseas

Cummins begins building its first international manufacturing plant in Shotts, Lanarkshire, Scotland. The first unit built at Shotts is a 335-horsepower Model H, which is shipped to Euclid for use in mining equipment.

Several countries around the globe

1959

Global presence

By the end of the 1950s, Cummins is regularly exporting mining engines and other equipment to 121 countries.

Dust protection for mining and construction engines

1960

Leaving competitors in the dust

Many exclusive dust protection features designed to extend the life of mining and construction engines become standard equipment in the 1960s.

Komatsu logo

1961

Alliance with Komatsu

Cummins signs a 15-year license agreement with Komatsu Manufacturing Company, Ltd., marking Cummins’ entry into East Asia. Much of Komatsu’s growth coincides with Japan’s post-war reconstruction effort.

Cummins remanufactured diesel engine

1966

Recon Division formed

With the founding of the Recon facility in Memphis, Tennessee (USA), Cummins begins making remanufacturing history. Mining operations can now turn to Cummins for the reconditioning of existing diesel engines and other components by a factory-trained team.

Cummins Technical Center

1967

Cummins Technical Center opens

Situated on 24 acres, the sprawling $22 million Cummins Technical Center demonstrates the company's dual focus on research and innovation. The facility's impressive proportions mirror the sizable contributions it will make in years to come.

Cummins Big Displacement

1969

Big Displacement

By the end of the 1960s, Cummins’ power range expands to 700 horsepower thanks in part to the “Big Displacement Concept, which provides more power, longer life, greater reliability and better fuel economy.

Cummins Holset

1973

Acquisition of Holset

To bring the emerging trend of turbocharging in-house and expand its business, Cummins purchases Holset, a world-class producer of turbomachinery based in England. The company later evolves to become the Cummins Turbo Technologies business unit.

Cummins Daventry plant

1973

Daventry plant opens

Cummins boosts its presence in the international mining sector with a new manufacturing facility at Daventry in the English Midlands. The first engine produced by 26 operators is a K38 engine supplied to Komatsu for a mine truck application.

Cummins K Series

1974

The K Series kicks off a new era of mining engines

The first K Series engines begin the transformation of the high-speed diesel market for mining. The new engines overcome the previous limitations of diesel power, helping to establish Cummins as a mining industry standard.

Cummins expands into China

1975

Expansion into China

Mining trucks equipped with Cummins high-horsepower diesel engines are first used in Chinese iron mines, starting a legendary long-term partnership with the country. Cummins is one of the first American companies to pursue business in China.

UH801 Ultra-large Hydraulic Excavator

1979

Hitachi Construction Machinery mining partnership begins

Cummins and Hitachi Construction Machinery launched their mining partnership with the UH801 Ultra-large Hydraulic Excavator — one of the largest models at the time — powered by a Cummins KT19C engine and delivered to North America.

Mining quarry with mountains in the background

1985

Cummins Electronics Company formed

Anticipating changes that won’t be fully realized until the 1990s, Cummins invests heavily in electronics, intensifying the company’s movement from mechanical to electronically controlled engines that will later deliver significant benefits to miners.

Emission cloud icons

1987

Emissions foresight

Cummins makes an all-out commitment to new technologies for reducing nitrogen oxides (NOx) and particulate matter in its engine emissions, years ahead of regulation deadlines. These efforts will lead to significantly improved K, NH and V903 models.

CELECT electronic control system

1990

CELECT makes an immediate impact

Cummins releases CELECT, its first full-authority electronic control system produced by Cummins. Setting the stage for all future controls, the system delivers compliance a full year in advance of 1991 U.S. EPA emissions standards.

CENTRY™ system

1992

CENTRY™ system introduced

The CENTRY system is released as the first intelligent electronic engine control system designed by Cummins for heavy-duty and off-highway applications like mining, construction and agriculture.

Cummins High-horsepower diesels

1992

High-horsepower diesels enter a new age

Cummins continues its development of leading-edge diesel electronics with the launch of the K2000E and K1800E, along with upgrade kits for existing engines at the top of the K Series family.

Mining quarry

1995

CENSE Electronics

Capable of remotely observing and diagnosing engines already in operation, CENSE Electronics is one of the first systems to continually monitor and record critical engine functions, tracking safety trends and accurately predicting service issues.

HPI fuel system

1995

HPI fuel system

Designed for higher injection pressures, the HPI (high-pressure injection) fuel system improves combustion control compared to PT systems. It features electronic actuators for timing and metering, delivering better precision and emissions control.

Cummins QSK19

1996

A Quantum leap in innovation

Cummins introduces the QSK19, the first engine in the Quantum series, a family of electronically controlled engines that sets new benchmarks for the lowest cost of operation for mine engines. It is soon followed by the QST30, QSK45 and QSK60.

Eliminator filtration oil filter

1997

Eliminator filtration

Cummins collaborates with Alfa Laval to develop the Eliminator, a breakthrough in oil filtration technology for high-horsepower engines used in demanding applications like mining, marine and rail, overcoming the limitations of traditional spin-on oil filters.

Cummins QSK78

2000

The QSK78

Cummins unveils the QSK78, designed in conjunction with Komatsu and built at the Cummins plant in Daventry, England. It's the largest, most powerful and environmentally friendly mining engine available in the world at that time.

Mining gateway website

2000

MiningGateway.com

Cummins unveils MiningGateway.com, an interactive internet portal that provides mining customers the information they need to get the lowest operating costs from their Cummins-powered haul trucks, excavators and drills.

Cummins SCR aftertreatment

2006

SCR aftertreatment

Cummins first installs selective catalytic reduction (SCR) aftertreatment technology on midrange engines certified to Euro IV standards for commercial vehicle applications in Europe. SCR becomes standard for Tier 4 HHP surface mining applications after 2015.

Cummins MCRS fuel system

2008

MCRS fuel system introduction

The modular common-rail fuel system (MCRS) becomes the new standard for Cummins high-horsepower mining engines. Higher injection pressure and larger accumulator volume enable better fuel economy, longer engine life and other improvements over older systems.

Cummins Tier 4 badge

2014

Tier 4 Final

Cummins begins launching Tier 4 Final (T4F) solutions for high-horsepower mining engines, meeting near-zero emissions requirements. Engines above 751 horsepower (560 kW) adopt SCR for durability and uptime in harsh mining conditions.

PrevenTech® for Mining digital monitoring and reporting solution

2019

Introduction of PrevenTech® for Mining

PrevenTech for Mining launches as a new digital monitoring and reporting solution that provides advanced detection of potential equipment health issues.

Cummins QSK95

2022

QSK95 production begins

Capable of producing up to 4,400 horsepower at 1,800 rpm, the QSK95 transforms performance for remote mining operations with high output, low emissions and 16-cylinder capability. Today, it remains the largest and most powerful mining engine ever built.

HVO pump icon

2023

HVO approved for Cummins HHP engines

Cummins announces approval of its entire line of diesel high-horsepower engines across all ratings for use with unblended paraffinic fuels (EN15940), often referred to as renewable diesel, including hydrotreated vegetable oil (HVO).

Cummins Hybrid pilot

2024

Hybrid pilot with NHL

Cummins announces field testing of a diesel-battery hybrid mining truck with North Hauler Joint Stock Co., Ltd. (NHL), one of China's leading rigid mining truck manufacturers. The system allows the engine to be downsized from a QSK60 to a two-stage QSK50.

Cummins Dual-fuel partnership

2024

Dual-fuel partnership

Cummins, Vale and Komatsu join forces to retrofit existing diesel engines in Komatsu haul trucks to operate on both ethanol and diesel. These modified 230- to 290-ton haul trucks will be able to use up to 70% ethanol, lowering CO2 emissions by up to 70%.

Cummins acquires First Mode

2025

Cummins acquires First Mode

Cummins acquires First Mode, a leader in retrofit hybrid solutions for mining and rail operations. The acquisition includes the first commercially available retrofit hybrid system for mining equipment. 

Cummins Hybrid powertrain

2025

Hybrids gain more headway

Cummins and Komatsu sign a memorandum of understanding (MOU) to collaborate on hybrid powertrains for heavy mining equipment. Komatsu's drive system supplier Wabtec teams with Cummins and former First Mode experts to accelerate development.

Preventech platform

2025

PrevenTech enhanced

The PrevenTech platform receives a major upgrade. The new, more robust platform is built for advanced analytics, accelerated onboarding, enhanced user experience, more intuitive fleet visibility and streamlined alert management.