Cummins Case Studies
We're in it for the long haul. We build lasting partnerships that lead to smarter innovations for our customers. These customer stories demonstrate our commitment and success in providing customers like you with improved power solutions through world-class innovation in a number of industries.
Purpose: To install a standby power system for a remote lodge and associated water-treatment facility
The NEW Water wastewater treatment facility chose Cummins, after violent rainstorms left them without power for hours at a time, and two natural gas generator sets, and a DMC8000 Digital Master Control System was installed to ensure the facility continued to run smoothly through unpredictable weather conditions.
Following an intense storm and widespread power losses, Tulco Industrial Storage turned to Cummins to install seven generators and four transfer switches, as to keep the power on for its climate-controlled storage of mission-critical oilfield machinery.
To support the expansion of the water treatment plant, located in Oman, Cummins installed five generator sets, including the first QSK95 in the country, to power the Treated Effluent Substation, biological treatment plant and central pumping station.
Overview Challenge: Ecologically sensitive city required reliable standby power for sewage collection system upgrade to increase safety and reduce the risk of sewage backup. Cummins Solution: Seven Cummins generators ranging from 20 kW to 200 kW, with a sound-attenuated enclosures and compact footprint and transfer switches. Result:
Overview Challenge: A large regional water treatment plant wanted to ensure that water would continue flowing to more than 200,000 residents even if the electric utility failed. Solution: Cummins provided a complete standby power system solution that included two 2.7 MW diesel generator sets for a total capacity of 5.4 MW as well as transfer sw
Overview Challenge: A substantial redevelopment project in the town of Wayzata, Minnesota was going to bring hundreds of new apartments, additional office space and a small hotel. All of that required an expanded wastewater system with larger lift stations. One of the larger lift stations would handle wastewater for about half the town. Reliable standby po