""
Marine

Assembly Line For Tugs

by Alan Haig-Brown

Cummins Vessel Reference #614

Ready for work.

The shipyards of Sarawak are particularly adept at meeting the demands of multiple tug orders. Kian Juan Dockyard in Miri is currently in the midst of a ten-boat order all of which are built to the same design. As of late January this year two units had been delivered and six were scheduling for sea trails. The balance of two units had already been launched and were fitting out alongside. The large open area, extensive covered shop buildings and ample river frontage ease the logistical complexity of this sort of an undertaking. The ability of local suppliers to meet requirements on time and on schedule is equally important.

The Miri facility for Scott and English, supplied the 20 1200-HP Cummins KTA38-M2 main engines for the ten 30- by 8.6-meter tugs. Each tug will have 2400 HP turning a pair of 2000 by 1789-m/m props through Twin Disc MG5321 DC gears with 5.96:1 reductions. This power will give the tugs a 25-ton design bollard pull and a speed of eleven knots.


One of ten.

With a 4.13-meter molded depth, each tug has capacity for 203-tons of fuel, 50 tons of potable water, 57 tons of ballast water. Accommodation for crew is provided in two one-man cabins and four cabins for three people each. The boats have sewage holding tanks and treatment systems. They are also fitted with oily bilge-water separators.

A 25-ton single-drum towing winch with capacity for 500 meters of 48 m/m line is mounted on the after deck. The vessel is also fitted with a quick-release towing hook.

Scott & English also supplied the ten boats' 20 Cummins 6BT5.9-powered 78 kW generator sets. The tugs are classed GL +100 A5 +MC, Tug Unrestricted Navigation. The ten tugs are built to the account of Thaumas Marine Ltd, of Sabah, Malaysia. Spokesman for the owners, David Chee, reports that the vessels are for sale with prompt delivery ex Miri yard at USD 1.95 million net to the owner.


For further information:

Mr. Lim Pah Poh Meng – Yard Manager
Kian Juan Dockyard Sdn Bhd
Lot 2042, Kuala Baram Industrial Estate,
98000 Miri Sarawak, Malaysia.
Tel: 6085 605678
Fax: 6085 605455
Email: [email protected]

Thaumas Marine Ltd.
Mdm Jubie – Marketing Officer
Mobile: 60 13 863 8339
Correspondence Address: Block G • Lot 3B • Bandar Leila
W.D.T. 259 • 90009 Sandakan
Sabah • Malaysia
Phone: 60 89 616263
Fax: 60 89 616654
E-mail: [email protected]

MT Chong
Scott & English (M) Sdn Bhd
Lot 1450 & 1451, Block 3, M.C.L.D.,
Piasau Industrial Estate,
98000 Miri, Sarawak, Malaysia.
Tel: 6085 – 654984
Fax: 6085 – 654193
E-mail: [email protected]

Related case studies
Marine Case Study

Trophy fish are measured by weight and length at the dock. They almost always exceed the size of the angler reeling them in. The exception would be M/V Chelsea ...

Marine Case Study

Greek passenger vessel repowers with Cummins.  Cruising to Symi on a water taxi is more than a boat ride across the Aegean Sea. Departing the eastern sh...

Marine Case Study

Crews with no choice but to head out to sea in rough weather conditions rely on trawlers' inherently robust, stout design based on the DNA of highly capable fis...