INSITE performs engine diagnostics and displays electronic engine information on your PC. With step-by-step diagnostics, built-in engine drawings and schematic diagrams, working with INSITE is easy. Using this software application will reduce troubleshooting time, errors and incorrect procedures and quickly get your vehicle back on the road again.
Features:
• Quick access to trip information
• Adjust parameters and review/clear fault information quickly and easily
• Easy-to-follow troubleshooting assistance
• Wiring and sensor location diagrams
• Store engine and trip information for future use, or as programming templates
Software Downloads
Your company’s firewall may inhibit the installation of these files.
Please contact your system administrator for assistance if you receive such a message.
ATTENTION INSITE USERS: INSITE 8.6 has been released. With this release there is a special requirement customer need to prepare for:
Users must have .NET 4.7.1 installed in order to run the updated version of INSITE. This may impact some users if their Windows has not been kept updated. See the information below or the release notes for more details.
- Microsoft .NET Framework 4.7.1 is supported on Windows 8.1 and Windows 10.
- Microsoft .NET Framework 4.7.1 is not supported on Windows 7 and Windows 8.
Please refer to the table below for operating system versions.
Operating System | Version | Build number |
Windows 10< | 1607 | 10.0.14393 |
Windows 10 | 1703 | 10.0.15063 |
Windows 10 | 1709 | 10.0.16299 |
Windows 8.1 | N/A | 6.3.9600 |
- .NET Framework system requirements
- Release Information
- PC System Requirements
- INSITE 8.5.0 Quick Start Guide
All users must upgrade their Microsoft Windows Operating System to version 8.1 or newer, as Windows 7 is no longer supported after 20-Dec-2020.
All users using Microsoft Windows 8.1 or newer also must upgrade their Cummins Inc. Update Manager client to version 7.3 or later before 20-Dec-2020 to be able to continue to receive updates via Update Manager.
DOWNLOAD (Size: 1.7 GB)
Installation: During the installation of the INSITE 8.7.0.exe, the user may see multiple dialog boxes of antivirus detecting suspicious files during the whole installation. The user does not need to acknowledge them.
Calibration Security: On Dec 10, 2020, new engine control module (ECM) calibration codes will be released using industry standard encryption for all electronically controlled engine products. These ECM calibration codes are only supported in INSITE™ electronic service tool version 8.7.0 and newer. If user does not upgrade, users will not be able to use any calibrations downloaded through QSOL or Cal over web/ECM Code Search feature within INSITE™ after Dec 10, 2020.
This ZIP Contains:
· INSITE™ 8.7.0
· License Configuration Tool 1.16
· INSITE™ Guidanz Service
· INSITE™ ARA
· Update Manager 7.5
Note to Users: If a user wants to use the INSITE 8.7.0 Other Package, the extracted other package can only be used once. If user wants to use is a second time, the user needs to delete the extracted package and re-extract the OtherPackage.zip file.
DOWNLOAD (Size: 1.8 GB)
This package is used with Update Manager ONLY to upgrade from INSITE 8.4.X, INSITE 8.5.X, and INSITE 8.6.X
Installation Instructions:
Note: Once extracted into C:\Temp, Update Manager is required to install. Choose Source > Browse, and select the folder where you extracted the Update Manager to.
Note to Users: If a user wants to use the INSITE 8.7.0 Other Package, the extracted other package can only be used once. If user wants to use is a second time, the user needs to delete the extracted package and re-extract the OtherPackage.zip file.
This software is not available on mobile. To download for your office or home computer, please return to this page from that device.
Software Licensing
Some Cummins software and mobile applications – including INSITE™, Guidanz®, PowerSpec and QuickCheck – require unique software licenses for use. Licenses are available through a Cummins-authorized distributor or dealer. Please provide us a few details to find your local representative.
Results
Training Videos
Training Materials
INSITE Overview, updated 3/19/2018 (Size: 6 MB)
Visão Geral do INSITE, in Brazilian Portuguese (Size: 7 MB)
Licensing & License Configuration Tool Overview, updated 4/14/14 (Size: 3.8 MB)
INSITE 8.0.3 New Feature Training: ECM Code Search, updated 5/11/15 (Size: 0.9 MB)
How To Export/Backup/Email Work Order Image(s) (Size:0.5 MB)