Benefits of alternative fuels and fuel-flexibility

A pair of cupped hands holds a mound of soil, out of which grows a small plant. An outline of a light bulb is drawn around the plant.

Internal combustion engines using traditional and alternative fuels are an integral part of life in all parts of the world. They are almost universally used in motor vehicles of all kinds, in power generation, and more. Traditionally, internal combustion engines run on liquid fuels. These fuels are distilled from petroleum. Think gasoline, diesel, kerosene or heavy fuel oil. 

What are alternative fuels?

Liquid fossil fuels are convenient and affordable, but they are not the only fuels that engines can burn. In fact, alternative fuels have been available for as long as internal combustion engines have existed. For example, vehicles running on a fuel known as wood gas were widely used during World War II. This allowed to save fuel needed for the war effort. Wood gas was generated by the incomplete combustion of wood chips. The process would take place in a sort of large kettle. The kettle could be placed on a trailer behind a vehicle, and from there piped to the vehicle’s engine. 

Today, few vehicles run on wood gas, but many other alternative fuels are available, and several more are being developed. Some, such as compressed natural gas (CNG) and liquid petroleum gas (LPG—a mix of propane and butane), are derived from fossil fuels. Others, such as renewable diesel, biodiesel, ethanol and biogas are obtained from energy crops or from organic waste. You can check out what are the low carbon fuels to learn more.  

Advances in chemical engineering and other disciplines have also made it possible to synthesize methane, hydrogen, diesel and more from non-fossil feedstock such as carbon dioxide (CO2) and water using renewable electricity. These synthetic fuels are sometimes known as e-fuels. You can check out what are power-to-x and e-fuels to learn more.

Renewable diesel can be used as drop-in replacements. For most engines, no modification is required. Biodiesels must be blended with fossil diesel to be used in standard compression ignition (CI) engines. Ethanol—basically, alcohol—can also be used in traditional SI (spark ignition) vehicles when it is blended with gasoline. Ethanol blending is extremely common. More than 98% of all gasoline sold in the United States contain a significant proportion of ethanol. 

For example, The Cummins Inc. Ethos spark ignited engine can run E85 (85% ethanol) without any modification. Meanwhile, engines capable of running flex fuel can use a blend of gasoline and ethanol from 51% to 83% (E85). Vehicles with this capability, known as fuel-flex vehicles, are not rare—according to the U.S. Department of Energy, there are more than 21 million fuel-flex vehicles driving on US roads. 

What is fuel flexibility?

Fuel flexibility is also an option for equipment owners who wish to use CNG or LPG as an alternative to gasoline. Either can be achieved with the addition of a separate fuel system and the addition of a new set of fuel injectors in the engine. Owners of dual-fuel vehicles can thus run on CNG, and, if no CNG fueling station is nearby when the gaseous fuel runs out, continue driving on gasoline. 

Alternative fuels are not just for road vehicles. Agricultural machinery, mining equipment, ships, locomotives, and other vehicles can all potentially benefit from using alternative fuels. Alternative fuels are also an option for stationary internal combustion engines. Stationary engines are commonly used in industrial applications such as oil and gas extraction or power generation. Power plant owners can more easily meet their operational and financial objectives when they have the option to use either traditional diesel, biodiesel or natural gas in their power plant. Power plants based on reciprocating engine power generators, for example, can start their engines on natural gas. Once the engines are running, they can be switched to biodiesel, allowing net CO2-free operation.

Businesses operating fleets of vehicles are constantly making tradeoffs between multiple objectives such as reducing capital costs, reducing maintenance costs, reducing fuel costs, and reducing emissions, while taking into consideration range and refueling constraints, among others. Adopting the use of an alternative fuel can help further one or more of those objectives. 

Environmental benefits of alternative fuels

Using an alternative fuel can be a good way to reduce carbon emissions. Burning fossil fuels releases carbon into the atmosphere that was previously stored underground. 

Biofuels, in contrast, release the carbon which was taken from the atmosphere by the crops that they are made from. This is why biofuels are thought of as net-CO2 free fuels. Similarly, renewable natural gas fuel produced from landfill, or sewer gas can be considered as a fuel with negative carbon intensity.

For businesses who wish to reduce their carbon footprint, alternative fuels present a variety of options. Switching to CNG or LPG can result in significant CO2 reductions, despite their fossil nature. Using a fuel with a greater ethanol or biodiesel content can also be effective. For businesses seeking further reductions in CO2 emissions, full conversions to biodiesel, hydrotreated vegetable oil (HVO), ethanol, renewable natural gas, or even hydrogen, or an e-fuel may also be an option. 

Besides CO2, internal combustion engines emit other gases in their exhaust. Most businesses should be concerned by the non-carbon emissions of their vehicle fleets. Clean-burning alternative fuels can help in that regard. In some cases, for example, converting a diesel truck to run on CNG can be more cost effective in the long run than investing in diesel exhaust emissions control equipment. 

In certain industries, additionally, non-carbon emissions pose a specific set of problems. These problems can lead to transformative solutions designed around an alternative fuel. Mines, for example, require a powerful ventilation system in order to maintain a safe and breathable environment. With heavy machinery operating underground, this is no easy task. Operating that ventilation system can be very costly and consume a lot of energy. These considerations have led several mining companies to explore options to fuel this machinery with hydrogen. Using hydrogen as a fuel would result in no emissions at all, and thus far smaller ventilation needs.

Economical benefits of alternative fuels

Traditional fossil fuels such as gasoline and diesel are generally convenient and affordable, but there are situations where alternative fuels are cheaper. Natural gas, specifically, has been consistently cheaper than gasoline and diesel when measured on a gasoline gallon equivalent basis. Operators of city buses, dumpster trucks and other commercial vehicles have saved millions of dollars by converting their fleets to run on CNG. 

Biogas can be used to generate electricity and heat for the water treatment process

In addition to being low, the price of natural gas is also stable over time. Natural gas prices tend to avoid the cyclical price fluctuations that petroleum-based fuels such as gasoline experience. As a result, owners of compressed natural gas vehicles enjoy operating costs that are both lower and more predictable.

Maintenance and other advantages of alternative fuels

Alternative fuels present a variety of other advantages. Here are some additional benefits:

  • Shelf life: Unlike gasoline and diesel, natural gas and propane have an unlimited shelf life, as do hydrogen and ammonia-based e-fuels. This is also true of several newer biodiesel and synthetic diesel formulations, which can last up to 10 years. 
  • Environmental compatibility: Biodiesel and renewable diesel are also biodegradable, non-toxic and produce less fumes. Likewise, LPG and natural gas are not likely to result in any soil or water contamination if spilled, since they would simply vaporize.
  • Reduced maintenance needs: Natural gas and propane tend to burn cleaner than liquid fuels. A lesser amount of soot thus makes its way into the engine’s oil. Some operators take advantage of this by extending oil change intervals. When a large fleet of vehicles are involved, this can easily result in a savings of tens of thousands of dollars or more.
  • Performance: Biodiesel and ethanol blends also have higher cetane and octane ratings than unblended diesel or gasoline, providing improved performance and acceleration. This is one of the reasons why; in the United States, NASCAR advertises its use of a blend of ethanol and gasoline containing 15% of ethanol—significantly more than the average fuel available at the pump.

Alternative fuels are far more common than many people realize. Several types of alternative fuels with a proven track record are available and, when deployed judiciously, can help businesses meet their environmental and cost reduction objectives.

Benefits of alternative fuels specific to your business

Your business has distinct characteristics and needs. As a result, you might find some of these alternative fuels more valuable than others. There are also other factors such as fuel availability, use case, and local regulations that you need to consider. 

These additional factors often are more localized. You can benefit from working with a partner knowledgeable in these local aspects and understand your business more intimately. We recommend you reach out to a local partner to find the best fit solution for your business and needs

Alternative fuels’ compatibility with different engines

Whether you are in marine, mining, rail, power generation or another sector, you may be wondering if your equipment is compatible with different alternative fuels. Please work with your Cummins partner to find the most up to date information about your engines and alternative fuels available for your needs.
 

Raise Your Energy IQ

Grow professionally with energy trends and insights delivered to your inbox. Read about energy technologies and trends on our Energy IQ Hub.

Aytek Yuksel - Cummins Inc

Aytek Yuksel

Aytek Yuksel is the Content Marketing Leader for Cummins Inc., with a focus on Power Systems markets. Aytek joined the Company in 2008. Since then, he has worked in several marketing roles and now brings you the learnings from our key markets ranging from industrial to residential markets. Aytek lives in Minneapolis, Minnesota with his wife and two kids.

What markets and commercial vehicle applications are well-suited for propane ?

alt fuel

Medium duty vehicle fleets, from postal vans to school buses, are switching to alternative fuels. Among low-carbon emitting fuels, propane, also known as autogas, is one of the most readily available options.

As an alternative to gasoline and diesel, propane vehicles produce less greenhouse gases and harmful air pollutants. Thirty billion gallons of propane are produced domestically in the United States, with 20 billion gallons being exported each year. Its price is not subject to shocks connected to global supply and demand. This results in more stable prices over the long run, among other operational benefits. Therefore, propane vehicle operators can secure long-term fuel contracts at fixed costs.

Centralized, regional, and return-to-home base fleets are well suited for propane autogas vehicles. Propane-powered transit vehicles can help improve the air quality in densely populated areas. That’s because, compared to diesel, they have lower NOx emissions, particulate matter and other air pollutants.  Additional benefits for more suburban and rural fleets include easy, affordable, and scalable infrastructure as propane is available in every community across the country. Propane is also one of the most accessible alternative fuel sources not only nationwide, but worldwide. Most propane fleets own their fueling infrastructure due to low installation costs, but drivers can also access over 2,600 public refueling sites across the United States. 

Urban delivery trucks can lower emissions with propane autogas engines

In 2019, the U.S. Postal Service (USPS) committed to lowering its greenhouse gas emissions 30 percent by 2025. Today, USPS operates a fleet of over 30,000 alternative fuel vehicles and has implemented incentives for contractors to do the same. The Cummins B6.7 propane is an ideal engine for postal vehicles, like USPS and its contractors, seeking to achieve key sustainability goals. 

With 325 hp and 750lb-ft peak torque at 1800 RPM, the B6.7 propane can also be used in class 6 straight-box trucks for food and beverage delivery, tow trucks, and terminal tractors. Propane autogas offers fleets in these markets the lowest total cost-of-ownership compared with other fuels. In fact, many fleets have reduced their operating costs by 50 percent after making the switch from diesel.

Utility and service vehicles have been using propane for a long time

Propane is a good fuel source for everyday utility and service vehicles. Propane is widely used for forklifts and can be used for other utility vehicles such as golf carts, street sweepers, and snowplows. Propane is also well-suited for emergency service vehicle fleets such as ambulances and police cars. In 2021, the city of Petersburg, Virginia converted its public fleet of 49 vehicles to run on renewable propane. By switching to the propane fueled fleet, the city forecasted it would save $1,000 per vehicle per year.

School buses running on propane help improve air quality

As mentioned above, propane vehicles help improve air quality. Residents and passengers in city, suburban, and rural areas are less likely to be exposed to harmful exhaust fumes, as propane burns significantly cleaner than other fossil fuels.

School buses are one of the most visible markets for propane autogas. There are currently more than 22,000 propane autogas school buses transporting kids to school each day. Propane autogas engines are also quieter than gasoline/diesel engines and help decrease noise pollution. The Cummins B6.7 propane engine can provide large buses the power to run long, high-capacity routes.

Propane delivery trucks can lower fuel and maintenance cost

Propane delivery trucks, also known as bobtails, are specially designed bulk delivery vehicles that deliver propane to businesses and homes.

Bobtails that run on propane can benefit from lower fuel and maintenance costs while reducing carbon emissions. The new Cummins B6.7 propane engine is well-suited for use in bobtails.

Overall, propane offers many benefits and is well suited for delivery trucks, school buses, utility vehicles and bobtails. It’s a clean burning, low-cost alternative fuel source, available in abundant quantities across the United States and around the world. Are you interested in learning more about propane use in motor vehicles? Check out Cummins B6.7 propane engine for various medium duty applications.

Puneet Singh Jhawar

Puneet Singh Jhawar

Puneet Singh Jhawar is the General Manager of the global natural gas business for Cummins Inc. In this role, he is responsible for the product vision, financial management and overall performance of the natural gas business. Over his 14-year career at Cummins, Jhawar has cultivated successful relationships with a number of Cummins’ largest customers. Jhawar has extensive global experience, with roles based in the Middle East, India, Europe and the US.

Natural gas is well-positioned to fuel vehicles for today’s energy transition

truck on highway

Natural gas powers more than 175,000 vehicles in the United States and 23 million vehicles worldwide. It’s an ideal alternative to gasoline and diesel for heavy and medium-duty applications. These include freight-hauling trucks, buses, and garbage trucks. Natural gas engines provide horsepower, acceleration, and cruise speed comparable to conventional fossil fuel engines. This fuel can also replace gasoline in smaller applications, such as forklifts and commercial lawn equipment. 

Natural gas engines reduce emissions and environmental risks

Many companies are setting carbon reduction targets for tailpipe emissions. Fleets can meet these requirements by replacing older vehicles or generators that run on diesel to new ones that use natural gas. 

Switching to natural gas can reduce hydrocarbons, carbon dioxide (CO2), nitrous oxide and other greenhouse gas (GHG) emissions. The size of the reduction depends on vehicle type, duty cycle, and engine calibration. Vehicles that use compressed natural gas (CNG) can reduce their GHG emissions by 13-18%. That percentage is a lot higher when using renewable natural gas (RNG) or a blend between the two gases. 

Natural gas vehicles offer additional air quality and environmental justice benefits too. They emit almost no particulate matter, volatile organic compounds or carbon monoxide which lead to poor air quality.

There are also other environmental risks that can be eliminated. For example, natural gas can’t spill because it’s lighter than air. It doesn’t puddle or cause ground contamination like a diesel or gasoline spill would.

Renewable natural gas is a carbon neutral fuel alternative

RNG is manufactured from agricultural by-products and organic waste from food manufacturing, farming and groceries. The systems needed to fuel a vehicle with RNG or with fossil natural gas are identical. Both fuels are interchangeable and can be blended. National, state and local incentives for RNG projects are also available. RNG is considered a carbon neutral fuel and it can even be carbon negative when using waste from landfills -that’s at least a 100% GHG reduction! 

RNG provides more benefits than CNG. Methane (CH4) from a landfill or a wastewater treatment facility is typically vented into the atmosphere. Its global warming potential (GWP) is more than 25 times greater than CO2. That makes capturing and refining methane into a fuel for natural gas engines a better alternative. 

Enabling fleets to more affordable engine solutions with natural gas

Natural gas engines meet stringent environmental standards with less complicated emissions controls. As a result, they offer an affordable advantage over diesel engines.

Additional cost savings can be achieved by converting conventional vehicles to run on natural gas. Kits are available to retrofit existing fleets. And automotive original equipment manufacturers (OEMs) offer natural gas versions of their medium and heavy-duty vehicles.

Natural gas refueling stations also can be less expensive to construct than those for hydrogen (H2) or electric vehicles. Their proven equipment and systems are less complex.

National gas also allows fleets to better predict operational costs. The fuel itself costs less than gasoline and diesel. In some areas, natural gas can even be half of the price of diesel. These prices have remained relatively flat for 20 years. This helps fleet operators by being able to reliably forecast monthly and yearly natural gas costs.

Expanding the natural gas supply for national energy independence

The United States has an estimated 2,926 trillion cubic feet of natural gas — enough to last about 98 years. In 2021, 64% of all on-road fuel used in natural gas engines was renewable natural gas. That percentage increases in California, where it’s 98%. The growing use of RNG further diversifies domestic energy supplies. 

Natural gas is readily available through established distribution channels. Supplies are so abundant that natural gas is also compressed and exported. It moves across the United States through a pipeline network that links production areas and storage facilities with 77 million customers.

Compressor stations utilize natural gas engines to keep fuel flowing to distribution companies. They deliver natural gas to consumers through small-diameter, lower-pressure service lines.

Natural gas is available at nearly 900 compressed natural gas (CNG) stations. Another 60 liquefied natural gas (LNG) fueling stations are located in areas that service long-haul trucks. 

Refueling is done at:

  • Fast-fill stations, where natural gas vehicles can fill up in about the same time it takes to refuel gas and diesel vehicles
  • Long-fill stations, where natural gas vehicles slowly fill up overnight or during extended breaks between trips

In summary, natural gas engines can help fleets lower their total transportation emission and operating costs without major disruptions to their day-to-day operations. Natural gas, as a fuel, has a key role to play in our renewable future.  

Traci Kraus headshot

Traci Kraus

Traci Kraus is a Director of Government Relations where she leads US federal advocacy for Cummins. She focuses on energy, climate, hydrogen, transportation and budget legislative and regulatory issues. 

Prior to joining Cummins, Traci worked for former U.S. Senator Russ Feingold.  She has a Master’s in Public Administration from the George Washington University and B.A.s in Government and Politics and Communication from the University of Maryland in College Park. She is originally from Chicago, and now lives outside of Washington, D.C. with her husband, Aaron and two children Liam (8) and Sloane (5).

How is the United States investing in clean energy?

GR hero

Our planet is facing a dire crisis: carbon dioxide concentrations in the atmosphere continue to soar above record highs. If gone unaddressed, the collective stress of climate change will produce an irreparable impact. Our health, energy, water, and food ecosystems are at risk. 

As it stands, there are many long-term effects of climate change. In North America, climate change is forecasted to cause decreasing snowpack in the western mountains. It will also lead to a 5–20% increase in yields of rain-fed agriculture and great intensity of heat waves. In fact, over the last five years, the United States has incurred roughly $120 billion a year in damages as a result of natural disasters caused by extreme weather and climate events.

Beyond natural catastrophes, climatic risks to the United States will have a cascading effect on the country’s interconnected ecosystems. Reduced labor and overall economic productivity, and altered crop yields, will disproportionately harm lower-income and marginalized populations. These groups lack the resources to prepare or cope with extreme weather and climate events.

The world is investing in clean energy innovation

Combating the intensifying climate crisis requires a strategic combination of research and development (R&D), innovation, technology — and bold attempts.

Around the globe, countries are investing in clean energy to contribute to a livable planet now and for generations to come. In 2022, the US passed the Inflation Reduction Act, which includes a historic $370 billion investment to address the climate crisis. The Inflation Reduction Act provides tax credits and incentives to power homes, businesses, and communities with clean energy by 2030. The Act will increase investments in the fastest-growing power generation technologies, solar and wind. It will also advance cost-saving clean energy projects and protect two million acres of national forests. These initiatives are in addition to substantial tax credits and rebates offered to families and businesses in the United States.
Consequently, a stronger clean energy economy will contribute to overall economic growth and competition. As a result, there will be millions of new well-paying jobs for Americans to make clean energy.

It is possible to start decarbonizing now

Governmental policy strategies and investments in decarbonization technologies are part of the solution to produce increasingly cheap, dependable, and clean energy.

Strong communities and vibrant economies depend on a healthier planet. As a global power technology leader, Cummins is in a unique position to power customer success by leading during this energy transition. We intent to do so by providing customers with the right technology at the right time, understanding of their needs and applications.

We think of this journey to carbon neutrality in two distinct and complementary ways. First, by innovating zero-emission solutions and introducing them in markets and applications where the infrastructure, development and deployment are ready. Secondly, by advancing internal combustion engines through efficiency improvement and by running them on cleaner alternative fuels for a well-to-wheels solution.

Through Destination Zero, we are advancing low- and no-carbon platforms. This includes diesel and natural gas engines, hybrid, and electric platforms, as well as powertrain components, controls, and related technologies.

Join Cummins in powering a better tomorrow

Cummins environmental sustainability strategy includes goals timed for 2030. Progress toward the reduction of carbon emissions from company plants and facilities — in addition to our products — is in full swing. For more than one hundred years, we have brought technological solutions to market. As a power solutions leader, we will continue to power a more prosperous world for today and tomorrow. Are you ready to consider investing in new power solutions?

Traci Kraus headshot

Traci Kraus

Traci Kraus is a Director of Government Relations where she leads US federal advocacy for Cummins. She focuses on energy, climate, hydrogen, transportation and budget legislative and regulatory issues. 

Prior to joining Cummins, Traci worked for former U.S. Senator Russ Feingold.  She has a Master’s in Public Administration from the George Washington University and B.A.s in Government and Politics and Communication from the University of Maryland in College Park. She is originally from Chicago, and now lives outside of Washington, D.C. with her husband, Aaron and two children Liam (8) and Sloane (5).

Economic and Operational Benefits of Propane Engines

semi trucks driving on highway

Propane is a low carbon energy source commonly used in millions of homes across the country for cooking, home heating, hot water and many other applications. It can also be used as a clean vehicle fuel in medium duty applications including school buses, delivery and beverage fleets, paratransit vehicles and more.

Thousands of fleet owners choose propane autogas because it offers many environmental, economic and operational benefits. With new technology like the Cummins B6.7 propane engine, fleet owners can experience the power of diesel while producing less greenhouse gas emissions and air pollutants, ultimately saving on operations costs.

Propane is a clean fuel

In testing, the Cummins B6.7 propane engine delivered the lowest greenhouse gas emissions of any propane autogas-powered engine. It will also deliver some of the lowest GHG emissions in the medium-duty market. It is an ultra-low, .02 NOx engine that will meet or exceed EPA and CARB regulations in 2024 and beyond.

For fleets and other end users looking to meet environmental goals, renewable propane is available in the market. It has the same chemical structure and physical properties as conventional propane. It has an even lower carbon intensity than conventional propane because it’s produced from renewable, raw materials. This fuel can be used in any existing propane autogas engine or propane autogas infrastructure. Therefore, fleet owners will be able to easily implement this cleaner energy source in their own vehicles.

Propane is an abundant domestically produced fuel

Approximately 30 billion gallons of propane are produced annually in the United States and about 80% of U.S. propane is produced during the natural gas refining process. Because of that, its price is decoupled from the price of crude oil set by the global market.

Propane is an abundant and portable natural resource in North America. It can be distributed in liquid form using ships, rail cars, trucks and via pipelines. Best of all, propane is an environmentally friendly energy source. When compared with other options like diesel or gasoline, propane can significantly reduce harmful emissions.

Since propane is produced in the U.S., the domestic supply is shielded from global geopolitical and economic shocks. Unlike gasoline and diesel, it provides a reliable energy source for business owners.

Propane engines provide low total operating costs

Due to propane’s widespread and long-standing usage, propane autogas engines are a mature technology. The B6.7 propane engine will be built on Cummins’ fuel agnostic platform, meaning many parts are shared across an array of other engines. This will help reduce cost and complexity to the customer in terms of vehicle acquisition, integration of lower carbon fuel types, and vehicle maintenance.

As a vehicle fuel, propane autogas is affordable and typically costs as much as 50 percent less than diesel. The wholesale cost of propane autogas falls between the price of oil and natural gas, which are the fuel’s two sources. Because of this, propane autogas prices don’t fluctuate as sharply as other fuels, so fleet owners are able to easily manage fuel budgets.

Additionally, there is no need for an exhaust treatment system. That’s because propane is a clean energy source that produces 20 times less nitrogen oxides and particulate emissions than diesel. The B6.7 propane engine is instead fitted with a maintenance-free, three-way catalyst exhaust system.

Due to the cost-effectiveness of the fuel and reduced maintenance costs, propane autogas provides fleet owners with the lowest total cost of ownership. Propane autogas engines like the Cummins B6.7 propane will provide a strong return on investment and a low cost per mile.

Propane engines offer a simple refueling experience

A benefit of propane autogas that many fleet owners may not immediately think about is the ease and affordability of refueling. Fleets can choose from several refueling options. Each one offers distinct advantages that help a company identify and customize a solution that best fits its business and maximizes productivity.

Options range from private on-site stations that are fully scalable to meet the demands of a fleet, to temporary field stations to employ around a site in the field. Some fleets can even use any of the more than 2,800 public refueling stations around the country. Best of all, propane suppliers will often lease the refueling infrastructure to a fleet in exchange for a fuel contract that locks in a set price per gallon for a duration beneficial to both parties.

Fleet owners must consider what energy source will best meet their environmental, economic, and operational needs. With new propane autogas innovations, the Cummins B6.7 propane engine becomes an attractive solution.


Never miss the latest news. Sign up below to receive the latest in technologies, products, industry news, and more. 
 

Never miss the latest

Stay ahead with the latest in new technologies, products, industry trends and news.

Send me the latest news in (check all that apply):
Puneet Singh Jhawar

Puneet Singh Jhawar

Puneet Singh Jhawar is the General Manager of the global natural gas business for Cummins Inc. In this role, he is responsible for the product vision, financial management and overall performance of the natural gas business. Over his 14-year career at Cummins, Jhawar has cultivated successful relationships with a number of Cummins’ largest customers. Jhawar has extensive global experience, with roles based in the Middle East, India, Europe and the US.

Redirecting to
cummins.com

The information you are looking for is on
cummins.com

We are launching that site for you now.

Thank you.