Second quarter revenues of $6.2 billion increased 1 percent from the same quarter in 2018. Increased truck production in North America and stronger demand in North American power generation markets was partially offset by lower demand in oil and gas and international truck markets. Currency negatively impacted revenues by 2 percent primarily due to a stronger US dollar.
Cummins Vessel Reference #861
Iguazú Jungle is a company providing tourist excursions on Argentina’s Iguazú River. In total, the fleet transports approximately 1,200 passengers daily up through the river’s powerful currents to the foot of the Iguazú Falls in the National Park.
1993 Toyota 4Runner
Preventing power outages caused by severe weather. Keeping the lights on. Keeping our critical facilities up and running when the most severe weather strikes. These challenges are not unique to one region of the U.S. Weather events, disasters and power outages occur in your state too.
Not only that, the Niger International Airport represents a major gateway into the country, expanding Niger’s global connection by servicing both domestic and international routes from its capital, Niamey.
The terminal configuration is a double-sided pier, allowing gates and aircraft parking on both sides, with 16 contact stands and six remote stands. With an area of 120,000 square meters and at 35 meters tall, the building boasts an indoor park.
Cummins B6.7 engine has been integrated with CLAAS’s powertrain to deliver the optimum fit and performance for the AVERO. Delivering 157 kW (213 hp) maximum power and 990 Nm peak torque in CLAAS’s larger model and 123 kW (167 hp), 746 Nm peak torque in the smaller model, the B6.7’s power and torque curves have been tailored specifically to AVERO’s duty cycle using Cummins’ in-house electronic controls, fuel injection, air handling and exhaust aftertreatment technologies.
Autonomous operation combined with diesel-power and a U-shaped design allow Dot to carry, rather than tow, a multitude of implements. Norbert Beaujot, President & Owner, Dot Technology tells us more about this unique application:
Joseph Collins came to Cummins nearly a year ago after experiencing firsthand the power of its "legendary culture." Collins' uncle had worked for Cummins for close to thirty years beginning in the 1960s, and he always spoke fondly of the men and women he worked alongside.
It was those same co-workers who traveled across state lines years later to celebrate his uncle's life when he passed away. This show of Cummins' caring culture was ultimately what drew Collins to follow in his uncle's footsteps and pursue a career with Cummins.
There, in the corner of the lobby of the Tech Center office building, amid the models of classic Cummins engines through the years, Blanz saw a small piece of equipment on a work bench that he hadn’t noticed before. The machine was just a little bit bigger than what you might see in a hobbyist’s home workshop today.
In her latest blog post for Cummins, Donna shares her top six weekend getaways for baby boomers, that could easily turn into a week-long vacation.
3191 - 3201
of 9042
Perhaps try searching for a different keyword or phrase.
-------
If you don't find what you're looking for here, try the Cummins Care page. There you can search our product support database or contact us for help.
Looking for Parts Catalogs? Please visit parts.cummins.com.
Looking for Manuals? Please visit the manuals support page for electronic versions or store.cummins.com to purchase hard copies.