alternator
Mining Generators

Reliable Power Solutions: Arken Generator's project with Erdemir Maden

Discover how customized power solutions ensure continuous operation and meet the rigorous demands of high-altitude industrial environments.
by Cummins Inc., Global Power Technology Leader
Arken Generator, in collaboration with STAMFORD | AvK, powers critical operations at Turkey’s Ermaden Coal Mine.
Location
Zonguldak, Turkey
Date
December 2024

Ensuring uninterrupted operations in Turkey's leading coal mines with advanced power solutions

Founded in 2012, Arken Generator is a 100% Turkish-owned company committed to providing dependable power solutions under its motto, “Life Goes On.” Operating out of its high-capacity production facility in Arnavutköy, Istanbul, Arken manufactures up to 5,000 generator sets per year, ranging from 2 to 2,750 kVA. With a network of established distributorships across the Middle East, Europe, and Africa, Arken has become a trusted name for energy solutions in diverse industries worldwide.

Powering Erdemir Maden’s essential mining operations

Erdemir Maden, responsible for 34% of Turkey’s iron ore production, is a key supplier to OYAK Mining Metallurgy. Facing critical power needs for its Ermaden Coal Mine in Zonguldak, Erdemir Maden required a Diesel Electrogen Group and Synchronisation System to support essential operations in challenging conditions. The system needed to power two main water pumps (345kW at 3.3kV) and a 315kW air compressor, essential for rapid water discharge in the event of sudden flooding within the mine galleries. Designed for the Ermaden site’s high-altitude, high-humidity environment, Arken Generator's power solution met the requirements of operating at 35°C, 1000 meters altitude, and 90% humidity.

Tailored solution and key benefits

Arken specified two STAMFORD S7 alternators paired with a 1750kVA prime mover and a step-up transformer to achieve the necessary 15.8kV voltage. Key performance features, including STAMFORD’s CoreCooling™ technology, allow for high efficiency and enhanced thermal performance. This setup ensures reliability, increased power density, and reduced maintenance. The Ermaden Coal Mine’s unique environmental and access challenges required a customized approach, including a special coupling design tailored to meet Erdemir’s needs. Arken’s decision to work with STAMFORD | AvK was driven by the alternator’s proven durability, efficient fuel consumption, and consistent performance worldwide, all critical for demanding industrial applications.

With over a decade of partnership, STAMFORD | AvK’s technical expertise and support were integral to the project’s success. The seamless installation at Ermaden highlights Arken Generator’s capability to deliver bespoke solutions in challenging industrial environments, ensuring the continuous operation of essential systems.


 

Learn more about STAMFORD | AvK

The collaboration further strengthened our trust and partnership with STAMFORD | AvK as a reliable and efficient power solutions provider.

Arken Generator
Related case studies
Mining Generators Case Study

STAMFORD P7 alternators play a critical role in powering the Ambatovy Project, a landmark mining and processing development in Madagascar.