The particles and contaminants that we are trying to filter out are far smaller than can be seen with the naked eye, magnifying glass or even a low powered telescope.

What is a Micron?

The unwanted particles found in today’s DEF are measured in microns (μ). A micron is a unit of linear measure in the metric system used to measure distance from one point to another. A micron rating for DEF filtration is a generalized way of quantifying the ability of a filter’s media to remove contaminants of a particular size.

For example, a filter with a micron rating of “7” will filter out contaminants of 7 microns or larger and a filter with a micron rating of “3” will filter out contaminants of 3 microns or larger. Filter efficiency refers to a measurement of the filter’s retention efficiency. The measurement is typically the number of particles retained by a filter compared to the number of particles present in the DEF that will pass through the filter. A 7 micron filter with 98.7% efficiency rating removes 98.7% of the particles at or above the 7 micron size.

Proper Storage and Filtration of DEF is Critical

As the graphic below illustrates, the wide variance in filtration throughout the manufacturing and delivery process of DEF makes awareness of proper storage and filtration an essential part of your Selective Catalytic Reduction (SCR) aftertreatment system’s reliability and performance.

def process illustration

Case Study Actions

Cotton Seed Distributor chooses Cummins' reliable engines for pumping

View

Cummins 15-litre ISXe5 selected as standard for Matthews Transport

View

Farmer Cuts Cost with Cummins Genset Fuel Economy

View

世界の農業を支えるカミンズ―排ガス規制をクリアする農機用エンジン製造にも注力

View

Cummins CustomPaks

View


To view all case studies, click here.