The internal components of modern injectors are often extremely small and very susceptible to wear or sticking due to particles and other kinds of contamination. Wear of internal parts of the fuel system will decrease the life of the components and may even cause malfunctions that could result in severe damage to the other engine components.

Some common contaminants found in today's fuels include water, microorganisms, wax, hard particles, debris and other sediments.

Time

As with most things, time has an adverse affect on diesel fuel. The shelf life for diesel fuel is only six to twelve months but in extreme conditions, that time could be much shorter. Furthermore, the longer it is stored, the more opportunities will present themselves for contaminants to enter the fuel.

Weather

Other than water from rain or snow and dirt from the wind entering the storage tank, temperature and humidity have adverse affects. Warm moisture laden air coming in contact with cold diesel fuel or a cold tank can cause the water in the air to condense. The amount of water in the air, or humidity, can greatly affect the amount of water that is added to the fuel from condensation as the tank breaths. Also, warmer ambient temperatures can speed up the natural deterioration of diesel fuel. The composition of diesel fuel can vary dramatically depending on the region and temperatures. Fuel intended for warm weather will not store properly in cold weather.

Micro-organisms

Diesel fuel in a storage tank is a smorgasbord to many forms of micro-organisms. These bacteria and fungi live in the ever present water and feed off of the hydrocarbons found in diesel fuel. Their living and dead bodies are contaminants. Any opening, whether it is the fill port, ventilation or hole caused by damage, is an easy, direct path for contaminants to enter the fuel. Any damaged caps, seals or gaskets are also perfect opportunities for contamination.

Case Study Actions

Cotton Seed Distributor chooses Cummins' reliable engines for pumping

View

Cummins 15-litre ISXe5 selected as standard for Matthews Transport

View

Farmer Cuts Cost with Cummins Genset Fuel Economy

View

世界の農業を支えるカミンズ―排ガス規制をクリアする農機用エンジン製造にも注力

View

Cummins CustomPaks

View


To view all case studies, click here.