Truck driving alone in desert with mountain in the background
The power of choice

At Cummins, we are committed to empowering our customers with first-rate options to meet their needs. That's why we've expanded our portfolio and partnerships over time.

Cummins has been producing engines for more than 100 years, and we now offer complete powertrain solutions - from engine to transmission to axles - with every component working in harmony.

Why integrate?

With Cummins Integrated Power, the pieces fall into place.

Higher efficiency

By optimizing factors like gear and axle ratios, Cummins Integrated Power maximizes fuel economy. Further, the integrated, fuel-agnostic design reduces parts proliferation and OEM integration, thus improving the total cost of ownership.

Performance

Cummins engines offer superior horsepower ratings and productivity for their size. Our Cummins component businesses and partnerships, like Meritor and Eaton-Cummins, contribute top-of-the-line axles, transmissions, and other parts.

Lower emissions

As a growing Cummins HELM™ platform, Cummins Integrated Power puts our customers in the driver's seat to select the low or zero-emissions fuel that works best for them and the planet.

Ease of integration

With Cummins Integrated Power, customers can be confident that Cummins supports their entire powertrain and that they can get problems resolved with one call.

Product range:

2.8 - 15L

 

Engines for on-highway markets, globally

 

Long-haul | Vocation and bulk haul | Regional haul | Pick-up and delivery | School | Motor coach | Shuttle and transit

Today and tomorrow's solution

x15n natural gas engine
Heavy-duty engine

X15N

Discover the industries first big bore natural gas engine that delivers solutions for a range of long-haul applications. With power ratings up to 500 hp and torque up to 1850 lb-ft, this engine will revolutionize transportation and your application needs. The X15N is now available for purchase in North America

Learn more

next generation x15 fuel agnostic engine
Heavy-duty engine

EPA27 X15™

Introducing the next generation X15. The next step in the Cummins fuel-agnostic 15-liter platform. Offering up to 605 hp and 2,050 lb-ft torque, this engine demonstrates our continues commitment to the evolution of internal combustion technology.

Learn more

Brett Merritt speaking in an office building
Brett Merritt speaking in an office building

Innovation, technology, and services

Leap Ahead: Introducing Cummins HELM™ platforms

HELM is our industry fuel agnostic platforms strategy that is posed to help customers meet their sustainability goals and business needs. These platforms feature a series of engines that are derived from a common base.

Road surrounded by trees next to body of water

Going further, faster

Destination Zero™

It's our mission to power a more prosperous world. We do this by helping customers navigate the energy transition with our innovative and dependable products. 

Connect with us