""
Marine

Tom Aliotti: Designed and Built by Fishermen for Fishermen

by Alan Haig-Brown

Cummins Vessel Reference #814

Tom Aliotti’s new Bristol Bay boat on sea trials.

 

Tom Aliotti's new Bristol Bay gillnetter Mariola did 36 knots on sea trials. Asked the secret of getting that speed, he replied, "I'm not going to tell you my secret, except that I have fished Bristol Bay for 33 years and I use that knowledge to build boats for fishermen.
 

 

And the Mariola at rest.

 

Staying within the legally proscribed 32-foot limit for Bristol Bay gillnet boats creates a challenge that eager designers like Aliotti are happy to take on. "But it is not all about light boat speed," he explained, "It matters to me what speed you can maintain with the weight of fish onboard and how a boat performs in weather. There are compromises to be made and I can design and build to those."
 

 

Indy Walton putting the finishing touches on the Sniper’s name.

 

From that description, the discussion gets interesting as a client coming to Aliotti Enterprises for a new boat can tell Tom just what compromises he is interested in making and Tom can design to that desired balance. In the past few days, there have been two, near sister ships, launched into Bellingham Bay in anticipation of the June opening on Bristol Bay that will last for only six weeks.
 

 

A remarkably attractive and well laid out bridge.

 

Alioitti's hulls have a wide lift chine, but even there, he balances it to allow for a finer entrance at the bow. This is so that the boat won't pound when driving up against a nasty chop that summer winds can bring to the Bay. Aliotti built three boats this past winter. The same Cummins QSC8.3-liter engines, producing 493-HP each at 2650 RPM, power two of the three. These two boats have identical 15.5-foot wide hulls. But the drives, aft of the engines, have some differences.
 

 

Twin Cummins QSC8.3 liter 493 HP each at 2600 RPM, Britol Bay gillnetter, 32X15.5-feet

 

Both boats have ZF gears and Ultrajet, water-jet drives, Indy Walton's boat, Sniper, has Ultrajet 340 drives turned by ZF305 gears, and Aliotti's boat, the Mariola, has Ultrajet 340hd drives turned by ZF286 gears. "My drives are 1.5-inches bigger in circumference than Indy's drives," Aliotti said. The difference in performance, he explained, is pronounced. With 400 gallons of fuel onboard, both boats weigh about 28,000 pounds. On sea trials Walton's Sniper will likely clock 40 or more knots, in virtually identical trials, Aliotti's Mariola with the bigger jets did 36 knots.
 

 

Lift chines and fine entry.

 

Light boat sea trial speeds are important, but these are fishing boats and are designed to perform, ready to fish, at 28 to 30,000 pounds net weight. In addition, they can pack up to 30,000 pounds of sockeye salmon in their 13 individual RSW holds. The two boats will fish different regions of Bristol Bay, Walton in Naknek and Aliotti in Egegik, but the two regions put similar demands on the boats with a mix of distance, tide and wind. The most important factor is personal preference as to where speed matters. Aliotti feels a greater need for loaded speed. "I put 16,000 pounds of water on and still got up on the step and did 26-knots," he said.
 

 

Net guards on the stern allow the boat to back over a net.

 

Meanwhile, Walton, opting for a greater light boat speed, expects that he will still get up on the step and make good speed with 10,000 or even 12,000 pounds onboard. Building a boat that costs well north of $600,000 is done by fishermen with very particular expectations. "My boat interior is nicely finished and comfortable for a crew of five," explained Aliotti, "But if you want to see a really classy finish, take a look at the interior of Indy's boat."
 

 

Indy Walton admires his Cummins QSC8.3 liter engines each delivering 493 HP each at 2600 RPM.

 

Walton chose Aliotti to design and build his boat because of the strong framings system, with the frames only 28-inches apart with multiple stiffeners running fore and aft. With the engines, gears, jets and exhaust all set in place, Walton moved the Sniper over to Bellingham's Colony Wharf Coop where a team of gifted trades people did the detailed finishing The result is a spectacular boat from the carbon fiber dash cover in the wheelhouse to the carbon fiber lettering for the name and home port on the stern. An innovative design allows for a comfortable skipper's berth in the wheelhouse and a exceptionally clean finish to the walls with one-inch of insulation in the accommodation area with fridge, stove and private head. This, together with cargo holds and engine room is all fitted into a 32-foot hull.
 

 

Fast boat.

 

On deck, both boats have Kennimatics anchor winches and net drums. Asked about the apparently narrow (18-inch by six-foot net drum, "Walton says, "That allows me to set my net at 25 knots without getting a back lash."

 

Walton will fish with a crew of five including his 22-year-old daughter Bristol and 13-year-old son Dylan. “We bleed and float all of our fish in RSW to get about 25 cents additional per pound,” he explained, “The large crew allows us to do this even in heavy fishing.
 

The F/V Sniper showing her maneuvers.

 

This summer Walton's mom, wife, and another daughter will continue the family set-net operations while his son Dagen will take over his other boat, Double Dippin'. And so, in one of the world's most valuable, most intense and briefest fisheries, these two boats, that are possibly the best twin Cummins-powered, Bristol Bay jets, will join what is undoubtedly the world's most high-tech, small boat fleet.

 

 

For further information:


Tom Aliotti
Aliotti Enterprises
PO Box 32148
Bellingham, WA
Phone: 360 739 3770
E-mail: [email protected]

 

Indy R. Walton
43622 Sterling Hwy.
Suite B Soldotna, AK 99669
Mobile: 907 394 2663
E-mail: [email protected]

Joe Tobin
Marine Regional Sales Manager
Cummins Sales and Service
1030 SW 34th St., Suite A
Renton, WA 98057
Phone: 425 235 5400 | Extension: 3414
Mobile: 425 757 4220
E-mail: [email protected]

Related case studies
Marine Case Study

Trophy fish are measured by weight and length at the dock. They almost always exceed the size of the angler reeling them in. The exception would be M/V Chelsea ...

Marine Case Study

Greek passenger vessel repowers with Cummins.  Cruising to Symi on a water taxi is more than a boat ride across the Aegean Sea. Departing the eastern sh...

Marine Case Study

Crews with no choice but to head out to sea in rough weather conditions rely on trawlers' inherently robust, stout design based on the DNA of highly capable fis...