Требуется помощь: компании Cummins необходимы передовые идеи по снижению выбросов углекислого газа

Предприниматель Сэмюэл Уолкер из компании Interface выступает с предложением на конкурсе Innovation Gateway в Великобритании в 2017 г.
Предприниматель Сэмюэл Уолкер из компании Interface выступает с предложением на конкурсе Innovation Gateway в Великобритании в 2017 г.

A popular Cummins program in the U.K. that asks entrepreneurs to pitch their best ideas for reducing the company’s carbon footprint is coming to North America.

Программа Innovation Gateway ищет новые идеи, которые помогут компании Cummins достичь своих целей по уменьшению потребления воды, снижению количества отходов, оптимизации энергопотребления и утилизации материалов. Those judged to have the best proposals will advance to the gateway finals, 9 a.m. to 1 p.m. April 8 at the Columbus Commons, 300 Washington St., Columbus, Indiana (U.S.A.).

"This is our chance to listen to ideas we might not have considered to help us meet our goals," said Jim Gruwell, Executive Director of Strategic Purchasing at Cummins and a judge at the finals. "This initiative worked really well in the U.K. and I can't wait to see how it works here."

Innovation Gateway: Register Now and Submit Your Idea

Loosely inspired by reality TV shows where entrepreneurs and inventors pitch their ideas to potential investors, the gateway competition resulted in several initiatives that Cummins leaders in the U.K. have put into practice to help meet their environmental targets.

Judges confer in the Innovation Gateway
Antonio Leitao (center), Vice President of Cummins Europe Area Business Organization, listens to a presentation at the gateway initiative in the U.K. in 2017.

The winning ideas included capturing low gas waste heat from the engine testing process and converting it into energy that could be used on site, equipment to reduce water flow, implementation of a furniture refurbishment service and energy efficient hand dryers.

"We were really pleased with the ideas the gateway generated," said James Johnson, Cummins' Innovation Gateway Project Leader, who oversaw the initiative in the U.K. and is now leading the North American version. "It's really about powering environmental innovation through diversity in thought and partnership."

Cummins has established a special website where people can create an account and present their ideas in writing. Finalists will be notified by the company and the winners could end up becoming suppliers to Cummins, or pick up additional business if they already have a relationship with the company. People must sign up by March 15 to be eligible for the finals.

The company is asking for ideas with a connection to one or more of the following areas:
 
•    Materials management: Identifying solutions for moving waste streams up the hierarchy. 
•    Capture/recovery: Searching for ready- or near-ready to implement technologies that recover and capture energy and water to reuse. 
•    Controls:  Identify controls and systems that will help to reduce energy consumption. 
•    Manufacturing process efficiency: Identifying solutions and alternatives to improve the efficiency of manufacturing processes. 
•    Packaging: Seeking cost neutral, environmentally friendly packaging solutions that are alternatives to plastic and foam and also easily reusable and recyclable. Solutions with corrosion inhibitor capabilities are a bonus. 
•    Other Innovations

Judges for the North American gateway in addition to Gruwell include Brian Mormino, Executive Director of Worldwide Environmental Strategy and Compliance; Laura Jones, Functional Excellence Manager – Cummins facilities; Morgan Andreae, Executive Director of the Company’s Growth Office and Helena Hutton, Diversity Procurement Director at Cummins.

In addition, Dr. John W. Sutherland, the leader of Environmental and Ecological Engineering at Purdue University, and Eli Levine, leader of the Clean Energy Manufacturing Initiative at the U.S. Department of Energy, will also serve on the panel.

Not sure what the Innovation Gateway is all about? Check out this video on the project in the United Kingdom.

 

Предоставить общий доступ:
Блэр Клафлин директор по устойчивому коммуникаций

Блэр Клафлин

Блэр Клафлин является директором по устойчивому коммуникаций для КАММИНЗ Inc. Блэр присоединился к компании в 2008 году в качестве директора по коммуникациям по разнообразию. Блэр родом из газетного фона. Ранее он работал в Индианаполис-звезде (2002-2008) и в регистре Де-Мойн (1997-2002) до этого. [защищенный адрес эл. почты]

 

Делаем свою часть защиты земли

На заводе по производству двигателей на каменистой горе в Северной Каролине имеется система очистки воды, которая включает теплицу в качестве составной части процесса обработки.
На заводе по производству двигателей на каменистой горе в Северной Каролине имеется система очистки воды, которая включает теплицу в качестве составной части процесса обработки.

По мере того как мир празднует 50-ую годовщину дня земли на этой неделе, вот четыре способа, по которым Камминс работает над сокращением своего влияния на окружающую среду.

Эти четыре шага не являются единственными мерами, которые компания приняла, но они являются четырьмя существенными шагами, чтобы быть уверенными:

Председатель и главный исполнительный директор том Лайнбаргер раскрывает экологическую стратегию компании PLANET2050.
Председатель и главный исполнительный директор компании том Лайнбаргер раскрывает стратегию PLANET2050 в области охраны окружающей среды.

1. ЭКОЛОГИЧЕСКАЯ СТРАТЕГИЯ PLANET2050

<А> PLANET2050 стратегия , выпущенная в конце 2019 г., устанавливает для компании цели по снижению выбросов парниковых газов на основе научных данных (ПГ), приуроченная к 2030 года, и 2050 стремление к снижению влияния Камминса на экологические проблемы, такие как изменение климата. Цели, которые заменят текущие 2020 цели, включают в себя сокращение выбросов углекислого газа (CO2) на 300 000 000 метрических тонн и сокращение выбросов летучих органических соединений (Лос), начиная с лакокрасочных и лакировочной деятельности, на 50%. Научно-основанные на 2030 цели превосходят цели, установленные в соглашениях Организации Объединенных Наций по климату в Париже. Компания КАММИНЗ рассчитывает на углеродно-нейтральное положение 2050.

2. ЭКОНОМИЯ ВОДЫ

Успехи в области сохранения водных ресурсов являются одним из самых больших успехов в экологических задачах компании, срок действия которых истекает в 2020 году. Приблизительно 1 000 000 000 галлонов водопользования удалось избежать с 2010 года за счет природоохранных усилий компании, которые варьировались от относительно простых шагов до использования сложных технологий, что снижает количество воды, используемой для охлаждения двигателей большой грузоподъемности во время испытаний, и улавливать энергию, которую эти двигатели производят для повторного использования на заводах Камминза. Теперь, компания экспериментирует с ультрасовременными системами очистки воды, которые включают в себя такие вещи, как теплицы, обильные с жизнью растений, чтобы помочь фильтровать воду для повторного использования.

3. ЭКОНОМИЯ ЭНЕРГИИ

Кроме того, компания Камминз успешно сберегать энергию, которую он использует в своих 2020 целях. Компания сократила энергоемкость, количество используемой энергии, скорректированной на отработанный рабочий час, более чем на 30% с 2010 года. Компания КАММИНЗ предприняла такие шаги, как замена старых огней на светодиодное освещение, и более старые воздушные компрессоры с более эффективными моделями в дополнение к шагам, указанным в пункте No 2, для улавливания энергии, вырабатываемой крупными двигателями в испытательных ячейках. Компания также обучила сотрудников поиску оборудования и процессов на своих заводах на дому, которые можно было бы улучшить с точки зрения энергетики. Между тем, выбросы парниковых газов Камминса, скорректированные на отработанных часов, снизились на 6% в 2018 году по сравнению с предыдущим годом. Ожидается, что данные за 2019 в ближайшее время будут опубликованы.

Расширение ветропарка Медоу-Лейк
Расширение Медфермы лугово-Лейк-направление возобновляемых источников питания для энергосети.

4. ОХВАТЫВАЯ ВОЗОБНОВЛЯЕМУЮ ЭНЕРГИЮ

Компания сделала значительные инвестиции в <а> солнечная энергия , с солнечными установками завершены или ведутся на более чем двух десятков мест, включая 650 000 квадратных футов массивов, установленных в 2016 году в верхней части Пекина Foton КАММИНЗ компании в Пекине, Китай, который выдает около 15% от потребностей здания электроэнергии. Компания также поддержала расширение 2018 <а> в Индиане на ветряной ферме за счет договора купли-продажи электроэнергии в виртуальной реальности. Он почти отправит в энергосети достаточно возобновляемых источников энергии, чтобы компенсировать все электричество, которое компания использует на всех своих объектах в штате. Поощрение использования и развития возобновляемых источников энергии является одной из 2020 экологических целей компании.

Предоставить общий доступ:
Блэр Клафлин директор по устойчивому коммуникаций

Блэр Клафлин

Блэр Клафлин является директором по устойчивому коммуникаций для КАММИНЗ Inc. Блэр присоединился к компании в 2008 году в качестве директора по коммуникациям по разнообразию. Блэр родом из газетного фона. Ранее он работал в Индианаполис-звезде (2002-2008) и в регистре Де-Мойн (1997-2002) до этого. [защищенный адрес эл. почты]

 

Глобальная Командная работа обеспечивает маскировную маску для сотрудников компании КАММИНЗ в Китае

Сотрудники компании КАММИНЗ в Шанхае стоят перед одной из партий масок.
Сотрудники компании КАММИНЗ в Шанхае стоят перед одной из партий масок.

Поставив свои рабочие навыки на работу, сотрудники Камминза из Йоханнесбурга в Колумбус, штат Индиана, вскочил в действие в прошлом месяце и закупил более 500 000 Защитные маски для своих коллег сотрудников в Китае.

Жители Китая должны носить дыхательные маски, когда они находятся на публике в качестве первой линии обороны к распространению нового коронавируса. Более 90 000 человек в более чем 65 странах были инфицированы вирусом, и более чем 3 000 умерли.

"Многие коллеги по всему миру оказали большую поддержку в оказании помощи нам источника масок и неустанно вождения на окончательное решение этой неотложной просьбой". Саид Стив Чэпмен, вице-президент группы КАММИНЗ, Китай и Россия.

«Закупки маски 500 000 FFP2 не только обеспечивают защиту здоровья и безопасности наших сотрудников, но и помогают нам устранить одно из основных препятствий для обеспечения непрерывности деловой деятельности в Китае»,-добавил Чэпмен.

Группы, находящиеся в КАММИНЗ, включая непрямые закупки и производственные группы в рамках Организации, компании, занимающихся цепочкой поставок, а также глобальные операции по распространению бизнеса, агрессивно обратились к потенциальным поставщикам и выделили другие ресурсы для решения этой проблемы для своих коллег в Китае.

Несмотря на то, что группа успешно обеспечила некоторые заказы из США, Великобритании и нескольких других стран, все еще существовал огромный разрыв между спросом и предложением, необходимыми для возобновления работы и защиты более чем 12 000 сотрудников Камминза в Китае.

Энни Чу и Юецянь Чжан сыграли ключевую роль в приобретении масок.
Энни Чу (слева) и Юэцянь Чжан (справа) сыграли ключевую роль в приобретении масок.

ПОВОРОТНЫЙ МОМЕНТ

Переломный момент наступил в Южной Африке. После получения срочных запросов от своих коллег в Китае, Африка и регион Ближнего Востока бизнес-организации сразу же мобилизованы. Энни Чу и Юэцянь Чжан в Йоханнесбурге провели выходные в поисках поставщика. В феврале 2 г. они успешно обеспечили защиту 500 000 FFP2 масок.

Однако поставщик обратился с просьбой о немедленном платеже, что сделало этот процесс еще более актуальным. Сотрудники компании в Китае и Африке работали с корпоративными цепочками поставок, Финансировками и другими функциями круглосуточно для решения бизнес-задач при соблюдении всех норм и требований.

Первая партия 160 000 маски прибыла в Шанхай февраля 8, и в феврале 14, все оставшиеся маски прибыли. Маски сыграли важнейшую роль в возобновлении бизнеса во многих операциях Китая Камминза. Трансграничная Командная работа продолжается по мере того, как еще один набор масок готовится для отправки в Китай.

«Для нас было большой честью быть в том положении, когда мы могли сделать что-то, чтобы помочь, и я очень горжусь самоотверженностью и самоотверженностью наших сотрудников в Африке и на Ближнем Востоке и большим сотрудничеством между ними и нашими коллегами в Китае»,-сказал Тьерри Пимы, Исполнительный директор Организации по вопросам бизнеса в Африке и на Ближнем Востоке.

РАБОТА В КОМАНДЕ НИКОГДА НЕ ПРИСУТСТВУЕТ

Командная работа на этом не остановилась. Многие группы сотрудников компании по Камминным вопросам также мобилизуют свои силы для получения пожертвований для физических лиц в пострадавших регионах. Например, Китайская ассоциация Колумбуса, ресурсная группа сотрудников группы стран Восточной Азии и многие другие изучили различные возможности источника и пожертвования масок и других предметов. В результате этих усилий 10 000 масок были успешно отправлены сотрудникам и местным общинам в Ухане и Сянъяне.

Кампания по закупке масок еще раз продемонстрировала, что командную работу не просто говорят на КАММИНЗ. Он введен в действие каждый день, чтобы создать сильную компанию и сильные сообщества во всем мире.

 


 

Предоставить общий доступ:
Офисное помещение КАММИНЗ

Cummins Inc.

КАММИНЗ является глобальным лидером в области энергоснабжения, проектирует, изготавливает, продает и предлагает дизельные и Альтернативные топливные двигатели от 2,8 до 95 литров, дизельное топливо и альтернативные работающие электрические генераторные установки мощностью от 2,5 до 3 500 кВт, а также сопутствующие компоненты и технологии. Компания КАММИНЗ обслуживает своих клиентов через свою сеть 600 принадлежащих компании и независимых дистрибьюторов, а также более 7 200 дилерских центров в более чем 190 странах и территориях.

Завод, который опередил свое время

Пекин Фотон КАММИНЗ компания использует технологии для улучшения целого ряда проблем, от качества до удовлетворенности клиентов. Руководство завода, слева направо, включает в себя Чжао он, руководитель по производству инженерных наук; Мигель Киндлер, директор по заводской установке; Чэнь Хуа, Генеральный директор; и тишина Чэнь, IT-лидер.
Пекин Фотон КАММИНЗ компания использует технологии для улучшения целого ряда проблем, от качества до удовлетворенности клиентов. Руководство завода, слева направо, включает в себя Чжао он, руководитель по производству инженерных наук; Мигель Киндлер, директор по заводской установке; Чэнь Хуа, Генеральный директор; и тишина Чэнь, IT-лидер.

Пекинская Компания по производству двигателей в Пекине FOTON (BFCEC) настолько соединена с высокотехнологичными инструментами, что она может практически определить дефекты определенных задач и узких мест в производственной сфере до того, как они произойдут.

Сеть датчиков, связанных с Интернетом, искусственным интеллектом, передовыми аналитикой и другими изменениями, меняет то, как работает завод. Производство вверх. Качество вверх. И клиенты тоже довольны.

Поэтому неудивительно, что этот завод был назван в прошлом месяце Всемирной сетью маяка Всемирного экономического форума, элитным списком лидеров в области применения технологий, которые некоторые называют 4-й промышленной революцией.

«Это признание демонстрирует надежность передовых производственных и управленческих концепта Камминса»,-сказал Чэнь Хуа, Генеральный директор Foton-КАММИНЗ, который производит более 250 000 двигателей в год. «Наши усилия по цифровизации цепочек поставок и смарт-производству не только помогают повысить эффективность наших предприятий, но и обеспечивают оптимальное качество наших заинтересованных сторон».

Пекинский Завод по производству двигателей в Пекине Фотон КАММИНЗ
Пекин Фотон КАММИНЗ компания представляет собой массивный, двух-строительный объект на окраине столицы Китая и крупнейший город. Это совместное предприятие между компанией "КАММИНЗ" и "Foton Motor". Солнечный массив на одном здании генерирует около 15% от его потребностей в электроэнергии.

РЕДКАЯ ЧЕСТЬ

BFCEC была одной из 18 компаний, добавленных к сети маяк в январе, присоединившись к 26 объектам, ранее названным в списке. Более 1 000 компаний из различных отраслей по всему миру были оценены по поводу обозначения маяка, который управляется для форума компанией Маккинси и компания, Глобальная консалтинговая фирма в области управления.

"Изготовление часто является отправной точкой для инновационной новой, всей компании, работающей на основе новейших технологий, для достижения новых уровней устойчивости, маневренности, скорости на рынке и производительности",-сказал Энно де Бур, партнер и лидер мировой производственной практики компании "Маккинзи". "Это значение не останавливает заводскую дверь; Вместо этого, маяки находят влияние на всю цепочку создания ценности, от поставщиков до клиентов».

На форуме говорится, что глобальная сеть маяк, созданная в 2018 году, служит «платформой для разработки, тиражирования и расширения масштабов инноваций, создания возможностей для кросс-компании в области обучения и сотрудничества, а также для установки новых контрольных показателей для глобального производственного сообщества».

Члены сети отражают удивительный потенциал 4-й промышленной революции, также иногда именуемой индустрией 4,0, которая включает в себя все, начиная от совместных роботов и заканчивая искусственным интеллектом, дополненной реальностью, передовыми аналитикой и улучшенной интеграцией между информационными технологиями и производственными операциями.

МОЩНОСТЬ ТЕХНОЛОГИИ

BFCEC, совместное предприятие между КАММИНЗ и китайской крупнейшей коммерческой автомобильной компании, FOTON Motor, буквально предлагает заглянуть в будущее промышленного производителя. И его влияние простирается далеко за пределы массивного двухэтастроительного кампуса на окраине столицы Китая и крупнейший город.

Вот один небольшой пример того, что происходит в BFCEC. Утечки масла, вызванные неисправным герметизации металлических сковородок, могут быть основной головной болью для производителей и клиентов, так. Объединяя искусственный интеллект, Специальные камеры и информационные технологии, система на заводе в ФотоНе-КАММИНЗ автоматически определяет качество уплотнения поддона и может отклонить его для дальнейшего использования в том случае, если оно не проходит проверку. Требования в отношении неисправного уплотнения сковородок сведены к нулю.

В целом, ежемесячные требования к качеству на BFCEC вниз 40% по сравнению с 2017 и идентификация ложных претензий составляет 300%. Среднее количество претензий на двигатель вниз почти на 70%. Производительность составляет более 40%.

За пределами завода клиенты видят, что их уровень потребления топлива повышается примерно на 5% и в течение времени, количество времени, которое двигатель остается в обслуживании, возросло примерно на 10%.

Что дальше

Пожалуй, самое удивительное в изменениях в BFCEC в том, что есть возможности для совершенствования. Объем собираемых данных постоянно увеличивается, что может помочь в проведении анализов, необходимых для поиска большей эффективности. Сотрудники завода также считают, что еще одна треть завода все еще может быть оцифрована.

Как часть надежной стратегии, чиновники компании КАММИНЗ инвестируют в аналогичные технологические достижения заводов по всему миру, поскольку промышленность 4,0 формируется на предприятии. Например, компания КАММИНЗ, как ожидается, закончится 2019 с около 30 совместных роботов совместного пространства с человеческими сотрудниками в более чем десятка пунктов. Они часто выполняют самые повторяющиеся задачи, улучшая здоровье и безопасность сотрудников в дополнение к эффективности.

Чэнь Хуа говорит, что он рад поделиться тем, что было изучено в БФКЕ, в то время как 4-я промышленная революция расширяется. Он говорит, что он имеет потенциал для увеличения производства, повышения качества, повышения безопасности и сокращения отходов.

«Мы надеемся, что наш успех вместе с промышленностью 4,0 станет стимулом для отрасли в области будущего производства»,-сказал он.

Включает в себя репортаж Дианы Чжао.


 

Предоставить общий доступ:
Блэр Клафлин директор по устойчивому коммуникаций

Блэр Клафлин

Блэр Клафлин является директором по устойчивому коммуникаций для КАММИНЗ Inc. Блэр присоединился к компании в 2008 году в качестве директора по коммуникациям по разнообразию. Блэр родом из газетного фона. Ранее он работал в Индианаполис-звезде (2002-2008) и в регистре Де-Мойн (1997-2002) до этого. [защищенный адрес эл. почты]

 

Компания КАММИНЗ присоединяется к ценным 500 для содействия включению в инвалидность

Компания КАММИНЗ уже давно считает, что разнообразие является основой успеха для бизнеса.
Компания КАММИНЗ уже давно считает, что разнообразие является основой успеха для бизнеса.

Компания КАММИНЗ берет свою повестку дня в сфере разнообразия и инклюзивности на новый уровень, присоединившись к ценным 500 вместе с одними из самых влиятельных предприятий в мире.

Созданная социальным предпринимателем и активисткой Кэролайн Кейси, <а> ценным 500 ставит своей целью поставить инвалидность на повестку дня глобального руководства бизнесом.

Бизнес-лидеры во всем мире делают твердые и осязаемые обязательства по искоренению отчуждения инвалидов в бизнесе. Members span 24 countries, reaching more than 9.3 million employees.

«Мы рады продемонстрировать свою приверженность делу включения в список инвалидов, присоединившись к ценным 500»,-сказал Деннис Хитфилд, Исполнительный директор Камминса, люди с ограниченными возможностями и ветераны. «Это один из многих шагов, которые мы предпринимаем для создания более инклюзивных рабочих мест и сообществ для людей с ограниченными возможностями. Будучи частью ценного 500 предоставляет уникальную платформу для Камминс, чтобы узнать от и внести вклад в глобальное сотрудничество, которое вяжет вместе других транснациональных корпораций с унифицированных миссии, чтобы сделать мир более инклюзивным местом для людей с ограниченными возможностями ".

Логотип для ценного веб-сайта 500
Ценные кампании 500 поддержаны лидерами бизнеса во всем мире.

Представленная на ежегодном совещании Всемирного экономического форума в январе 2019 года, ценная кампания 500 впервые была обсуждена на главном этапе встречи при поддержке глобальных бизнес-лидеров.

Кампания поддерживается несколькими мировыми лидерами бизнеса и партнерами, в том числе полом Полманом, бывшим главным исполнительным директором компании Unilever и Председателем ценного 500; Основатель Virgin сэр Ричард Брэнсон; Директор по операционным вопросам Virgin Media Джефф Доддс; Председатель Блумберга Петер Грауэр; Глобальный Председатель и главный исполнительный директор EY Кармин Ди Сибио и стратегические партнеры Omnicom и Virgin Media.

«Нам необходимо 500 национальных и многонациональных корпораций частного сектора для того, чтобы они оказались переломными для изменений и для раскрытия деловой, социальной и экономической ценности людей, живущих с ограниченными физическими возможностями во всем мире», ценных состояний 500 на своем веб-сайте. "Because the potential of 1.3 billion should not be ignored."

Кроме Камминза, к этой инициативе присоединились и другие компании: Проктер энд Гэмбл, IBM, Бэй, Total, Герберт Смит, Спектерами, Эли Лилли и компания Deutsche Bank в Великобритании, АРЗ, Adobe, ПВХ, Hilton и Perrigo.
 

Предоставить общий доступ:
Лорен О'делл Сидлер-КАММИНЗ Inc.

Лорен О'делл Сидлер

Как старший специалист по коммуникациям с компанией "Камминз Инк.", Лорен О'делл Сидлер работает с лидерами компании по разработке и внедрению коммуникационных стратегий, которые достигают глобальную аудиторию камминза.

Перенаправление на
cummins.com

Информация, которую вы ищете, находится в
cummins.com

Мы запускаем этот сайт.

Спасибо!