Cummins Home Generators

Home Standby and Portable Generators

Cummins is the brand homeowners trust for reliable, durable and powerful home standby power. Com um gerador doméstico ou portátil da Cummins, a sua família não vai ficar no escuro.

Do I need an installed home standby generator or a portable generator?

Your natural gas-, propane-, or diesel-fueled standby generator delivers power quietly and automatically during a power outage. A Cummins gasoline-powered portable is easy to move so you'll always have power where and when you need it. This chart can help you determine if an installed whole house generator or a portable generator is best for you.

 

  Cummins Standby Generator Cummins Portable Generator
Aplicações Backup power to keep your home running when utility power goes out Emergency home power, camping, tailgating, outdoor events and more
Combustível Fueled by your home's natural gas or liquid propane line. No refueling required Run on gasoline or liquid propane, depending on model
Manutenção Automatic maintenance and remote system monitoring Regular maintenance intervals recommended for readiness and long life
Start-up Switches on automatically when utility company power goes out Must be connected and switched on manually

How much generator power do I need?

 

What appliances and necessities can you run with a home standby or portable generator? You can use our Home Generator Sizing Calculator to determine the size that's right for you.

 

Evaluate Your Home Generator Needs

 

The size of your generator depends on how much power you need. The power you need is driven by the essentials you want to power during an outage.

The list below details what a few popular generator sizes can power. For simplicity, these examples use approximate power needs of appliances. The actual power consumption of your appliances could vary.

 

Here's a general guide to what you can power with different size generators:

what-appliances-with-generator-sizes.JPG

What can a 9,000-watt generator power?

This range of power needs mean you can probably use a portable generator instead of a whole house generator. A 9,000-watt portable generator can run one of the following combinations, but not both at the same time:

  • Refrigerator, microwave oven, electric stove and dishwasher, OR
  • Central AC in smaller homes, washing machine and iron

 

What will a 13,000-watt generator run?

This size generator is a great entry level generator to power rooms of your choice. A 13,000-watt generator could power all the following basic amenities:

  • Central air conditioner
  • Electric water heater
  • Gas furnace
  • Electric garage door
  • Refrigerator
  • Freezer
  • Microwave

 

What can you run with a 20,000-watt generator?

A 20,000-watt home standby generator is ideal for powering the whole house through an outage, especially if you have a larger home or longer outages. A 20,000-watt generator could power the following essentials in addition to the list above.

  • Dishwasher
  • Washer
  • Dryer (Electric)
  • Cooktop (Gas or Electric)

A informação é potência

Junte-se a dicas, ofertas e promoções de preparação meteorológica e interrupções de energia, ofertas de novos produtos e atualizações remotas do software de monitoramento.

Redirecionando para
cummins.com

As informações que você está procurando estão no
cummins.com

Estamos disponibilizando esse site para você agora.

Obrigado.