Additional Factors to consider
Precious Metal Content is Critical
The right amount of precious metal content and correct distribution throughout the filter are critical. The will-fit DPFs tested did not meet Cummins standards. This creates significant consequences downstream in the SCR portion of the aftertreatment system, including the potential to trigger fault code lamps and increased consumption of Diesel Exhaust Fluid (DEF).
A Minimum of $1,400 Saved in Total Cost of Operation
Owners can plan on buying two will-fit DPFs versus one Genuine Cummins product. At today’s prices, that would cost about $3,400 versus $2,000 for the Genuine Cummins DPF. That’s roughly $1,400 extra for the DPFs alone. Downtime, missed deliveries, reduced fuel efficiency and labor costs all add even more.
We've Got Your Back
A product is only as good as the company that stands behind it. Genuine Cummins DPFs are backed by North America’s largest and most capable parts and service network, with over 3,500 authorized locations. So no matter where the next load takes you, rest assured that there’s a nearby Cummins facility.