Cummins fuel-agnostic engine platform delivers low-to-zero carbon fuel capability

Las Vegas, NV (U.S.)
Hydrogen engine

Heavy-Duty Hydrogen, Natural Gas And Advanced Diesel Engines To Align With Tier 5

Cummins Inc. (NYSE: CMI) showcased its new fuel-agnostic 15-liter engine platform with hydrogen, natural gas and advanced diesel engines offering low-to-zero carbon fuel capability. The next generation engine is designed to accelerate the decarbonization of heavy-duty off-highway applications. 

“Cummins’ all-new platform takes internal combustion to a new level, capable of meeting future ultra-low emission standards, such as EPA Tier 5 and EU Stage 6, together with a low-to-zero carbon fuel capability to help put construction and quarrying sites on a lower cost path to decarbonization,” said Antonio Leitao, VP Global Off-highway Engine Business. 

The new engine is a clean sheet design that points to the future of diesel: more capability with less environmental impact.  Its high power density sets the standards for heavy-duty performance in key off-road applications including excavators, wheel loaders, drilling rigs, road planning, milling machines, haul trucks and air compressors.  Innovatively designed hardware provides lower weight with maximum engine durability, even when working on the most challenging jobs

The fuel-agnostic architecture of the 15-litre platform utilizes a common base engine with cylinder heads and fuel systems specifically tailored for it to use carbon-free hydrogen or biogas with up to a 90 percent carbon reduction. Cummins’ 15-liter hydrogen has ratings up to 530 hp (395 kW) and natural gas up to 510 hp (380 kW). The advanced diesel version can use either sustainable HVO fuel or biodiesel with ratings up to 650 hp (485 kW) for the most demanding off-highway duty-cycles. 

“The 15-liter has a significant increase in power density with a more compact installation envelope providing equipment manufacturers with the capability to do more with their machines,” added Leitao.

A key design feature of the new platform is a Double-Overhead-Camshaft (DOHC) realizing significant advances in combustion and thermal efficiency. Friction losses across the engine design have also been reduced and a sculpted block contributes to weight saving. The DOHC design also enables a more efficient integral engine brake to be accommodated.

 

Next Generation 15-Liter Engine

The 15-liter hydrogen engine with direct-injection, lean-burn combustion will be available with ratings from 400-to-530 hp (298-395 kW) and a peak torque of 2600 Nm. Running on zero-carbon green hydrogen, it can use a 700-bar pressure high-capacity fuel storage system for maximum operating hours between refueling.

The 15-liter advanced diesel features Cummins latest XPI ultra-high pressure fuel injection system and will offer a broad power range of 450-to-675 hp (335-503 kW) with an impressive 3000 Nm peak torque. Using B100 biodiesel enables up to a 70 percent reduction in carbon and using HVO renewable fuel achieves up to a 90 percent reduction. 

For applications powered by renewable biogas, the 15-liter natural gas will offer ratings extending from 400-to-510 hp (298-380 kW) with a peak torque of 2500 Nm available. Very low noise is a further benefit of this engine, particularly for when operating in urban areas.

“Moving forward, our aim is to offer the same agnostic capability across the next-generation of our current 6.7 liter and 9 liter engine platforms,” concluded Leitao. 

About Cummins Inc.

Cummins Inc., a global power technology leader, is a corporation of complementary business segments that design, manufacture, distribute and service a broad portfolio of power solutions. The company’s products range from internal combustion, electric and hybrid integrated power solutions to components including filtration, aftertreatment, turbochargers, fuel systems, controls systems, air handling systems, automated transmissions, electric power generation systems, microgrid controls, batteries, electrolyzers and fuel cell products. Headquartered in Columbus, Indiana (U.S.), since its founding in 1919, Cummins employs approximately 73,600 people committed to powering a more prosperous world through three global corporate responsibility priorities critical to healthy communities: education, environment and equality of opportunity. Cummins serves its customers online, through a network of company-owned and independent distributor locations, and through thousands of dealer locations worldwide and earned about $2.2 billion on sales of $28.1 billion in 2022. 

Media Contact
Redirecting to
cummins.com

The information you are looking for is on
cummins.com

We are launching that site for you now.

Thank you.