Cummins B6.7 reduces running costs and CO2 emissions with stop-start capability

Darlington, UK
Cummins B6.7 Performance Series with stop-start capabilities
The latest Cummins B6.7 Performance Series engine not only meets EU Stage V, but it features stop-start capability.

Cummins Inc. (NYSE: CMI) announces the latest B6.7 Performance Series engine not only meets EU Stage V, delivering near-zero emission levels of NOx and PM, but it features stop-start capability which can help operators further reduce running costs, as well as their environmental impact, through lower noise and CO2 emissions.

Jeremy Harsin, Cummins Off-Highway Business Director said, "Stop-Start capability is included in the B6.7 to further cut fuel consumption as well as overall maintenance costs. Fuel savings should be between five and 10% but could be higher based on the machine duty cycle. This feature also delivers the sociability benefits that contractors are looking for by reducing on-site noise and exhaust emissions. Improving fuel efficiency reduces CO2 greenhouse gas emissions." 

Stop-start has been integrated into the B6.7 platform with both hardware and software changes. Specially developed bearings in the engine, along with upgrades to the flywheel ring gear and starter motor, ensure long life and reliable performance with frequent starts. The engine system was thoroughly tested to confirm its durability for the rigors of stop-start operations.

Cummins engineers work closely with the OEM customer to integrate the engine electronic control module (ECM) software with the OEM’s machine controller software. The OEM controller monitors the machine operation and communicates to the ECM when it is appropriate and safe for the machine to shut off. The ECM monitors engine parameters such as coolant temperature, intake manifold temperature, engine load, and fan operation to make sure it is safely able to shut down. When all criteria are met, the engine will stop. The machine controller will then request an engine restart when required, and the ECM automatically restarts the engine to continue working. 

"Many machines sit idling on construction sites for long periods in between tasks. Stop-start not only reduces running costs, it lowers running hours for the machine, helping maintain higher residual values," added Harsin. 

The six-cylinder B6.7 engine is available from 116-243 kW (155-326 horsepower) with a high peak torque of 1375 Nm. With a low weight and compact size, it delivers a high-power density that enables it to replace engines of higher displacement with no impact on machine operation. This supports machines needing higher-speed power delivery, with low-end torque capability for transient performance benefits. Equipment manufacturers can use the B6.7 to improve machine capability and offer more value to their customers.

The B6.7 engine is combined with the Cummins Single Module™ after-treatment system to meet and exceed the ultra-low emissions levels demanded by Stage V. The efficient SCR technology means cooled exhaust gas recirculation (EGR) is not needed on the engine. Having no EGR means the engine is lower weight and has a simpler design, allowing for easier installation into equipment; together with lower cooling requirements. The simpler configurations also mean better reliability, reducing the total cost of operation and boosting availability. 

This product is ideal for use in a range of off-road equipment including crushers, screeners, wheel loaders, excavators, fork-lift trucks, terminal tractors, and empty container handlers. It can be tailored by Cummins engineers mechanically and electronically to each machine type. This powertrain integration capability delivers the best all-around performance and running costs to match the required operating cycle.

 

About Cummins Inc.

Cummins Inc., a global power leader, is a corporation of complementary business segments that design, manufacture, distribute and service a broad portfolio of power solutions. The company’s products range from diesel, natural gas, electric and hybrid powertrains and powertrain-related components including filtration, aftertreatment, turbochargers, fuel systems, controls systems, air handling systems, automated transmissions, electric power generation systems, batteries, electrified power systems, hydrogen generation and fuel cell products. Headquartered in Columbus, Indiana (U.S.), since its founding in 1919, Cummins employs approximately 57,800 people committed to powering a more prosperous world through three global corporate responsibility priorities critical to healthy communities: education, environment and equality of opportunity. Cummins serves its customers online, through a network of company-owned and independent distributor locations, and through thousands of dealer locations worldwide and earned about $1.8 billion on sales of $19.8 billion in 2020. Learn more at cummins.com.

Cummins Information

 

 

Media Contact
Redirecting to
cummins.com

The information you are looking for is on
cummins.com

We are launching that site for you now.

Thank you.