Cummins continues to power Bustech with new battery electric and fuel cell electric powertrains

Columbus, Indiana
Cummins and Bustech announce partnership to build battery electric and hydrogen busses

Cummins and Bustech will build the next-gen Bustech XDi low floor transit bus using Cummins zero-emission battery electric and hydrogen fuel cell technology

Production will ramp up in late 2021 and early 2022

Cummins will also provide local service to customers through its company-owned distributor network, one of the largest in Australia

Cummins Inc. (NYSE: CMI) and Bustech, Australia’s largest supplier of transit buses designed, engineered and manufactured in Australia, announced an agreement to build the next generation Bustech XDi low floor transit bus using Cummins zero-emission battery electric and hydrogen fuel cell technologies. The agreement provides for initial units to be developed for both battery electric and fuel cell electric, with plans to ramp up production in late 2021 and early 2022, respectively.

“We are excited to continue working with Bustech to provide the next evolution in clean, dependable solutions from Cummins,” said Amy Davis, President of New Power at Cummins. “Our ability to offer a full portfolio of solutions, allows our customers to seamlessly transition to one of several decarbonized solutions depending on their needs and specific use case. With a global support and service network already established, we’re equipped to support customers as they integrate zero-emission vehicles into their fleets.” 

“We have leveraged Cummins diesel technology for many years to produce over 500 integrated chassis, and now we are excited to work together to deliver the next evolution of the platform,” said Christian Reynolds, group managing director at Bustech. “With technology evolving rapidly and a long vehicle lifecycle, we know customers need a vehicle architecture that provides commonality but allows them to adapt. We are focused on value for money and total cost of ownership.”

The Battery Electric System from Cummins debuted in 2019 after extensive development, testing and validation. Cummins battery packs, which form an integral part of the battery electric powertrain, are designed and built by Cummins. The batteries feature a lightweight enclosure and flexible energy dense modules, all controlled by a proprietary battery management system (BMS) to keep the packs operating at maximum performance. Within the system, the packs can be scaled from 444 kWh to 518 kWh. The battery electric powertrain for Bustech will have a range up to 350 km between recharging.   

The Cummins fuel cell electric powertrain will maintain a large amount of commonality with the battery electric system and will be built on the same chassis from Bustech. Cummins, which acquired Hydrogenics Corp. in 2019, will combine Cummins proprietary batteries with its 90kW proton exchange membrane (PEM) fuel cell to provide a 450-600 km range based on various on-board hydrogen storage options. 

“Cummins shares our philosophy of building a vehicle platform to ease the transition to zero emission vehicles. An operator can select the best energy solution for a route, taking advantage of the unique properties of the battery and hydrogen powered vehicles. The updated XDi architecture simplifies mixed fleet vehicle maintenance through the quantity of shared components,” said Gregg Dinning, chief technology officer of Bustech. “Leveraging Cummins knowledge of zero-emissions technology and powertrain operation in Australia enables Bustech to deliver a vehicle that is optimized for Australian conditions from conception.”

To support Bustech’s XDi zero-emission products, Cummins will provide local service to customers through their company-owned distributor network, one of the largest in Australia supporting the bus market. Cummins has over 35 branch locations in Australia and New Zealand, and more than 6,000 dealer and distributor locations globally. The electric and fuel cell powertrain components will be manufactured in the United States, with final assembly and integration into the buses taking place in Australia. 

“We’re excited to strengthen our already strong relationship with Bustech, allowing our mutual customers to experience the journey to zero emissions with partners they know and trust,” said Chris Bowerman, bus and coach business manager for Cummins South Pacific. “Being able to offer customers everything from Euro 6 clean diesel, to battery electric and hydrogen fuel cell electric within one bus, should create confidence that we can provide the best-fit solution for each customer’s unique needs.” 
 

About Bustech

BustechBustech is Australia's largest privately-owned bus manufacturer. Bustech is 100% Australian owned and operated and is based in Burleigh Heads on Queensland's famous Gold Coast. Bustech designs, engineers and manufactures chassis' and bodies for mass passenger vehicles. Bustech has established facilities in Queensland and South Australia, with a production capacity of 400 buses per annum and also has a joint venture arrangement in Tasmania, supplementing the overall capacity for the group by 100 per annum, respectively.

About Cummins Inc.

Cummins Inc., a global power technology leader, is a corporation of complementary business segments that design, manufacture, distribute and service a broad portfolio of power solutions. The company’s products range from internal combustion, electric and hybrid integrated power solutions and components including filtration, aftertreatment, turbochargers, fuel systems, controls systems, air handling systems, automated transmissions, electric power generation systems, microgrid controls, batteries, electrolyzers and fuel cell products. Headquartered in Columbus, Indiana (U.S.), since its founding in 1919, Cummins employs approximately 59,900 people committed to powering a more prosperous world through three global corporate responsibility priorities critical to healthy communities: education, environment and equality of opportunity. Cummins serves its customers online, through a network of company-owned and independent distributor locations, and through thousands of dealer locations worldwide and earned about $2.1 billion on sales of $24 billion in 2021.

Media Contact
Redirecting to
cummins.com

The information you are looking for is on
cummins.com

We are launching that site for you now.

Thank you.