Cummins power unit capability boosted with new power take-offs

Cummins Inc. (NYSE: CMI) announces that the B6.7 and L9 Performance Series Power Units will feature new engine power take-off (PTO) capabilities to support key applications such as cranes, crushers and screeners.
Launched at Hillhead 2018, Cummins’ power units are available from 75 – 503kW (100 – 675hp) delivered as a complete and ready-made package. This comprises an engine, exhaust aftertreatment system, radiator and cooling system, plus auxiliaries such as mounting feet, hoses and an air cleaner. More than 60% of the content is pre-approved, making the machine integration process simpler and quicker.
Jeremy Harsin - Cummins Off-Highway Marketing Director said, ”Our Performance Series power units offer a flexible drop-in solution for manufacturers. The high-power density of our engines enables them to deliver high machine capability for hard working applications such as crushing, screening and pumping.”
Examples of installations to date include the L9 Power Units powering Anaconda’s new J12 and I12 crushing machines. The B6.7 version is available with Bandit in their Intimidator® 20XP tree chipper plus NLB Corp’s water jetting systems.
“To increase the flexibility and capability of the power units, we are integrating new single and dual rear-engine power take-offs (REPTO). These compliment their standard PTO capability used for items such as hydraulic pumps. We are also making these available on the base engines without the pack,” added Harsin.
As an example, fitted with the dual REPTO, the L9 will have a total drive capability of 560 Nm. This will make the engine capable of driving additional pumping capability through SAE B 2 and 4 bolt mounts. Integrated into the flywheel housing the dual REPTO is compact and has a minimal impact on engine packaging. Added weight is approximately 100kg.
"For equipment manufacturers, they have the ability to efficiently drive more from the engine without the need for additional aftermarket systems. This would support driving of hydraulic pumps for all sorts of machine functions from steering systems to fans, etc. It will reduce installation costs and complexity, for a more integrated solution," concluded Harsin.
Cummins Inc., a global power technology leader, is a corporation of complementary business segments that design, manufacture, distribute and service a broad portfolio of power solutions. The company’s products range from internal combustion, electric and hybrid integrated power solutions to components including filtration, aftertreatment, turbochargers, fuel systems, controls systems, air handling systems, automated transmissions, electric power generation systems, microgrid controls, batteries, electrolyzers and fuel cell products.
Headquartered in Columbus, Indiana (U.S.), since its founding in 1919, Cummins employs approximately 59,900 people committed to powering a more prosperous world through three global corporate responsibility priorities critical to healthy communities: education, environment and equality of opportunity. Cummins serves its customers online, through a network of company-owned and independent distributor locations, and through thousands of dealer locations worldwide and earned about $2.1 billion on sales of $24 billion in 2021.