Performance That’s A Cut Above - Cummins Performance Series Powers Claas Avero Combine Harvesters

Columbus, IN

Building on its longstanding history of powering agricultural equipment, today Cummins announced its Stage V B6.7 Performance Series engine will be available in CLAAS AVERO combine harvesters from Quarter 4 2019.

Cummins B6.7 engine has been integrated with CLAAS’s powertrain to deliver the optimum fit and performance for the AVERO. Delivering 157 kW (213 hp) maximum power and 990 Nm peak torque in CLAAS’s larger model and 123 kW (167 hp), 746 Nm peak torque in the smaller model, the B6.7’s power and torque curves have been tailored specifically to AVERO’s duty cycle using Cummins’ in-house electronic controls, fuel injection, air handling and exhaust aftertreatment technologies.

Ann Schmelzer, General Manager, Global Agriculture at Cummins explains, "During the integration process, we worked closely with CLAAS to understand the requirements of both their machine and their customers - the farmers who operate AVERO. As such, the B6.7 engine delivers the high power density, machine capability and efficiency required from a combine harvester, while its simpler architecture with fewer parts means higher reliability, easier accessibility, less maintenance and more productivity for farmers."

Cummins Performance Series B6.7While many manufacturers have adopted a ‘same as’ strategy from Stage IV to Stage V, Cummins technology leadership means its Stage V products deliver more power and less complexity through the removal of exhaust gas recirculation (EGR) on engines up to 12 liters displacement. Stage V emissions requirements are met through Cummins’ Single Module™ aftertreatment system which combines a diesel oxidation catalyst (DOC), a diesel particulate filter (DPF) and selective catalytic reduction (SCR) in a single unit. The system is 40% smaller and 20% lighter than Cummins’ Stage IV solution and features a compact AdBlue®/DEF mixer which removes the need for a decomposition reactor tube, making the whole system easier to keep clean.

Cummins decision to remove EGR at Stage V offers benefits for CLAAS global operations, as well as for its farming customers. Without EGR, the same Cummins engine platform can be applicable for sales to multiple emissions standards, from Stage V and Tier 4 Final, all the way down to unregulated levels. 

"We’re really excited to be powering the AVERO and we know that efficiency and productivity are key to the success of the whole CLAAS POWER SYSTEMS (CPS). Our Stage V Performance Series technology works to those objectives. Not only does it provide efficiencies to CLAAS through regional installation commonality, but farmers get fuel efficient, reliable performance in a simpler and easier to maintain engine package," concludes Schmelzer.

Cummins B6.7 Performance Series engines are manufactured at its Darlington, UK plant. 

To find out more about Cummins power solutions for agricultural equipment at Agritechnica 2019; Hall 16, stand D19 or visit: www.cummins.com/engines/agriculture

To find out more about CLAAS AVERO or make an enquiry, visit: www.claas.com/worldwide

About Cummins Inc.

Cummins Inc., a global power leader, is a corporation of complementary business segments that design, manufacture, distribute and service a broad portfolio of power solutions. The company’s products range from diesel, natural gas, electric and hybrid powertrains and powertrain-related components including filtration, aftertreatment, turbochargers, fuel systems, controls systems, air handling systems, automated transmissions, electric power generation systems, batteries, electrified power systems, hydrogen generation and fuel cell products. Headquartered in Columbus, Indiana (U.S.), since its founding in 1919, Cummins employs approximately 61,600 people committed to powering a more prosperous world through three global corporate responsibility priorities critical to healthy communities: education, environment and equality of opportunity. Cummins serves its customers online, through a network of company-owned and independent distributor locations, and through thousands of dealer locations worldwide and earned about $2.3 billion on sales of $23.6 billion in 2019. See how Cummins is powering a world that’s always on by accessing news releases and more information at https://www.cummins.com/always-on.

Cummins Information

 

 

Media Contact
Redirecting to
cummins.com

The information you are looking for is on
cummins.com

We are launching that site for you now.

Thank you.