Cummins Shows 100 Years of Innovation at Bauma

Munich, Germany

As part of Cummins’ centenary, visitors to stand A4.325 at the Bauma show saw 100 years of engine technology, with the company’s first engine known as the HVID shown alongside the latest B6.7 2019 Stage V engine.

Alexei Ustinov, Vice President Off-Highway Engine Business said: “Our founder Clessie Cummins recognised the benefits of diesel technology and transformed it into a reliable, everyday power source for a broad range of uses.  It is appropriate that we are here at Bauma for our anniversary, as industrial applications are where the company started.  During the first ten years Cummins delivered reliable power for pumping, grinding, sawing and stationary power.”

Cummins HVID engine
Cummins HVID engine produced in 1919.

The HVID was the first engine model that Cummins produced in 1919.   Available from 1.5-8 hp it ran on diesel or kerosene and was called an “Oil Engine”.  On display was one of only two 3hp versions that has survived to present day.  With a rated speed of 600 rpm it had a displacement of just over 1 litre, with a bore of 98.4 mm and stroke of 139.7 mm.  The unit weighed 280 kg.  Around 3,000 were manufactured by Cummins in Columbus, Indiana up to 1924. 

In comparison, the latest B6.7 Stage V engine produces more than 300 hp.  This is over 45hp per litre vs 3hp per litre of the original engine.  Weighing 583kg, it produces 0.6 hp per kilo versus 0.01 of the HVID, reflecting over one hundred times the power with only two times the weight.  This has also been achieved while reducing emissions by over 99%.

“Whilst the basic physics of the engines remains the same, the precision engineering and technology has changed significantly.  Cummins has developed key enablers in-house; combustion, air handling, fuel systems, filtration, electronic control and exhaust aftertreatment to get to where we are today. We have made significant strides for Stage V, but we won’t stop there.  We will continue to develop clean diesel technology, complimented by our alternative power solutions, that meet the needs of our customers and the environment in the future,” added Ustinov. 

Cummins B6.7 Stage V engine
Cummins B6.7 Stage V engine.

The B6.7 is one of a range of Stage V engines available from 100–675 hp (75–503 kW).   They come with more power and torque, are less complex and easier to install, and require less servicing.  For OEMs it enables them to increase machine capability and offer more value or downsize engines to reduce cost.  For operators it offers higher reliability with lower running costs.  The B6.7‘s increase in power and torque at Stage V means OEMs can more easily replace engines of higher displacement without impacting machine operations.  The engine is suitable for many applications including wheel loaders, excavators, dump trucks, fork lift trucks and empty container handlers.

Also featured was the Stage V F3.8 power unit. Delivered as a complete and ready-made power package, it comprises an engine, Single Module™ aftertreatment, radiator and cooling system – as well as auxiliaries such as mounting feet, hoses and an air cleaner.  The unit is more than 70% pre-approved for installation, reducing customers’ time and resources for integration.  Ideal for installations such as crushing, screening, air compressors and pumps. 

“We hope that Clessie Cummins would be proud of the company’s latest achievements if he saw them today,” concluded Ustinov.

About Cummins Inc.

Cummins Inc., a global power leader, is a corporation of complementary business segments that design, manufacture, distribute and service a broad portfolio of power solutions. The company’s products range from diesel, natural gas, electric and hybrid powertrains and powertrain-related components including filtration, aftertreatment, turbochargers, fuel systems, controls systems, air handling systems, automated transmissions, electric power generation systems, batteries, electrified power systems, hydrogen generation and fuel cell products. Headquartered in Columbus, Indiana (U.S.), since its founding in 1919, Cummins employs approximately 61,600 people committed to powering a more prosperous world through three global corporate responsibility priorities critical to healthy communities: education, environment and equality of opportunity. Cummins serves its customers online, through a network of company-owned and independent distributor locations, and through thousands of dealer locations worldwide and earned about $2.3 billion on sales of $23.6 billion in 2019. See how Cummins is powering a world that’s always on by accessing news releases and more information at https://www.cummins.com/always-on.

Cummins Information

 

 

Media Contact
Redirecting to
cummins.com

The information you are looking for is on
cummins.com

We are launching that site for you now.

Thank you.