Cummins Debuts China Stage IV Products at Bauma Shanghai

Shanghai, China
Cummins Distributor Sign

At Bauma China 2018, Cummins Inc. (NYSE: CMI) demonstrated a full line of China Stage IV (CS IV) engines with the unveiling of the upgraded high performance 8.9-litre L series engine which moves up to 400 hp (298 kW) with a peak torque of 1800 Nm – an 11 percent increase over that of CS III, offering class-leading fuel economy and the ability to run at high altitudes while maintaining power capability. 

Cummins full line-up of engines for the January 2020 CS IV emission standards spans 2.8 to 15 litres displacement with a power capability of 46 hp to 675 hp (34 kW to 503 kW). The proven technology and platforms move easily from CS III by leveraging the US Tier 4 Final and EU Stage V experience as well as on-highway NS VI.  The CS IV engines do more with less, offering up to 10 percent increased power density with better transient performance for improved machine productivity. Improved reliability with best in class fuel economy delivers lower total cost of ownership.

For CSIV, the 4.5-litre to 6.7-litre B engines are available from 89 hp to 300 hp (66-224 kW). The 8.9-litre L engine is available from 202 hp to 400 hp (151-298 kW). The 12-litre and 15-litre X engines are available from 335 hp to 675 hp (250-503 kW). All these are suitable for a wide range of construction equipment including wheel loaders, excavators, forklifts, cranes, drills, air compressors and road machinery.

“At Cummins we design our products to deliver the optimum balance of performance, reliability and cost that best fits the customer and market needs. Our significant technology experience has enabled us to select the most appropriate solution for China and the Stage IV emissions regulations,” said Dr. Lixin PENG, Cummins Vice President - Engineering, China ABO. “Cummins CS IV engines are designed and developed for a wide range of applications. With our upgraded performance systems, we are able to achieve low emissions without compromising the ability of the engines to perform at the highest load factors or in the toughest conditions.”

Cummins electronic control system and unique air-intake to exhaust-out system capability has enabled seamless machine integration for the OEM, and easier emissions upgrade for their customers. With the common technology with Cummins EU Stage V, it makes next generation upgrade more flexible and easier, and offers more choices for the customers with full line of Cummins EU Stage V engines that will be dual certified to CS IV.

Cummins Emission Solutions brings aftertreatment technology expertise to support Chinese customers with optimum choices including Diesel Oxidation Catalyst (DOC), Diesel Particulate Filter (DPF) and Selective Catalytic Reduction System (SCR).  “Over the past ten years Cummins has supplied SCR and DPF units to over 2 million vehicles and non-road equipment around the world.  Over 7 billion hours and 265 billion kilometers of operation have been accumulated while reduced 4.26 million tons of NOx,” added PENG.

Cummins CS IV solution for 6.7-litre to 15-litre engines use SCR technology and DPF plus DOC to significantly reduce Oxides of Nitrogen (NOx) and Particulate Matter (PM) emissions versus CS III.  The lower displacement engines adopt Exhaust Gas Re-circulation (EGR) combined with DOC and DPF for lower total cost of machine operations.

About Cummins Inc.

Cummins Inc., a global power leader, is a corporation of complementary business segments that design, manufacture, distribute and service a broad portfolio of power solutions. The company’s products range from diesel, natural gas, electric and hybrid powertrains and powertrain-related components including filtration, aftertreatment, turbochargers, fuel systems, controls systems, air handling systems, automated transmissions, electric power generation systems, batteries, electrified power systems, hydrogen generation and fuel cell products. Headquartered in Columbus, Indiana (U.S.), since its founding in 1919, Cummins employs approximately 61,600 people committed to powering a more prosperous world through three global corporate responsibility priorities critical to healthy communities: education, environment and equality of opportunity. Cummins serves its customers online, through a network of company-owned and independent distributor locations, and through thousands of dealer locations worldwide and earned about $2.3 billion on sales of $23.6 billion in 2019. See how Cummins is powering a world that’s always on by accessing news releases and more information at https://www.cummins.com/always-on.

Cummins Information

 

 

Media Contact
Redirecting to
cummins.com

The information you are looking for is on
cummins.com

We are launching that site for you now.

Thank you.