Cummins Reveals New Integral Innovations to Meet Stage V Emissions Regulations

Munich Germany

Cummins Inc. (NYSE:CMI) will today reveal a selection of new integral innovations for the off-highway market at the BAUMA show, running through 17 April, providing customers with reliable, next generation technologies to meet Stage V emissions regulations.

Cummins Emission Solutions, a global leader in aftertreatment technologies, is excited to unveil further developments of the Single Module™ aftertreatment system. Already announced for 6-cylinder engines, this efficient solution that offers up to a 30 percent reduction in weight and up to 50 percent in size compared to today’s Tier 4 Final solutions in this market, will be complemented with variations of this technology for equipment spanning from 74 hp to 430 hp (55-321 kW). Offering the latest innovation in aftertreatment, this product platform delivers multiple benefits to customers, including greater reliability and robustness due to simplified packaging and optimised on-board diagnostics.

Recognising the unique and diverse needs across the off-highway markets, Cummins Emission Solutions will reveal the Flex Module™, a more flexible Single Module technology package. This system will enable customers to fit the product into the challenging space claims often seen in off-highway applications. 

In addition to the Flex Module, Cummins is also developing a Single Module for 4-cylinder engines, which will deliver an efficient aftertreatment solution for equipment covering 74 hp to 200 hp (55-150kW) that need to meet the requirements of Stage V regulations. The concept product would offer customers an option to engine-mount the aftertreatment while delivering improved NOx conversion in the Selective Catalytic Reduction (SCR) system and a greater ash capacity in the Diesel Particulate Filter (DPF) with the use of advanced catalyst technologies.

All of these new solutions have been optimised for accessibility and serviceability, leading to simplified system maintenance. The DPF’s passive regeneration events result in longer maintenance intervals thus reducing the amount of service time required, ensuring less down time for the operator.

Cummins Turbo Technologies, a global engineering leader in turbocharger technology, will be introducing its HE250WG turbocharger. Designed to improve fuel economy by up to 2 per cent, this innovation in turbocharger technology offers durability and reliability in a compact and module design. Features include an optimized bearing design, which reduces sensitivity to contamination while maintaining excellent rotor system stability, to help minimise down-time.

Cummins Filtration, the world’s leading designer and manufacturer of filtration, coolant and fuel additive technology, will also be showcasing the latest in NanoNet® Technologies. NanoNet media is a proven protection for common rail systems, designed to be up to 13 times more effective than competitive filter products as removing and/or retaining particles. Unlike conventional filters, Nanofiber media is not affected by water in fuel and provides the structural integrity needed for high level performance. The benefits to customers are considerable, including extended service intervals, sustained high efficiency and reduced down-time and maintenance costs.

Mark Firth, Executive Director, Components Engineering, said: “Customers are increasingly looking for solutions to meet the requirements of Stage V emissions regulations. These new component technologies have been developed to meet customer demand whilst also offering innovation to the off-highway market, which deliver greater efficiency, flexibility and dependability.  By carefully considering the needs of our customers we have delivered technological solutions which are simpler to fit and service, reduce downtime and help to generate greater cost efficiencies, thereby supporting long-term business growth.”

Redirecting to

The information you are looking for is on

We are launching that site for you now.

Thank you.