Ground-breaking Fuel Saving Technology Revealed at IAA Hannover

Hannover, Germany

Cummins Turbo Technologies, a global engineering leader in turbocharger technology, will be revealing a suite of near-market and future solutions capable of improving the fuel efficiency of any modern diesel engine by at least 6% at IAA Hannover in September.

The shift in focus - from emissions driven innovation towards solutions that prioritise fuel economy - highlights Cummins Turbo Technologies’ belief that the industry has now reached the tipping-point at which global engine and vehicle manufacturers are developing products designed to insulate customers from rising fuel prices. Executive Director for Product Line Management & Marketing, Mark Firth comments: “Our close working relationship with customers has informed the research and development that is shaping our future product range and has led to the creation of technologies that will be revealed in Hannover next month. “Holset turbochargers are the component of choice for many international automotive customers because we don’t simply provide them with off-the-shelf products. We develop advanced technological solutions that are ‘fit for market’ – in other words they are developed in partnership to meet customers’ specific requirements.” The trend towards downsizing – which sees engine and vehicle manufacturers aiming to maintain or increase the power outputs from their products, whilst making them smaller and lighter - represents a significant engineering challenge and among the next generation technologies that are being revealed to meet it are:

• A Waste Heat Turbine Expander prototype - which captures what would otherwise be lost energy, in the form of heat, from a number of sources on board the vehicle and turns it into useful mechanical (25kW) or electrical (5kWe) power that is capable of reducing vehicle fuel consumption by 5% and delivering fuel savings of up to £3,500 per annum.

• A Next Generation Variable Geometry Turbocharger - based on a validated platform that can be tailored to meet the needs of individual customers without re-engineering, which is 2kg lighter and substantially lowers initial cost than the model it replaces whilst featuring a high efficiency compressor stage, delivering improved fuel economy.

• An Inverse Impeller that replaces conventional designs and, through the use of flow optimisation software, has the capability to improve compressor stage efficiency by 1% on its own – delivering a £100 per annum fuel saving for on-highway applications.

• A Super Map Width Enhancement ‘collar’ that enhances map width by 15% and facilitates engine downsizing, improves driveability, widens the operating range, aids efficiency mapping and delivers fuel savings.

• Rolling Element Bearings – Cummins Turbo Technologies has developed its own, high durability, low friction ball-bearing solution which improves both transient response and lowers fuel consumption – delivering a 1% improvement in overall turbocharger efficiency.

• Holset Rotary Turbine Control (RTC) – patented flow channelling technology that directs exhaust gas to selected ‘ports’ for limited exhaust control capability. RTC is integrated into the turbine housing within Cummins Turbo Technologies Modulated 2 stage (M2) and Serial 2 stage (S2) products.

Whilst Cummins Turbo Technologies anticipates that its future technologies will attract a great deal of interest at IAA Hannover, it will also be exhibiting currently available turbocharging solutions which can be tailored to meet the demands of any vehicle duty cycle or market regulation.

Mark Firth added: “We are known for providing a wide range of innovative, reliable and durable turbochargers which can be seamlessly integrated into a variety of vehicles and engines – so we will also be exhibiting our latest Euro 6, Tier 4 Final and US13/14 compliant products for customers seeking more immediate solutions to forthcoming emissions targets.

“These competitive, market-proven products and technologies draw on our 60 year history of innovation and engineering excellence to delivering savings without compromising on performance.”

To find out more about Cummins Turbo Technologies’ turbocharging solutions visit Hall 1, Stand D19 at IAA Hannover.

Redirecting to
cummins.com

The information you are looking for is on
cummins.com

We are launching that site for you now.

Thank you.