Ahoy Rotterdam, The Netherlands

Cummins Stage V Engines will be delivering MORE with LESS at TOC Europe.

Taking place from June 12th to 14th at Ahoy Rotterdam in The Netherlands, Cummins will feature its latest Stage V products and showcase the power it has to transform your business.

From 55 to 503 kW (74-675 hp), Cummins Stage V engines do MORE with LESS, delivering benefits for equipment operators and manufacturers. For operators of container handling equipment they deliver higher performance for more machine capability. Simpler architecture with fewer parts means more reliability, and more productivity. Improved fuel efficiency with extended service intervals drives lower running costs. The engines are more compact with less weight, less to cool, less installation complexity and lower installation costs for manufacturers.

Showcased at booth C24 will be the new B6.7 & X12 Cummins Stage V engines:

B6.7

Top-rated power for the Stage V B6.7 moves up to 243 kW (326 hp) with a peak torque of 1375 Nm – a 31% increase over that of Stage IV. Recently, Cummins announced that is latest B6.7 and L9 Stage V engines are now fully certified and in production at its Darlington UK plant.

X12

The X12 features a torque rise of as much as 60%, so it responds faster to increasing load factors even at lower engine rpm. With ratings covering 250 kW (335 hp) to 382 kW (513 hp), the X12 offers an ideal power solution for a wide variety of applications.
Check out our More with Less page and learn more about our next-generation engines for Off-Highway markets.

Register for your free visitors pass, and we look forward to meeting you there.


Stay Connected with Cummins

cumminseurope.com | @CumminsEurope

Redirecting to
cummins.com

The information you are looking for is on
cummins.com

We are launching that site for you now.

Thank you.