Hillhead Quarry, Buxton, UK

Taking place from June 26th to 28th at the Hillhead Quarry in Buxton, UK, Cummins will feature its latest products for construction, quarrying and mining equipment - showcasing how Cummins engines have the power to transform your business.

Press Release: Cummins Extends Its Stage V Lineup With New Power Unit Range

Stage V
Cummins Stage V Engines will be delivering MORE with LESS at Hillhead 2018:

  • MORE PERFORMANCE 
  • MORE MACHINE CAPABILITY 
  • MORE PRODUCTIVITY 
  • MORE REPLIABILTY 
  • MORE UPTIME 

From 55 to 503 kW (74-675 hp), Cummins Stage V engines deliver key benefits for equipment operators and manufacturers. For operators of construction and mining equipment they deliver higher performance for more machine capability. Simpler architecture with fewer parts means more reliability, and more productivity. Improved fuel efficiency with extended service intervals drives lower running costs. The engines are more compact with less weight, less to cool, less installation complexity and lower installation costs for manufacturers.
B4.5
Delivering exceptional power and responsiveness for faster cycle times, the 4-cylinder B4.5 delivers 16% more power and 11% more torque than the Stage IV version of this engine.
B6.7
Top-rated power for the Stage V B6.7 moves up to 243 kW (326 hp) with a peak torque of 1375 Nm – a 31% increase over that of Stage IV. Recently, Cummins announced that is latest B6.7 and L9 Stage V engines are now fully certified and in production at its Darlington UK plant.
L9
Cummins L9 offers some serious power. With ratings from 206-321 kW (275 – 430 hp), this engine delivers higher performance for more machine capability. 
X12
The X12 features a torque rise of as much as 60%, so it responds faster to increasing load factors even at lower engine rpm. With ratings covering 250 kW (335 hp) to 382 kW (513 hp), the X12 offers an ideal power solution for a wide variety of applications.
X15
New technologies and innovations delivered 15% greater horsepower and 60% more torque at Tier 4 Final, which have been maintained in the Performance Series.
Check out our More with Less page and learn more about our next-generation engines for Off-Highway markets.

Cummins engines for quarrying and mining applications
Next to our Stage V engine line up is our QSK19 & QST30 engines for mining and quarrying applications. More than 28,000 Cummins engines are active in mining operations around the globe in everything from excavators, drills and haul trucks to generators and underground mining equipment. No matter what you’re quarrying or where your equipment runs, Cummins engines provide exceptional dependability, reliability and productivity – even in the most challenging environments.
QSK19
With the Stage IIIA / Tier 3 rating of 377 kW (506 hp) rating, the QSK19 delivers the lowest life cycle cost with the longest life-to-overhaul of any engine in its class. 
QST30
With Stage II / Tier 2 ratings of 567 - 895 kW (760 – 1200 hp), the QST30 delivers the power you need for a range of applications including haul trucks, excavators, and drills.

Register for your free visitors pass, and we look forward to meeting you on our stand CE2.
 

Stay Connected with Cummins
cumminsengines.com | cumminseurope.com | @CumminsEurope

Redirecting to
cummins.com

The information you are looking for is on
cummins.com

We are launching that site for you now.

Thank you.