International Agri-Center; Tulare, California
Booth No. M6-M8
Join Cummins at World Ag Expo, February 11-13, 2020 to see how Cummins powers everything from the farm to the field to the future. This year you can find everything from agricultural engines to home generators at the Cummins booth, including the F3.8 structural engine for tractors, which will be making its North American debut at the show.
Read more below about Cummins’ display at the 2020 show.
F3.8 Structural Engine:
Customer flexibility was a core consideration during the design of the new structural F3.8 Performance Series engine. This extension of Cummins’ agriculture engine lineup provides compact and capable four-cylinder options for tractors in the 90 – 200 hp power band. This is the company’s latest innovation for tractor applications and, alongside the six-cylinder B6.7 engine, expands Cummins structural product coverage from 90 – 326 hp.
Learn more about Cummins' proven structural engine capabilities.
Performance Series Engines:
- MORE PERFORMANCE
- MORE MACHINE CAPABILITY
- MORE PRODUCTIVITY
- MORE RELIABILITY
- MORE UPTIME
- LESS FUEL USED
- LESS MAINTENANCE
- LESS INSTALLATION COST
- LESS WEIGHT AND SIZE
Simpler, easier installation with greater flexibility for global markets. Higher power density with greater low-end torque for improved productivity and efficiency. Lower total cost of ownership with extended maintenance intervals and improved fuel economy. This year’s display will feature the B4.5 and L9 Performance Series engines, plus F3.8, B4.5, B6.7 and L9, power units.
Power Generation:
Also new to the show this year is Cummins line of home and portable generators.
Guidanz:
Guidanz is Cummins’ suite of genuine service products, features and capabilities that maximize efficiency by streamlining processes associated with any service event. With everything from on-board diagnostics with the Guidanz app; to an interface with Cummins systems through Guidanz web. Learn more about the Guidanz suite of products.
World Ag General Info:
The World Ag Expo has an estimated annual average of 100,000 individuals from 70 countries in attendance each year. World Ag hosts 1400 exhibitors displaying cutting-edge agricultural technology and equipment on 2.6 million square feet of show grounds. For more information visit https://www.worldagexpo.com/.