Alstom leads the way with hydrogen fuel cell trains

Hydrogen molecule

When it comes to greener transportation, the future isn’t so far away — just ask Stefan Schrank, project manager of the Coradia iLint hydrogen-powered train from Alstom.

Based in Paris, rail technology manufacturer Alstom is a world leader in transport solutions. As a leading supplier of railroad technology, the company is the only leading supplier purely focused on railway technology. Alstom’s 38,000 employees across 60 countries provide groundbreaking solutions and service to over 280 customers at 100 sites. With a major global footprint, it’s no wonder Alstom is speeding toward the future of greener transportation.

As our world continues to change, customers everywhere are seeking greener and smarter mobility solutions. That’s why Cummins continues to invest in new forms of power with global manufacturers like Alstom.

The Coradia iLint is the world’s first hydrogen fuel cell passenger train. It’s completely emission-free, using electrical energy for propulsion and putting off only steam and water. The fuel cell system provides for a comfortable passenger experience, too — Amy Adams, Vice President of Fuel Cell & Hydrogen Technologies at Cummins, was impressed by the train’s quiet and smooth ride.

Hydrogen fuel cell technologies’ journey to adoption, however, has had some bumps along the way. One of the most common criticisms of hydrogen as a power source is that infrastructure must be updated and built new to accommodate hydrogen applications. However, Alstom’s hydrogen fuel cell train is designed for use on existing non-electrified lines, relieving the need for expensive electrification of existing lines. The Coradia iLint is already in use on more than 200,000 kilometers of passenger service lines in Germany and Austria, and has been tested already in the Netherlands. 

Not only does the hydrogen-powered train run on previously diesel-only rails, but it also matches the reliability of today’s diesel trains — a key factor in increasing adoption. And as its adoption grows, hydrogen’s economic viability continues to catch up with traditional diesel technology. Schrank predicts that a significant number of diesel propulsion trains will be replaced with hydrogen trains within 30 years, potentially sooner with government support.

Alstom is already a leader in railroad technology, and their latest innovations continue to provide creative mobility solutions for customers of the future looking to convert their fleets to zero-emission powertrains. Success stories are already on the rise, with more on the way. Alstom recently sold 41 trains with Cummins fuel cells to two customers in Germany, with passenger service beginning in 2021 and 2022.

The future of hydrogen remains bright. And with every successful journey of Alstom’s Coradia iLint, hydrogen fuel cell technology gains miles and miles of promise as a long-term sustainable power solution.
 

Cummins Office Building

Cummins Inc.

Cummins is a global power leader that designs, manufactures, sells and services diesel and alternative fuel engines from 2.8 to 95 liters, diesel and alternative-fueled electrical generator sets from 2.5 to 3,500 kW, as well as related components and technology. Cummins serves its customers through its network of 600 company-owned and independent distributor facilities and more than 7,200 dealer locations in over 190 countries and territories.

Cummins New Power President emphasizes decarbonizing now at The New York Times Climate Hub

Cummins New Power President emphasizes decarbonizing now at The New York Times Climate Hub

Amy Davis, Vice President and President of New Power, painted a picture of a decarbonized transportation sector with the help of both battery electric and hydrogen-powered solutions at The New York Times Climate Hub in Glasgow, Scotland, earlier this month. And while the debate between various low- and zero-carbon solutions continues around the world, she urged governments and corporations to start doing something now – because the carbon you put out today, tomorrow and next week cannot be taken back.

Cummins is over 100 years old, and we’ve been powering all kinds of commercial applications. One of the things we know is that [transportation] is very diverse, and we believe it’s not going to take just one solution [to decarbonize it].” – Amy Davis, President of New Power

In parallel with the 2021 United Nations Climate Change Conference, COP26, the Climate Hub hosted its program The Forum.  Over nine days, people across the globe tuned in to 45 live discussions, debates and workshops that addressed the mounting threat of climate change and what actions can be taken to stop it. 

Davis’ presence at The Forum was just one of numerous engagements and initiatives occurring in Glasgow that week. Cummins Chairman and CEO Tom Linebarger also attended COP26, meeting with governments, industry leaders and media to advocate for the shift from fossil fuels to low- and no-carbon solutions and demonstrating how Cummins will be part of the energy transition.

In the days leading to COP26 and The Forum, Cummins was accepted into two influential groups advocating for climate action

The consensus across conversations was that moving toward a carbon-free world is essential – but is it easier said than done? How do we make decarbonization happen? What does decarbonization even look like?

During the Transport and Mobility panel Time and Space: Moving People and Goods in a Carbon-Free World, Davis participated alongside Avinash Rugoobur, President of Arrival; Laura Lane, Chief Corporate Affairs Officer of UPS; and Peter Vanacker, President and CEO of Neste – all transportation and technology companies moving the industry toward a cleaner, greener future.

Watch the full discussion below as The New York Times climate reporter and panel moderator Brad Plumer opens the floor to Davis to discuss why Cummins is approaching decarbonization beyond just electrification, how infrastructure challenges have influenced hydrogen in mobility, and how transitionary periods lead to innovation in aftermarket solutions. 

Watch the full panel:

Keep up with alternative power innovation

From long-range possibilities to innovations happening now, Net Zero News delivers monthly highlights for low-carbon energy. Subscribe today to receive the next issue in your inbox.

Cummins Office Building

Cummins Inc.

Cummins is a global power leader that designs, manufactures, sells and services diesel and alternative fuel engines from 2.8 to 95 liters, diesel and alternative-fueled electrical generator sets from 2.5 to 3,500 kW, as well as related components and technology. Cummins serves its customers through its network of 600 company-owned and independent distributor facilities and more than 7,200 dealer locations in over 190 countries and territories.

What is a fuel cell?

Fuel cells are a key technology to unlocking our carbon-neutral future

Fuel cells aren’t new. In fact, the first reference to hydrogen fuel cells appears in 1838 in the December issue of The London and Edinburgh Philosophical Magazine and Journal of Science. Almost 200 years later, the world is recognizing fuel cells as a key technology to unlocking a carbon-neutral future.

Here is what they are, how they work and two fuel cell types that Cummins is investing in.

What is a fuel cell in simple terms?

Like batteries, fuel cells are energy converters – they use an electrochemical reaction to take the chemical energy stored in a fuel source and convert it to electricity. Unlike batteries, which contain a fixed supply of energy, fuel cells do not require recharging. As long as fuel is continuously supplied to the fuel cell, electricity, water and heat will be produced.

How does a fuel cell work?

A fuel cell is comprised of two electrodes and an electrolyte membrane. The electrodes are called a cathode and an anode, and they sandwich the electrolyte membrane between them. Within that system, a series of chemical reactions occur to separate the electrons from the fuel molecules to create energy.

The fuel, typically hydrogen, is fed into the anode on one side while oxygen is fed into the cathode on the other. At the anode, the hydrogen fuel molecules are separated into protons and electrons that will travel different paths toward the cathode. The electrons go through the electrical circuit, creating the flow of electricity. The protons travel through the electrolyte to the cathode. Once at the cathode, oxygen molecules react with the electrons and with the protons to create water molecules.

A fuel cell is a clean energy source with the only byproducts being electricity (power), heat and water. A single fuel cell alone only produces a few watts of power; therefore, several fuel cells can be stacked together to create a fuel cell stack. When combined in stacks, the fuel cells’ output can vary greatly, from just a few kilowatts of power to multi-megawatt installations.

What fuels can be used in fuel cells?

Fuel cells offer flexibility in the fuel type that can be used. While hydrogen is the most common fuel source for fuel cells (hence the common name, hydrogen fuel cells), hydrogen-rich fuels such as natural gas and ammonia are also viable fuel sources.

Hydrogen: When produced using renewable electricity – like solar, wind and hydropower – hydrogen is completely decarbonized and produces zero emissions. Hydrogen fuel cells (i.e. fuel cells that are fueled by hydrogen) produce power, heat and water and release no carbon dioxide or other pollutants into the air.

Natural gas: As widespread production of green hydrogen is still in progress, natural gas is currently the most-used fuel to power fuel cells. In this case the fuel cells are not completely emission-free, but they do offer significantly lower emissions than other fuels, like oil and coal.

Ammonia: Ammonia is most used in agriculture as fertilizer. However, in recent years, several companies have been working to develop green ammonia. Green ammonia is made with hydrogen that comes from water electrolysis powered by alternative energy, making it another option for a low-carbon fuel.

What types of fuel cells is Cummins investing in?

There are six types of fuel cells that are under development, each primarily classified by the kind of electrolyte they employ. Each type of fuel cell has its own advantages, limitations and potential applications. Out of the six, Cummins has recognized the potential in two types of fuel cells – proton exchange membrane fuel cells and solid oxide fuel cells - and has invested in the advancement of their technologies and their application.

Proton exchange membrane (PEM) fuel cells: Also referred to as polymer electrolyte membrane fuel cells, this type of fuel cell uses a polymer electrolyte and operates at lower temperatures of around 80 degrees Celsius. PEM fuel cells are more suitable for mobile and back-up power applications due to their high-power density and quick start-stop capabilities.

Solid oxide fuel cells (SOFCs): SOFCs use a hard, non-porous ceramic compound as their electrolyte and operate at high temperatures, as high as 1,000 degrees Celsius.  This type of fuel cell is most suitable for stationary applications because it is highly efficient and fuel flexible. In addition, waste heat may be harnessed and reused to increase the overall system efficiency.

Why invest in fuel cells?

Already leaders in PEM electrolyzers that produce green hydrogen through electrolysis, we are working on making green hydrogen more readily available for future use in fuel cells. Cummins was awarded a U.S. Department of Energy grant for the advancement of SOFCs and have seen our fuel cells successfully support the operation of battery electric vehicles.

Fuel cells may predate the beginning of Cummins, but we are wasting no time discovering how to advance their technology to create a zero-emission future.

Keep up with alternative power innovation

From long-range possibilities to innovations happening now, Net Zero News delivers monthly highlights for low-carbon energy. Subscribe today to receive the next issue in your inbox.

Cummins Office Building

Cummins Inc.

Cummins is a global power leader that designs, manufactures, sells and services diesel and alternative fuel engines from 2.8 to 95 liters, diesel and alternative-fueled electrical generator sets from 2.5 to 3,500 kW, as well as related components and technology. Cummins serves its customers through its network of 600 company-owned and independent distributor facilities and more than 7,200 dealer locations in over 190 countries and territories.

Video Case Study: Cummins HyLYZER® PEM electrolyzer in Bécancour, Quebec

The Cummins HyLYZER in Bécancour, Quebec, Canada, is the largest proton exchange membrane (PEM) electrolyzer in operation in the world. A new video case study highlights the installation’s ground-breaking green hydrogen production capabilities, making it a beacon for a zero-carbon future.

Watch below: 

Commissioned in January and installed at the Air Liquide hydrogen production facility in Quebec, this 20-MW electrolyzer system features industry-leading technology, including four compact, pressurized HyLYZER electrolyzer skids fitted inside the existing building. The systems are modular and scalable, perfect for large-scale utility applications.

Through a phased ramp up, the Cummins HyLYZER system is now at full operation and can produce up to 8.2 tons of low-carbon hydrogen per day — or nearly 3,000 tons of hydrogen annually. It’s powered by the region’s electric grid, which is largely supplied by renewable hydro-electric power. This means the hydrogen produced at the plant is “green” and almost entirely carbon-free.

Through this green hydrogen production, the facility is preventing approximately 27,000 tons of CO2 emissions per year. This is equivalent to taking 10,000 fossil-fueled cars off the road.

Since its commissioning, the system in Bécancour has increased Air Liquide’s hydrogen production capacity by 50%, allowing them to respond to the growing demand for low-carbon fuel in the North American market for both industrial and mobility purposes.

Keep up with alternative power innovation

From long-range possibilities to innovations happening now, Net Zero News delivers monthly highlights for low-carbon energy. Subscribe today to receive the next issue in your inbox.

Cummins Office Building

Cummins Inc.

Cummins is a global power leader that designs, manufactures, sells and services diesel and alternative fuel engines from 2.8 to 95 liters, diesel and alternative-fueled electrical generator sets from 2.5 to 3,500 kW, as well as related components and technology. Cummins serves its customers through its network of 600 company-owned and independent distributor facilities and more than 7,200 dealer locations in over 190 countries and territories.

Redirecting to
cummins.com

The information you are looking for is on
cummins.com

We are launching that site for you now.

Thank you.