14 Tips to Make Your Home and Family Safer This Fall

As the summer heat begins to fade away, fall is the perfect time to step up disaster preparedness, both inside and outside the home.

Whether it’s making sure you are prepared for the heart of hurricane season, confirming you and your kids have a family-communicated disaster plan, or ensuring your home is ready for Old Man Winter, now is the time to get all your ducks in a row.

To prepare the outside of your home, take a look around your property:

  1. Inspect your gutters and make sure they are clean so water can drain properly.
  2. Are bugs getting into your home? Perhaps you need to seal gaps and cracks around windows and doors to keep both bugs and the cold air out.
  3.  Don’t forget to look up. Inspect your roof for any damage or leaky vents.
  4.  How are your driveway, sidewalk and steps holding up? Be sure to repair anything that needs attention.
  5. Trim any dead branches or trees that may be leaning over your home.

To prepare the inside of your home, remember these tips:

  1. After all the spring and summer pollen, now is a good time to repair dirty filters. 
  2. Clean your clothes dryer exhaust duct and the space behind the dryer and remove any lint or dust that may have accumulated.
  3. Hire a professional to check out your furnace, fireplace and chimney.
  4. Insulate water pipes that may be prone to freezing temperatures.
  5. Now is also the time to test your smoke and carbon monoxide detectors.

Make sure you and your family are all on the same page:

  1. Have a family-communicated disaster plan and kit for each family member, as well as a meeting place if you were to all get separated.
  2. Build a mini-disaster kit for your child to keep at school.
  3. Have back-up battery chargers for electronic devices to ensure you can stay connected with loved ones if you experience a power outage.
  4. Consider investing in a standby generator to maintain your home’s power in the event of a weather-related or non-emergency power outage.

Cummins QuietConnect™ home standby generators deliver peace of mind, giving you confidence that your home and family are prepared for whatever Mother Nature throws your way. QuietConnect generators are also extremely quiet and incredibly affordable. They even add to your home’s resale value.

With a little planning, a little elbow grease and the right equipment, your family’s preparedness will be in great shape this fall. In the meantime, enjoy the cooler temperatures and vivid fall colors as we transition to autumn.

 

Cheryl Nelson, Certified Broadcast Meteorologist

Cheryl Nelson

Cheryl Nelson is an Emmy-nominated and AP award-winning Certified Broadcast Meteorologist, TV Host, FEMA-Certified Instructor and Weather and Preparedness Advisor for Cummins. You can visit Cheryl’s website at www.PrepareWithCher.com and follow her on Twitter and Facebook @CherylNelsonTV. 

What is the number pi and why is it so important?

Pi Day - March 14 - Cummins Inc.
Pi Day, the celebration of the number 3.14, is celebrated in mathematics and engineering circles every March 14

Pie is delicious (but pi is not). Unlike your favorite baked dish, however, a world without pi would look drastically different than the one we live in today. 

Question: What do Archimedes, Euler and Isaac Newton have in common?

Answer: First, they were all famous mathematicians. Archimedes discovered the law of hydrostatics; Euler is, to date, considered the most successful mathematician of all time; and Newton formulated the law of gravitation.

Second, they all spent considerable time working on the mathematical constant known as "pi." But what makes the pi so important for these and several other bright minds that they'd spend so much of their time focusing on it? Before we answer this question we have to first cover the basics.

What is the pi?

Simply put, pi is the ratio of a circle’s circumference to its diameter, and this ratio is approximately 3.14. So it's no coincidence that the mathematics, science and engineering worlds celebrate Pi Day every year on March 14 (3/14).

Pi is a constant, stays the same no matter how large or small the circle is and it is represented by the Greek letter π. 

Calculating the circumference of a circle using pi
Calculating the circumference of a circle using the pi.

Here is an interesting fact about the pi: Pi has infinite decimals that are randomly distributed. If you were to look at all the decimals of the pi, you will find your birthday (month | day | year) somewhere within the string of numbers. In fact, you can use this tool to find out where your birthday falls within the pi.  

Now that the basics are covered, let’s dive into why so many bright minds across the history spent their time studying pi number. 

Why the pi is so important? 

Well, our lives would be a little different without the pi. Practically most things we use in our everyday lives leverage the pi in their designs or in the way they operate. Let’s skip the most obvious ones such as tires, pipes at your home or the cup that holds your morning coffee, and focus on some of the lesser known yet indispensable uses of pi in our lives. 

  • Space exploration: From ancient Egyptians to modern scientists at NASA, humankind always had the utmost desire to explore space. Whether it was Sputnik becoming the first artificial satellite in space, or the Apollo 11 spaceflight doing the first lunar landing, pi has always been there. Today, NASA commonly uses pi to drive Mars rovers, discover potentially habitable worlds and investigating alien ice and beyond
  • Your daily entertainment: Streaming your favorite shows, talking to your friends and ordering food online, all depend on electromagnetic waves for wireless communication. Pi is used in calculating the wavelengths of these communications. 
  • Keeping your life Always On: Energy is one of most essential ingredients of our lives. We use electrical energy to keep our lights on, have smart devices connected and to power our everyday activities. Power generators are often used to generate this electricity keeping us Always On. Pi is used in many places in power generators from the calculation of engine displacements to the estimation of the fuel droplet size within the combustion system. 

A world without pi would have been very different, but thanks to all the bright minds humankind had, we don’t need to speculate that world and instead enjoy the world as we know it.

Sign up below for Energy IQ to periodically receive energy insights and trends. To learn more about how Cummins is powering a world that’s “Always On,” visit our web page.

Think your friends and colleagues would like this content? Share on LinkedIn and Facebook.
 

Raise Your Energy IQ

Grow professionally with energy trends and insights delivered to your inbox. Read about energy technologies and trends on our Energy IQ Hub.

Aytek Yuksel - Cummins Inc

Aytek Yuksel

Aytek Yuksel is the Content Marketing Leader for Cummins Inc., with a focus on Power Systems markets. Aytek joined the Company in 2008. Since then, he has worked in several marketing roles and now brings you the learnings from our key markets ranging from industrial to residential markets. Aytek lives in Minneapolis, Minnesota with his wife and two kids.

Weather Related Tips for National Preparedness Month

This September, Cummins is partnering with meteorologist and FEMA-certified disaster expert Cheryl Nelson to offer weather preparedness tips for every season through a comprehensive video series and complementary guide available on our home generators website

The guide, downloadable here, provides seasonal advice for safely facing severe thunderstorms, hurricanes, high heat and winter storms, as well as general preparedness tips. In addition, we have specific tips for senior family members, children and pets in our infographic.

While most people know to have water, batteries and canned goods on hand, there are many other critical steps to take when preparing for a severe weather incident. A few of the unique tips found in our severe weather preparedness brochure include:

  • Keep important documents such as birth certificates, insurance cards and medical history on a flash drive.
  • Have a paper map of your area. Remember that your GPS may not work following a disaster.
  • Keep a disaster prep kit in your car in case you need to evacuate quickly or are away from home when disaster strikes.
  • Consider buying flood insurance, but keep in mind it takes 30 days to activate.
  • Invest in a home standby generator to keep your power on in the event of a long-term power outage caused by a disaster.
  • Include a photo of you with your pet in your disaster kit in case you are separated and later need to prove ownership.

While September is a time to highlight disaster preparedness, Cummins encourages preparedness year-round. Please visit https://homegenerators.cummins.com/ahead-of-the-storm to see all of our weather-related prep tips.

Cheryl Nelson, Certified Broadcast Meteorologist

Cheryl Nelson

Cheryl Nelson is an Emmy-nominated and AP award-winning Certified Broadcast Meteorologist, TV Host, FEMA-Certified Instructor and Weather and Preparedness Advisor for Cummins. You can visit Cheryl’s website at www.PrepareWithCher.com and follow her on Twitter and Facebook @CherylNelsonTV. 

6 Tips to Prepare Your Home and Property for Hurricane Season

Even though hurricane season runs just six months out of the year, when storms hit, they do significant damage - about $26 billion annually, according to researchers at MIT.

When it comes to actual damage, two elements cause the most--water from storm surge or relentless rains and wind. Secondary to wind and water are the destruction both leave behind. Power outages. Flooding. Building destruction.

With all that in mind, I've put together the following tips and video to help you prepare for hurricane season. These are being presented on behalf of Cummins Inc., manufacturer of home standby generators, with whom I've partnered. Three of these tips are DIY - or do it yourself - things you can easily do yourself to help minimize or hopefully even prevent damage. You should definitely hire a professional to tackle the other three tips.

 

DIY Hurricane Prep

When it comes to do-it-yourself hurricane preparation, I suggest sticking with activities that are easy for you to do and which do not put you at risk of hurting yourself. For example, one tip requires you to go up on a ladder. If you are unsteady on your feet, by all means get someone else to go up on that ladder. Or hire a professional. When in doubt, don't put yourself in danger.

The tips below all focus on keeping water away from your home's foundation. That's because water can do severe long-term damage to your home.

1. DIY Clean Your Gutters

You should clean your gutters twice a year. You do it once in fall, not only because it is hurricane season, but also to prepare for winter. You don't want water gathering in your gutters and then freezing. That's a great way to make your gutters rip away from your house. You clean your gutters again in spring because of those proverbial April showers. Again, you want your gutters clean and free of debris so water can move down and out. And speaking of out, make sure the down spouts are clear and aimed away from your house so water goes away, too.

2. DIY Prepare Your Landscaping

Another way to keep water from getting into your home's foundation is through your landscaping. You want all soil and mulch to slope away from your home, not towards it. This keeps water moving in the right direction.

3. DIY Seal Foundation Cracks

Water is like a ninja when it comes to affecting a home's foundation. It's going to find a way, somehow, to get to it. Stop the ninja dead in its tracks by using foundation crack epoxy sealer. You can find it at your local hardware store.

Hire a Pro for Hurricane Season

Sometimes you've just got to hire a pro. It goes along with the notion of not being penny wise and pound-foolish. In times like this, it makes sense to spend the money to get a job done right, because DIY just won't cut it.

Here are three hurricane season prep jobs for which you should bring in a professional to get your home ready for impending storms.

1. Pro to Trim High Branches

When I want to trim a few low-hanging branches here and there, I can easily get clippers from my shed and do the job myself. But when I have dead branches hanging high above my house, I hire a professional tree service to trim those and any other branches that might come lose in a storm. These folks know exactly how to trim a tree to keep your home safe and to keep the tree alive.

2. Pro to Install Sump Pump Alarm

The first summer we lived in our house, Hurricane Floyd hit. That was 1999. I'll never forget looking out my back door and seeing my neighbor go by in a canoe. There was that much water in our backyard. Thankfully, our basement remained dry during the height of the storm, thanks to our sump pump. Unbeknownst to us, all of that pumping of water eventually knocked the sump pump off kilter. Shortly, thereafter it stopped working all together--even though we didn't lose power. We were none the wiser, until I went downstairs the next day to do laundry and stepped into 12 inches of water. If you live in a place where your basement floods, always have a pro install an alarm when installing a sump pump. If we'd had an alarm, we would have known right away that the sump pump had stopped working, and we could have stopped our basement from flooding.

3. Pro to Install Standby Generator

Around the same time as Superstorm Sandy in 2012, we got a portable, gas-powered generator for our four-bedroom home. We thought we were so smart. Problem is, we never stopped to consider two post-hurricane scenarios. One, we couldn't leave our street to buy gas, because of downed trees and blocked roads. And, two, we couldn't get gas at all, even if we could get out of our street. That's because so many gas stations were without power and therefore couldn't pump it. In hindsight having a home standby generator to power our entire home would have made so much more sense.

Cummins home standby generator

Unlike portable generators that can be noisy and require manual set-up, running cords and gasoline, standby generators restore automatically when the power goes out, even if you aren’t home.

Cummins home standby generator installation

Standby generators are connected directly to your home’s electrical and natural gas/LP systems, so there are no trips to the gas station and no running out of gas. To see if a standby generator is right for your family, visit homegenerators.cummins.com, where you can find details about the products, how they work and how you can prepare. There’s also a handy sizing calculator where you can estimate your power needs.

Final thought when hiring a pro: don't wait until there is a hurricane in the weather forecast. You'll likely never get someone in to take care of the job in time.

Leah Ingram, Freelance Writer, Lifestyle and Money-Saving Expert

Leah Ingram

Leah Ingram is a freelance writer, lifestyle and money-saving expert. Her mission is to help you feel more confident about your spending, regardless of income.

 

She is the author of Suddenly Frugal: How to Live Happier and Healthier for Less, which compiles Leah’s unique money-saving advice, including how a family can save $25,000 a year. Her second title in the Suddenly Frugal series is Toss, Keep, Sell!: The Suddenly Frugal Guide to Cleaning Out the Clutter and Cashing In.

 

Currently, Leah is working on a personal finance book, chock full of ideas to help middle-class families pay for college. That book, tentatively called College Money Hacks, will be out from Career Press in Fall 2017.

 

For more information, visit Leah's website at http://www.leahingram.com/about/.

Important Tips to Endure Dangerous Heatwave Conditions

Summer heat wave

According to the National Oceanic and Atmospheric Administration, June 2019 was the hottest on record for the globe. With record-breaking high temperatures blanketing cities around the world, these tips can help you and your family stay safe during the extreme heat. 

One month into summer 2019, and the mercury is rising.

A heat wave will impact half of the U.S. over the coming week with temperatures in the 3-digits in some parts of the country. Heat waves of this magnitude are not just an inconvenience, they can be dangerous, even life-threatening, if proper precautons aren’t taken. There were 108 heat-related fatalities in 2018 according to NOAA. Of all natural disasters, heat holds the highest 10-yr average of fatalities with 101.

During the hot summer months, a home standby generator like the Cummins QuietConnect will keep your A/C running if you lose power.

Cummins home standby generator

People who are sick, the elderly and young children are most susceptible to heat-related-illnesses. However, anyone can suffer from a heat-related illness if they over-exert themselves or simply don’t take extreme heat warnings seriously. Whether your region is experiencing a heatwave or record-breaking temperatures, I’ve compiled some tips on behalf of Cummins to keep your family, friends and neighbors safe this summer.

Safety Tips for Extreme Heat

  • Never leave children or pets alone in hot vehicles – even for a second.
  • Stay inside during the hottest part of the day (10am-4pm) and limit time outside in the sun.
  • If A/C is not available, stay indoors on the lowest floor in a well-ventilated area with fans. Keep shades and blinds closed.
  • Stay hydrated with plenty of water - even if you’re not thirsty.
  • Don’t drink alcohol, soda or other caffeinated beverages as they make dehydration worse.
  • Avoid strenuous activity and postpone outdoor games and events.
  • Use sunscreen, wear a hat and light-colored clothing.
  • Visit air-conditioned public spaces such as malls, movie theaters and libraries to keep cool.
  • Check on family and friends with special needs and those who may not have A/C or live alone.
  • Keep your pets indoors and make sure they have access to a cool space and plenty of water.
  • Listen for weather updates from the National Weather Service (NWS) on a NOAA weather radio.
  • Go to a designated public shelter if your home loses power during periods of extreme heat. Text SHELTER + your ZIP code to 43362 (4FEMA) to find the nearest shelter in your area (example: shelter 12345) and listen to your local officials for shelter locations.

Preparing for Extreme Heat Conditions

  • Consider a home standby generator like the Cummins QuietConnect that will turn on automatically and keep your A/C running and your entire house on if you lose power.
  • Properly install window air conditioners (sealing any cracks) and insulate if necessary.
  • Check A/C ducts for proper insulation and clean filters.
  • Install awnings, blinds or light-colored drapes and keep them closed to keep sunlight and heat out.
  • Upgrade your windows and weather-strip door to keep heat out and cool air in.
  • Get trained in first aid and CPR.

Cheryl Nelson, Certified Broadcast Meteorologist

Cheryl Nelson

Cheryl Nelson is an Emmy-nominated and AP award-winning Certified Broadcast Meteorologist, TV Host, FEMA-Certified Instructor and Weather and Preparedness Advisor for Cummins. You can visit Cheryl’s website at www.PrepareWithCher.com and follow her on Twitter and Facebook @CherylNelsonTV. 

Redirecting to
cummins.com

The information you are looking for is on
cummins.com

We are launching that site for you now.

Thank you.