Wrigley Field Depends on Cummins for Power Protection

As part of a massive renovation of its historic ballpark, the Chicago Cubs’ choice for backup power at Wrigley Field is a hit with us: a Cummins QSK95 Series generator set.
The 16-cylinder QSK95 powered generator set is 80,000 pounds of near-zero emissions diesel power, designed to provide critical power protection without interruption, making it the perfect choice to keep the lights on in places like Wrigley Field, hospitals and utilities.
Though the QSK95 is the largest engine Cummins has ever produced, the generator set provides a reduced installation footprint and cost advantage compared with other high-speed generator sets, which typically require 20 cylinders to achieve the same power output.
While its sheer size allows the QSK95 Series generator set to produce incredible power, that’s not the only thing that makes it stand out from the competition. All Cummins Power Generation products leverage our “Power of One” capability. As the world’s only provider of pre-integrated power solutions, all key systems – including engine, alternator and controls – are designed and manufactured in-house.
https://www.youtube.com/watch?v=YHrovDLOQvw
Since all components are built to work together, Cummins power systems offer smaller footprints, highly efficient operation and the best system integration in the world. This advanced manufacturing sets a new standard for power generation around the world.
But while organizations like the Cubs rely on the dependability of Cummins power, the QSK95 can do more than keep the lights on.
Meet the QSK95

The QSK95’s appeal goes far deeper than its size – it’s a cross-industry workhorse, equipped with cutting edge technology. In addition to power generation applications, it sees duty in marine vessels, mining trucks and locomotives around the world. QSK95 delivers clean, efficient power in each of its markets, meeting strict environmental standards around the world.
Want to learn more about this giant diesel? Click below to explore why industries around the world turn to the QSK95 for dependable diesel power.