The Cummins Napier Railton Race Car: Coming Soon to INTERMAT

The original Napier-Railton race car was built in 1933 and made its debut in August of that year at the Brooklands race track in Surrey, England. Piloted by John Cobb, the car broke the Brooklands outer circuit lap record of 143.4 mph in 1935, and went on to set the 24-hour record of 150.6 mph at the Bonneville Salt Flats in 1936.
While diehard race fans have to visit the Brooklands Museum in the UK to view the original Railton car, Cummins will take a dimensionally-accurate diesel powered replica of the car to the INTERMAT show in Paris on April 20-25, 2015.

Throughout the duration of the five day show, the unique “Cummins Napier Railton” will be proudly displayed alongside the company's lineup of the latest engine technology. The Cummins Napier Railton replica is powered by a Cummins 6.7-liter diesel, the same base engine widely used in many types of construction equipment, including excavators and wheel loaders.
While the latest QSB6.7 engine meeting Tier 4 Final/Stage IV emissions regulations offers an impressive top rating of 300 hp (224 kW), Cummins engineers have achieved close to 500 hp (373 kW) output for the 6.7-liter diesel installed in the Railton replica.
Cummins has a strong history in racing, using it to test product durability as far back as the early 1930s. The 1931 Cummins Diesel Special No. 8 Indianapolis 500 car, built around the same time as the Napier Railton, was also driven at Brooklands during a European tour organized by company founder Clessie Cummins. This car still runs, and is displayed in the Indianapolis Motor Speedway Museum. The Cummins Diesel No.8 became the first diesel vehicle to reach 100 mph, running on the hard sand at Daytona Beach, Florida. Power came from a race modified Cummins Model U 4-cylinder, 6-liter diesel with 85 hp (63 kW).
Where to See the Cummins Napier Railton
Visitors to INTERMAT can see the unique Cummins Napier Railton diesel race car at the Cummins display, Hall 5B, booth 028. Cummins experts will be on hand to provide an insight into the race-engineered 6.7-liter engine.
Additional Resources
Cummins.com media release - “Cummins Napier Railton” Race Car Heads To INTERMAT"
Cummins.com media release - "Cummins To Extend Qsf Engine Line-Up At Intermat With Rental Equipment-Focused Configurations"
YouTube: Cummins Racing History