Cummins Turns Landfill Gas Into Power for Delaware Customers

Dignitaries including Delaware Gov. Jack A. Markell attended a ground breaking ceremony this summer for an innovative energy solution at Croda Inc. in Delaware featuring Cummins’ combined heat and power systems running on landfill gas.

Construction started earlier this summer on a first of its kind project for Cummins that will use landfill gas and the Company’s combined heat and power (CHP) systems to provide industrial customers in Delaware with a clean, sustainable source of energy.

The first recipient will be Croda Inc.’s Atlas Point chemical manufacturing plant in New Castle, Del. Croda, a global company with operations in 33 countries, estimates the project will provide enough energy to cover about 55 percent of its operations at Atlas Point.

Over the next two years, the City of Wilmington’s Wastewater Treatment Plant and the Port of Wilmington will join the system, also using Cummins’ combined heat and power systems running on landfill gas.

“Croda has a global goal to obtain 25 percent of its energy needs from non-fossil sources by 2015 and we are excited that this venture will help us achieve that goal,” said Croda Inc. President Kevin Gallagher, who estimates Croda’s investment will pay for itself in five or six years.

The project has gotten the attention of Delaware Gov. Jack A. Markell. He applauded Croda at a groundbreaking ceremony for the $6 million project on June 7 (2012).

“This project saves energy costs for a company that has chosen to locate here while putting more people to work,” Markell said. “We applaud Croda’s investment in Delaware, both environmentally and economically.”

Don Gesick, Cummins’ General Manager – Energy Solutions, said Cummins is excited to take a leadership role in providing Croda and its other customers with a “comprehensive, efficient and green solution.”

“Instead of the landfill gas being flared into the atmosphere, this system brings the gas directly to Croda and our other partners, reducing emissions,” he added. “The CHP system then allows for maximum productive use of the renewable energy.”

Construction on the Croda project started in June and is expected to wrap up sometime in the fall of 2012. Croda estimates the initiative will replace 2.2 megawatts of utility-supplied electricity, reducing annual greenhouse gas emissions equivalent to removing 33,000 passenger cars from the road.

The wastewater treatment plant project, part of an overall city Sustainable Energy Initiative costing $50.5 million, will be even bigger. The city expects to produce 4.4 megawatts of energy – essentially enough power to take the plant off the grid if officials wanted.

The Port of Wilmington is looking for a system to generate about 2 megawatts of power to help meet its overall power needs.

While it’s fairly common for landfills to use the gas they generate to power aspects of their operations or create energy that they then sell to a utility, rarely is the gas pumped off site to meet the energy needs of multiple companies and agencies. The use of CHP systems to get the most of the energy produced makes this initiative even more unusual.

Here’s how the project works: Cummins Power Generation obtained the right to use the landfill gas from the Delaware Solid Waste

Authority, which runs the 500-acre Cherry Island Landfill. The gas is currently being released by means of a flare to keep it from building up in the landfill.

More than 50 percent of landfill materials are organics and suitable for anaerobic digestion that yields biogas, typically about 50 percent methane. Gas-powered generator sets and on-site power plants can be designed to run on gas with low or variable energy content.

When the Delaware project is up and running, the gas will be collected and conditioned at the landfill, then piped to Croda and the other customers. The Croda plant is about four miles from the landfill.

Once it reaches its destination, the gas will fuel a Cummins CHP system that will produce electricity while also capturing the heat from generators that otherwise would be lost. Up to 85 percent of the available energy output with a combined heat and power system can be used productively.

The heat captured at Croda will be used in the facility’s boiler system. At the treatment plant, officials plan to use the heat to dry sludge, significantly reducing the volume that then has to be taken to an out-of-state landfill for disposal. The port plans to convert the heat captured by the combined heat and power system to run chillers to cool warehouses used for items like fruits and vegetables.

The solid waste authority says the landfill will generate enough gas for the system for at least 20 years and perhaps twice that long.
Gesick says every landfill situation is a little bit different so he’s not sure if the Cherry Island project will be a model for other customers looking to reduce their reliance on fossil fuels. Unlike many landfills, for example, Cherry Island is relatively close to potential customers. Often landfills are located in remote areas.

The Delaware project, however, is an example of the kind of innovative arrangement Cummins Power Generation can develop to meet customers’ needs.

In addition to industry leading generators and CHP systems, Cummins Power Generation offers financing, operations and maintenance programs. It even builds turnkey power systems, handling everything from design to installation and commissioning.

The Cherry Island project received high praise from Delaware’s Department of Natural Resources and Environmental Control Secretary Collin O’Mara.

“Croda should be commended for deploying one of the cleanest and most efficient energy projects in the nation,” he said at the groundbreaking.

“This project demonstrates innovation and environmental commitment by taking a readily available waste product that previously served no productive purpose – in this case landfill gas – and putting it to work making cleaner and more efficient energy while reducing emissions and fossil fuel dependence.”

blair claflin director of sustainability communications

Blair Claflin

Blair Claflin is the Director of Sustainability Communications for Cummins Inc. Blair joined the Company in 2008 as the Diversity Communications Director. Blair comes from a newspaper background. He worked previously for the Indianapolis Star (2002-2008) and for the Des Moines Register (1997-2002) prior to that. [email protected]

 

Cummins CEO highlights employee safety, ingenuity at Annual Meeting

CEO Tom Linebarger speaks at a past event, before the COVID-19 crisis. The 2020 Annual Meeting was held virtually to protect against the spread of the virus.
CEO Tom Linebarger speaks at a past event, before the COVID-19 crisis. The 2020 Annual Meeting was held virtually to protect against the spread of the virus.

Cummins is taking numerous steps to protect employees from COVID-19, Chairman and CEO Tom Linebarger said at the company’s Annual Meeting Tuesday.

The company has implemented health screenings and temperature checks for those entering plants, increased cleaning protocols and established a response center supported by medical personnel to answer employee questions 24 hours per day, seven days per week, Linebarger said.

He told shareholders the company has also established a leadership committee to respond to reported problems and a planning team focused on planning for future developments. Linebarger said the health and safety of employees and the communities where Cummins operates are the company’s first priority as it moves forward in these uncertain times.

“Most office employees around the world at Cummins are working from home as we comply with stay-at-home orders to reduce the spread of the virus,” Linebarger said. “At the time of this meeting, several of our plants have gone through periods of shutdown or reduced capacity, and many locations are now resuming operations, though at a very reduced level. …Things look very different now than how we operated prior to COVID-19.”

A Seymour Engine Plant employee at work
A Seymour Engine Plant employee in Seymour, Indiana, working under the new plant rules since the pandemic. 

Linebarger said with most office employees staying at home, the company has been able to divert cleaning resources to facilities where employees are coming in to work every day, significantly increasing cleaning and disinfecting protocols. For those employees working in plants, in addition to the screenings and temperature checks, immediate care is available for anyone displaying symptoms for COVID-19.

 For employees whose work requires them to be in close proximity to others, the company has additional personal protective equipment for them to wear.

A DIFFERENT WAY TO WORK

Cummins has also redesigned certain processes and facility layouts to allow employees to operate safely and effectively, re-configuring assembly lines and entrances and exits to promote social distancing and ensuring common surfaces are cleaned regularly. In addition to answering questions, the response center is available to conduct contact tracing to determine people who might have been exposed to someone with COVID-19.

The company is using medical personnel from Cummins’ LiveWell health center in Columbus, Indiana, to support the COVID-19 response. center.

Linebarger said the company has benefitted from having dealt with the crisis since January when the virus was first discovered in China. Cummins has several facilities in Wuhan, China, considered the epicenter of the outbreak. All of Cummins’ plants in China are now back in operation and business has been brisk as the company’s customers have responded to pent-up demand.

An employee works in Seymour, Indiana.
In addition to masks, anyone entering the Seymour plant must pass through a health check where they get their temperature taken.

OPTIMISTIC SIGNS

That is only one hopeful sign. Linebarger said Cummins is also in a strong financial position. At the end of the first quarter of 2020, the company had cash and cash equivalents of $2 billion, strong credit ratings and Cummins’ pension plans are fully funded. Linebarger said aggressive action to cut costs such as reducing pay and hours for some employees, while painful, will serve the company well during this unprecedented downturn.

Even in the middle of the crisis, Cummins has maintained its investment in low- and no-carbon technologies like hydrogen fuel cells and battery electric power platforms that will position the company well for the future when more normal conditions and demand returns.

“During our 100-year history we have encountered several unforeseen crises and economic challenges,” Linebarger said during the virtual meeting, another first caused by the pandemic. “I am confident we will successfully navigate this one as we have done before and emerge stronger as a company.”

He said also true to the company’s history, Cummins employees have risen to the challenges presented by COVID-19, responding in new and creative ways to help the company and the communities where they live and work.

Employees have engaged in a host of activities, from helping day care centers and hospitals plan for COVID-19, to powering essential shipments of food and medicine, building and servicing the generators at emergency medical centers around-the-world, and partnering with other companies to increase the production of personal protective equipment.

“It will come as no surprise to you that our employees around the world have stepped up and responded to the needs of their communities in innovative ways,” Linebarger said. “…As always, our employees and our company are doing all that we can do to address this crisis in new and creative ways, and we remain committed to powering a more prosperous world.”
 

blair claflin director of sustainability communications

Blair Claflin

Blair Claflin is the Director of Sustainability Communications for Cummins Inc. Blair joined the Company in 2008 as the Diversity Communications Director. Blair comes from a newspaper background. He worked previously for the Indianapolis Star (2002-2008) and for the Des Moines Register (1997-2002) prior to that. [email protected]

 

Team saves test using Cummins' ingenuity

The Cummins team had to figure out quickly how to keep testing going while practicing all the COVID-19 safeguards.
The Cummins team had to figure out quickly how to keep testing going while practicing all the COVID-19 safeguards.

On-Board Diagnostic Misfire Testing is as complex as its name would suggest. Keeping a recent test moving forward might have been even more complicated.

The labor-intensive test requires a driver and technician sit side by side to test an engine under “real life” circumstances to prove to regulators its onboard diagnostics are capable of detecting a misfire due to a component failure that produces excessive emissions. The testing is critical to keeping the regulatory process moving forward on the engine model for 2021.

The testing had been taking place at a college several hours away and was at a critical moment when the school suddenly had to shut the lab down as part of its response to the COVID-19 crisis. As the Cummins team quickly made plans to shift testing back to Columbus, Indiana, a feat in itself, plans were also being forged by the test team group leader Alex Marin Cruz to finish the critical testing at the Olympia Building (OLY) – this time while maintaining all the recommended COVID-19 safeguards, including the six-foot social distancing rule. 

FINDING THEIR INNER MACGYVER

In the midst of all the other personal and professional stresses caused by the fast-paced global pandemic, a team of engineers and technicians from both OLY and the Cummins Technical Center (CTC) quickly brainstormed a safe solution.

They pulled more than 50 feet of ethernet and specialized cables from rarely used storage closets in CTC and OLY. Two-way radios that hadn’t been used in some time were dusted off. The testing was slightly reconfigured, so the driver and technician no longer had to sit together but could still communicate using the radios. 

The team lost just under 48 hours, but testing was ready to continue.

A view of the testing.
The team  found cable and two-way radios that hadn't been used in some time to keep the testing going.

NEVER A DOUBT

“We never had any doubt,” Marin Cruz said when asked if he ever thought the testing would have to be postponed. “We were just focused on safety and keeping us six feet apart.”

They are now on track to submit data as part of the certification package to the California Air Resources Board (CARB) by the regulator’s deadline. Their extraordinary efforts to keep the engine testing on track will likely be critical to keeping the project moving forward.  

Team members in addition to Cruz include Shelley Knust, Curt Barnhart, Justin Owen, Ansh Sharma, Michael Tress, Shashank Sharma, Celso Gomez, David L Adams, Arun Shori D Sundaravel, Daniel Holle, and Robert S. Jones.

They demonstrated, once again, that both the company’s value of teamwork and its vision to innovate for its customers are alive and well at Cummins. Even in the midst of a global pandemic.
 

Cummins Office Building

Cummins Inc.

Cummins is a global power leader that designs, manufactures, sells and services diesel and alternative fuel engines from 2.8 to 95 liters, diesel and alternative-fueled electrical generator sets from 2.5 to 3,500 kW, as well as related components and technology. Cummins serves its customers through its network of 600 company-owned and independent distributor facilities and more than 7,200 dealer locations in over 190 countries and territories.

Trio of honors reflect Cummins’ commitment to sustainability

Cummins has long believed that a wide range of factors determine the sustainability of a company.
Cummins has long believed that a wide range of factors determine the sustainability of a company.

Cummins  recently received three honors for its work on ethics, environmental resiliency and supplier diversity.

The recognition reflects the company’s broad approach to sustainability, including everything from Cummins’ efforts to shrink its environmental impact to corporate responsibility, health and safety, diversity and inclusion, financial success, innovation and governance and ethics. The company, which celebrated its 100th anniversary in 2019, is committed to staying in business for the next 100 years.

“When we initiated the World’s Most Ethical Companies recognition in 2007, the concept of companies proactively aligning profits and purpose seemed unlikely,” said Ethisphere CEO Timothy Erblich, upon announcing the group’s list, which Cummins made for a 13th consecutive year. “However, leading CEOs and organizations continue to prove our long-held hypothesis that conducting ethnical business is the key to maximizing profits.”

WORLD’S MOST ETHICAL COMPANIES

Ethisphere is  the global leader in defining and advancing standards of ethical business practices. It said 132 honorees representing 51 countries and 21 industries were included in the group’s 14th annual recognition. There were 14 newcomers to the 2020 World’s Most Ethical Companies list, while seven companies have received the designation every year since the list was first announced in 2007.

To be eligible for the designation, companies must fill out a comprehensive survey on their business practices. Most of the survey questions deal with ethics and compliance, but there are also questions about the company’s environmental performance, community engagement, and supply chain engagement and oversight.

Honorees have historically out-performed other companies financially, demonstrating the connection between good ethical practices and performance that’s valued in the marketplace. Other companies on the 2020 list included Accenture, General Motors, Microsoft and Waste Management. 

Hoosier Resilience Hero logo
TheEnvironmental Resilience Institute has prepared a video to celebrate the 2020 heroes.

HOOSIER RESILIENCE HEROES

Cummins has been named to the Environmental Resilience Institute’s Hoosier Resilience Heroes list, which recognizes individuals and groups across the state of Indiana for their efforts to prepare Hoosiers for climate change and promote safe, healthy communities. The institute is part of Indiana University.

"We affect our environment, and our environment affects us," said the institute’s Director Janet McCabe. "Whether it is coronavirus, climate change or corn yields, we live in interconnected systems. The better we understand these connections, the more resilient we can become to protect our health, our communities and our economy.”

Cummins, which has its headquarters in Indiana, was recognized for its PLANET2050 environmental sustainability strategy to reduce the company’s environmental impact. The strategy was released in 2019 and includes science-based goals timed to 2030 and aspirations for 2050. Cummins was the only company among the 2020 heroes.

This is the second year the institute has released a list. The institute’s mission is to enhance resilience to environmental change in Indiana and the Midwest by accurately predicting impacts and effectively partnering with communities to implement “feasible, equitable, and research-informed solutions.”

SUPPLIER DIVERSITY AND INCLUSION

Cummins has been named a Top Global Champion for Supplier Diversity & Inclusion, which recognizes corporations that lead with globally inclusive sourcing efforts. The recognition comes from a trio of groups: the U.S. Pan Asia Chamber of Commerce, the National LGBT Chamber of Commerce, Disability:IN, the leading nonprofit for resource for business disability inclusion worldwide and WEConnect International, a global network that connects women-owned businesses to qualified buyers around the world.

Cummins finished No. 4 on the partners’ list behind only Kelly Services, Merc and IBM.

“If you are not sourcing inclusively everywhere you do business, you do not have full access to critical innovations and the best total value options that will help you meet and anticipate the needs of your clients,” said WEConnect International CEO and Co-Founder Elizabeth A. Vazquez. “This ranking showcases the acceleration of a truly global movement towards supplier diversity and inclusion.”
 

blair claflin director of sustainability communications

Blair Claflin

Blair Claflin is the Director of Sustainability Communications for Cummins Inc. Blair joined the Company in 2008 as the Diversity Communications Director. Blair comes from a newspaper background. He worked previously for the Indianapolis Star (2002-2008) and for the Des Moines Register (1997-2002) prior to that. [email protected]

 

Making the best of a bad situation to feed hungry kids

The canteen staff at the Daventry Engine Plant is now making lunches for disadvantaged youth in the community.
The canteen staff at the Daventry Engine Plant is now making lunches for disadvantaged youth in the community.

What do you do when you have more food than you know what to do with? For Cummins’ Daventry Engine Plant in the U.K. and the operator of its canteen, the answer became clear: feed hungry children. 

The plant and canteen are partnering with a not-for-profit group to make the best of the COVID-19 crisis, delivering prepared lunches to vulnerable children. Here’s how it all came together.

The canteen is operated by an outside supplier. It’s local manager and his staff have been working at the plant so long they are part of the plant family. As the plant implemented social distancing and work-from-home when possible, it became obvious the canteen should provide take-away service only.

As a result, canteen utilization decreased, and the canteen had excess food available that it didn’t want to spoil.The canteen manager spoke with Daventry Plant Manager Dave Barker about the challenges the canteen was facing and together they devised a plan.

First, the canteen began selling basic groceries to Cummins employees at cost, including pasta, eggs, bread and milk. This eased the shopping burden on the plant’s essential workforce at a time many grocery stores across the country, and around the world for that matter, were finding it hard to keep the basics on their shelves.  Then, the partners thought about what else they could do.

Lunches at the Daventry canteen packed and ready to go to children
Lunches at the Daventry canteen, packed and ready to go.

This time, they engaged the plant’s Community Involvement Team. The team reached out to local schools and learned some needed help providing lunches to vulnerable children with schools closed.

They also learned a Daventry charity needed a kitchen to continue providing meals to underprivileged children.The partners gave the charity a new option: focus on demand and distribution while the canteen staff takes on food production.

Today, the Daventry canteen staff is producing 300 packed lunches per day, which the charity delivers to local schools and sometimes directly to the homes of vulnerable children who typically receive free lunches when schools are open.

When the organization leaves a meal at a doorstep to maintain social distancing, the recipients often shout out their appreciation from doors or windows as the charity volunteers delivering the meals depart.

“These community actions are really impactful and they boost morale for our employees at a time when many are feeling a little nervous,” Barker said. “The overwhelming positive response from our community and our Daventry employees is motivating us all.”

Cummins Office Building

Cummins Inc.

Cummins is a global power leader that designs, manufactures, sells and services diesel and alternative fuel engines from 2.8 to 95 liters, diesel and alternative-fueled electrical generator sets from 2.5 to 3,500 kW, as well as related components and technology. Cummins serves its customers through its network of 600 company-owned and independent distributor facilities and more than 7,200 dealer locations in over 190 countries and territories.

Redirecting to
cummins.com

The information you are looking for is on
cummins.com

We are launching that site for you now.

Thank you.