Model year 2021 Apache sprayers get Cummins Performance Series power

Cummins Inc. (NYSE: CMI) announces that Equipment Technologies (ET) will feature Cummins’ latest Performance Series engine technology in their model year 2021 Apache AS850, AS1050, and AS1250/XP agriculture sprayers.
Powered by either the Cummins B4.5 or B6.7 Performance Series engines, Apache AS Series sprayers are equipped with both the power and torque required to conquer the toughest field conditions. The B4.5 and B6.7’s simpler architecture and EGR-free design means each engine is lighter and more compact than its predecessor, supporting ET’s objective of light-in-the-field machines for less soil compaction and reduced fuel consumption.
“With the new Performance Series engines, Apache AS Series sprayers receive a performance boost of up to 15% due to the increased power and torque available throughout the engine speed range. They are also more productive on the farm, saving farmers 8% in fuel with an overall combined fuel and Diesel Exhaust Fluid (DEF) saving of 3%. Not only does this have significant environmental and sustainability benefits, it also lowers operating costs – which is a big win for our customers. We are happy to collaborate with Cummins to introduce the Performance Series engines into our sprayer line-up.” explains Veera Rajendran, Vice President Engineering, ET.
Apache AS Series self-propelled sprayers are one of the first in the U.S. to adopt Cummins Performance Series power and are dual certified to comply with EU Stage V - the strictest emissions standard globally - as well as EPA Tier 4 Final. Cummins’ new Single Module™ aftertreatment is up to 40% smaller and 20% lighter than previous systems and is positioned vertically on the new AS Series sprayers to facilitate new storage features, while maintaining visibility from the cab.
Doug Keele, ET Account Manager at Cummins adds, “We were excited when ET approached us with a new objective to increase the power and capability of several AS Series sprayers. With a business relationship spanning more than 20 years, our work together has always focused on the farmers who operate Apache products. We knew our Performance Series engine technology could achieve ET’s objectives as well as provide additional performance, efficiency and value-retention benefits for Apache sprayer owners globally.”
Cummins Performance Series engines are manufactured at its Rocky Mount engine plant in North Carolina, U.S.
글로벌 전력 기술 리더인 Cummins Inc.는 광범위한 전력 솔루션 포트폴리오를 설계, 제조, 배포 및 서비스하는 보완 비즈니스 부문의 기업입니다. 이 회사의 제품은 내연, 전기 및 하이브리드 통합 전력 솔루션에서부터 여과, 후처리, 터보차저, 연료 시스템, 제어 시스템, 공기 처리 시스템, 자동 변속기, 전기 발전 시스템, 마이크로그리드 제어 장치, 배터리, 전해조 및 연료 전지 제품을 포함한 구성품에 이르기까지 다양합니다.
Headquartered in Columbus, Indiana (U.S.), since its founding in 1919, Cummins employs approximately 59,900 people committed to powering a more prosperous world through three global corporate responsibility priorities critical to healthy communities: education, environment and equality of opportunity. Cummins serves its customers online, through a network of company-owned and independent distributor locations, and through thousands of dealer locations worldwide and earned about $2.1 billion on sales of $24 billion in 2021.